EUSART - Extended USART#

Extended Universal Synchronous/Asynchronous Receiver/Transmitter.

Introduction#

This module contains functions to control the Enhanced Universal Synchronous / Asynchronous Receiver / Transmitter controller(s) (EUSART) peripheral of Silicon Labs' 32-bit MCUs and SoCs. EUSART can be used as a UART and can, therefore, be connected to an external transceiver to communicate with another host using the serial link.

It supports full duplex asynchronous UART communication as well as RS-485, SPI, MicroWire, and 3-wire. It can also interface with ISO7816 Smart-Cards, and IrDA devices.

EUSART has a wide selection of operating modes, frame formats, and baud rates. All features are supported through the API of this module.

This module does not support DMA configuration. UARTDRV and SPIDRV drivers provide full support for DMA and more.

Example#

EUSART Async TX example:

{
  EUSART_UartInit_TypeDef init = EUSART_UART_INIT_DEFAULT_HF;

  // Configure the clocks.
  CMU_ClockSelectSet(cmuClock_EUSART0CLK, cmuSelect_EM01GRPCCLK);
  CMU_ClockEnable(cmuClock_EUSART0CLK, true);
  // Initialize the EUSART
  EUSART_UartInitHf(EUSART0, &init);
  EUSART_Tx(EUSART0, data);
}

EUSART Sync SPI Transaction example:

{
  EUSART_SpiInit_TypeDef init_master = EUSART_SPI_MASTER_INIT_DEFAULT_HF;

  // Configure the clocks.
  CMU_ClockSelectSet(cmuClock_EM01GRPCCLK, cmuSelect_HFRCODPLL);
  CMU_ClockEnable(cmuClock_EUSART1, true);
  CMU_ClockEnable(cmuClock_GPIO, true);

  //Configure the SPI ports
  GPIO_PinModeSet(sclk_port, sclk_pin, gpioModePushPull, 0);
  GPIO_PinModeSet(mosi_port, mosi_pin, gpioModePushPull, 0);
  GPIO_PinModeSet(mosi_port, miso_pin, gpioModeInput, 0);

  // Connect EUSART to ports
  GPIO->EUSARTROUTE[EUSART_NUM(EUSART1)].TXROUTE = (mosi_port << _GPIO_EUSART_TXROUTE_PORT_SHIFT)
                                                   | (mosi_pin << _GPIO_EUSART_TXROUTE_PIN_SHIFT);
  GPIO->EUSARTROUTE[EUSART_NUM(EUSART1)].RXROUTE = (miso_port << _GPIO_EUSART_RXROUTE_PORT_SHIFT)
                                                   | (miso_pin << _GPIO_EUSART_RXROUTE_PIN_SHIFT);
  GPIO->EUSARTROUTE[EUSART_NUM(EUSART1)].SCLKROUTE = (sclk_port << _GPIO_EUSART_SCLKROUTE_PORT_SHIFT)
                                                   | (sclk_pin << _GPIO_EUSART_SCLKROUTE_PIN_SHIFT);
  GPIO->EUSARTROUTE[EUSART_NUM(EUSART1)].ROUTEEN = GPIO_EUSART_ROUTEEN_TXPEN | GPIO_EUSART_ROUTEEN_SCLKPEN;

  // Initialize the EUSART
  EUSART_SpiInit(EUSART1, &init_master);
  EUSART_Spi_TxRx(EUSART1, data);
}

EM2 guidelines for non EM2-Capable instances#

Note

  • EUSART instances located in the PD1 power domain are non EM2-capable. The EUSART_EM2_CAPABLE() and EUSART_NOT_EM2_CAPABLE() macros can be used to determine whether or not a EUSART instance is EM2-Capable.

Follow theses steps when entering in EM2:

  1. Wait for the current transaction to complete with TXCIF interrupt

  2. Disable TX and RX using TXDIS and RXDIS cmd

  3. Poll for EUSARTn_SYNCBUSY.TXDIS and EUSARTn_SYNCBUSY.RXDIS to go low

  4. Wait for EUSARTn_STATUS.TXENS and EUSARTn_STATUS.RXENS to go low

  5. Disable SCLKPEN and CSPEN in GPIO if they were previously enabled

  6. Enter EM2

On wakeup from EM2, EUSART transmitter/receiver and relevant GPIO (SCLKPEN and CSPEN) must be re-enabled. For example:

{
  // Enable TX and RX
  EUSART_Enable(EUSART0, eusartEnable);
  BUS_RegMaskedWrite(&GPIO->EUSARTROUTE[EUSART_NUM(EUSART0)].ROUTEEN,
                     _GPIO_EUSART_ROUTEEN_TXPEN_MASK | _GPIO_EUSART_ROUTEEN_SCLKPEN_MASK,
                     GPIO_EUSART_ROUTEEN_TXPEN | GPIO_EUSART_ROUTEEN_SCLKPEN);
}

Modules#

EUSART_AdvancedInit_TypeDef

EUSART_UartInit_TypeDef

EUSART_IrDAInit_TypeDef

EUSART_PrsTriggerInit_TypeDef

EUSART_SpiAdvancedInit_TypeDef

EUSART_SpiInit_TypeDef

EUSART_DaliInit_TypeDef

Enumerations#

enum
eusartDisable = 0x0
eusartEnableRx = (EUSART_CMD_RXEN | EUSART_CMD_TXDIS)
eusartEnableTx = (EUSART_CMD_TXEN | EUSART_CMD_RXDIS)
eusartEnable = (EUSART_CMD_RXEN | EUSART_CMD_TXEN)
}

Enable selection.

enum
eusartDataBits7 = EUSART_FRAMECFG_DATABITS_SEVEN
eusartDataBits8 = EUSART_FRAMECFG_DATABITS_EIGHT
eusartDataBits9 = EUSART_FRAMECFG_DATABITS_NINE
eusartDataBits10 = EUSART_FRAMECFG_DATABITS_TEN
eusartDataBits11 = EUSART_FRAMECFG_DATABITS_ELEVEN
eusartDataBits12 = EUSART_FRAMECFG_DATABITS_TWELVE
eusartDataBits13 = EUSART_FRAMECFG_DATABITS_THIRTEEN
eusartDataBits14 = EUSART_FRAMECFG_DATABITS_FOURTEEN
eusartDataBits15 = EUSART_FRAMECFG_DATABITS_FIFTEEN
eusartDataBits16 = EUSART_FRAMECFG_DATABITS_SIXTEEN
}

Data bit selection.

enum
eusartNoParity = EUSART_FRAMECFG_PARITY_NONE
eusartEvenParity = EUSART_FRAMECFG_PARITY_EVEN
eusartOddParity = EUSART_FRAMECFG_PARITY_ODD
}

Parity selection.

enum
eusartStopbits0p5 = EUSART_FRAMECFG_STOPBITS_HALF
eusartStopbits1p5 = EUSART_FRAMECFG_STOPBITS_ONEANDAHALF
eusartStopbits1 = EUSART_FRAMECFG_STOPBITS_ONE
eusartStopbits2 = EUSART_FRAMECFG_STOPBITS_TWO
}

Stop bits selection.

enum
eusartOVS16 = EUSART_CFG0_OVS_X16
eusartOVS8 = EUSART_CFG0_OVS_X8
eusartOVS6 = EUSART_CFG0_OVS_X6
eusartOVS4 = EUSART_CFG0_OVS_X4
eusartOVS0 = EUSART_CFG0_OVS_DISABLE
}

Oversampling selection, used for asynchronous operation.

enum
eusartHwFlowControlNone = 0
eusartHwFlowControlCts
eusartHwFlowControlRts
eusartHwFlowControlCtsAndRts
}

HW flow control config.

enum
eusartLoopbackEnable = EUSART_CFG0_LOOPBK
eusartLoopbackDisable = _EUSART_CFG0_RESETVALUE
}

Loopback enable.

enum
eusartMajorityVoteEnable = EUSART_CFG0_MVDIS_DEFAULT
eusartMajorityVoteDisable = EUSART_CFG0_MVDIS
}

Majority vote enable.

enum
eusartBlockRxEnable = EUSART_CMD_RXBLOCKEN
eusartBlockRxDisable = EUSART_CMD_RXBLOCKDIS
}

Block reception enable.

enum
eusartTristateTxEnable = EUSART_CMD_TXTRIEN
eusartTristateTxDisable = EUSART_CMD_TXTRIDIS
}

TX output tristate enable.

enum
eusartIrDARxFilterEnable = EUSART_IRHFCFG_IRHFFILT_ENABLE
eusartIrDARxFilterDisable = EUSART_IRHFCFG_IRHFFILT_DISABLE
}

IrDA filter enable.

enum
eusartIrDAPulseWidthOne = EUSART_IRHFCFG_IRHFPW_ONE
eusartIrDAPulseWidthTwo = EUSART_IRHFCFG_IRHFPW_TWO
eusartIrDAPulseWidthThree = EUSART_IRHFCFG_IRHFPW_THREE
eusartIrDAPulseWidthFour = EUSART_IRHFCFG_IRHFPW_FOUR
}

Pulse width selection for IrDA mode.

enum
eusartPrsTriggerDisable = 0x0
eusartPrsTriggerEnableRx = EUSART_TRIGCTRL_RXTEN
eusartPrsTriggerEnableTx = EUSART_TRIGCTRL_TXTEN
eusartPrsTriggerEnableRxTx = (EUSART_TRIGCTRL_RXTEN | EUSART_TRIGCTRL_TXTEN)
}

PRS trigger enable.

enum
eusartInvertIODisable = (EUSART_CFG0_RXINV_DISABLE | EUSART_CFG0_TXINV_DISABLE)
eusartInvertRxEnable = EUSART_CFG0_RXINV_ENABLE
eusartInvertTxEnable = EUSART_CFG0_TXINV_ENABLE
eusartInvertIOEnable = (EUSART_CFG0_RXINV_ENABLE | EUSART_CFG0_TXINV_ENABLE)
}

IO polarity selection.

enum
eusartAutoTxDelayNone = EUSART_TIMINGCFG_TXDELAY_NONE
eusartAutoTxDelaySingle = EUSART_TIMINGCFG_TXDELAY_SINGLE
eusartAutoTxDelayDouble = EUSART_TIMINGCFG_TXDELAY_DOUBLE
eusartAutoTxDelayTripple = EUSART_TIMINGCFG_TXDELAY_TRIPPLE
}

Auto TX delay transmission.

enum
eusartRxFiFoWatermark1Frame = EUSART_CFG1_RXFIW_ONEFRAME
eusartRxFiFoWatermark2Frame = EUSART_CFG1_RXFIW_TWOFRAMES
eusartRxFiFoWatermark3Frame = EUSART_CFG1_RXFIW_THREEFRAMES
eusartRxFiFoWatermark4Frame = EUSART_CFG1_RXFIW_FOURFRAMES
eusartRxFiFoWatermark5Frame = EUSART_CFG1_RXFIW_FIVEFRAMES
eusartRxFiFoWatermark6Frame = EUSART_CFG1_RXFIW_SIXFRAMES
eusartRxFiFoWatermark7Frame = EUSART_CFG1_RXFIW_SEVENFRAMES
eusartRxFiFoWatermark8Frame = EUSART_CFG1_RXFIW_EIGHTFRAMES
eusartRxFiFoWatermark9Frame = EUSART_CFG1_RXFIW_NINEFRAMES
eusartRxFiFoWatermark10Frame = EUSART_CFG1_RXFIW_TENFRAMES
eusartRxFiFoWatermark11Frame = EUSART_CFG1_RXFIW_ELEVENFRAMES
eusartRxFiFoWatermark12Frame = EUSART_CFG1_RXFIW_TWELVEFRAMES
eusartRxFiFoWatermark13Frame = EUSART_CFG1_RXFIW_THIRTEENFRAMES
eusartRxFiFoWatermark14Frame = EUSART_CFG1_RXFIW_FOURTEENFRAMES
eusartRxFiFoWatermark15Frame = EUSART_CFG1_RXFIW_FIFTEENFRAMES
eusartRxFiFoWatermark16Frame = EUSART_CFG1_RXFIW_SIXTEENFRAMES
}

RX FIFO Interrupt ans Status Watermark.

enum
eusartTxFiFoWatermark1Frame = EUSART_CFG1_TXFIW_ONEFRAME
eusartTxFiFoWatermark2Frame = EUSART_CFG1_TXFIW_TWOFRAMES
eusartTxFiFoWatermark3Frame = EUSART_CFG1_TXFIW_THREEFRAMES
eusartTxFiFoWatermark4Frame = EUSART_CFG1_TXFIW_FOURFRAMES
eusartTxFiFoWatermark5Frame = EUSART_CFG1_TXFIW_FIVEFRAMES
eusartTxFiFoWatermark6Frame = EUSART_CFG1_TXFIW_SIXFRAMES
eusartTxFiFoWatermark7Frame = EUSART_CFG1_TXFIW_SEVENFRAMES
eusartTxFiFoWatermark8Frame = EUSART_CFG1_TXFIW_EIGHTFRAMES
eusartTxFiFoWatermark9Frame = EUSART_CFG1_TXFIW_NINEFRAMES
eusartTxFiFoWatermark10Frame = EUSART_CFG1_TXFIW_TENFRAMES
eusartTxFiFoWatermark11Frame = EUSART_CFG1_TXFIW_ELEVENFRAMES
eusartTxFiFoWatermark12Frame = EUSART_CFG1_TXFIW_TWELVEFRAMES
eusartTxFiFoWatermark13Frame = EUSART_CFG1_TXFIW_THIRTEENFRAMES
eusartTxFiFoWatermark14Frame = EUSART_CFG1_TXFIW_FOURTEENFRAMES
eusartTxFiFoWatermark15Frame = EUSART_CFG1_TXFIW_FIFTEENFRAMES
eusartTxFiFoWatermark16Frame = EUSART_CFG1_TXFIW_SIXTEENFRAMES
}

TX FIFO Interrupt and Status Watermark.

enum
eusartClockMode0 = EUSART_CFG2_CLKPOL_IDLELOW | EUSART_CFG2_CLKPHA_SAMPLELEADING
eusartClockMode1 = EUSART_CFG2_CLKPOL_IDLELOW | EUSART_CFG2_CLKPHA_SAMPLETRAILING
eusartClockMode2 = EUSART_CFG2_CLKPOL_IDLEHIGH | EUSART_CFG2_CLKPHA_SAMPLELEADING
eusartClockMode3 = EUSART_CFG2_CLKPOL_IDLEHIGH | EUSART_CFG2_CLKPHA_SAMPLETRAILING
}

Clock polarity/phase mode.

enum
eusartCsActiveLow = EUSART_CFG2_CSINV_AL
eusartCsActiveHigh = EUSART_CFG2_CSINV_AH
}

Chip select polarity.

enum
eusartDaliTxDataBits8 = EUSART_DALICFG_DALITXDATABITS_EIGHT
eusartDaliTxDataBits9 = EUSART_DALICFG_DALITXDATABITS_NINE
eusartDaliTxDataBits10 = EUSART_DALICFG_DALITXDATABITS_TEN
eusartDaliTxDataBits11 = EUSART_DALICFG_DALITXDATABITS_ELEVEN
eusartDaliTxDataBits12 = EUSART_DALICFG_DALITXDATABITS_TWELVE
eusartDaliTxDataBits13 = EUSART_DALICFG_DALITXDATABITS_THIRTEEN
eusartDaliTxDataBits14 = EUSART_DALICFG_DALITXDATABITS_FOURTEEN
eusartDaliTxDataBits15 = EUSART_DALICFG_DALITXDATABITS_FIFTEEN
eusartDaliTxDataBits16 = EUSART_DALICFG_DALITXDATABITS_SIXTEEN
eusartDaliTxDataBits17 = EUSART_DALICFG_DALITXDATABITS_SEVENTEEN
eusartDaliTxDataBits18 = EUSART_DALICFG_DALITXDATABITS_EIGHTEEN
eusartDaliTxDataBits19 = EUSART_DALICFG_DALITXDATABITS_NINETEEN
eusartDaliTxDataBits20 = EUSART_DALICFG_DALITXDATABITS_TWENTY
eusartDaliTxDataBits21 = EUSART_DALICFG_DALITXDATABITS_TWENTYONE
eusartDaliTxDataBits22 = EUSART_DALICFG_DALITXDATABITS_TWENTYTWO
eusartDaliTxDataBits23 = EUSART_DALICFG_DALITXDATABITS_TWENTYTHREE
eusartDaliTxDataBits24 = EUSART_DALICFG_DALITXDATABITS_TWENTYFOUR
eusartDaliTxDataBits25 = EUSART_DALICFG_DALITXDATABITS_TWENTYFIVE
eusartDaliTxDataBits26 = EUSART_DALICFG_DALITXDATABITS_TWENTYSIX
eusartDaliTxDataBits27 = EUSART_DALICFG_DALITXDATABITS_TWENTYSEVEN
eusartDaliTxDataBits28 = EUSART_DALICFG_DALITXDATABITS_TWENTYEIGHT
eusartDaliTxDataBits29 = EUSART_DALICFG_DALITXDATABITS_TWENTYNINE
eusartDaliTxDataBits30 = EUSART_DALICFG_DALITXDATABITS_THIRTY
eusartDaliTxDataBits31 = EUSART_DALICFG_DALITXDATABITS_THIRTYONE
eusartDaliTxDataBits32 = EUSART_DALICFG_DALITXDATABITS_THIRTYTWO
}

DALI TX databits (8-32).

enum
eusartDaliRxDataBits8 = EUSART_DALICFG_DALIRXDATABITS_EIGHT
eusartDaliRxDataBits9 = EUSART_DALICFG_DALIRXDATABITS_NINE
eusartDaliRxDataBits10 = EUSART_DALICFG_DALIRXDATABITS_TEN
eusartDaliRxDataBits11 = EUSART_DALICFG_DALIRXDATABITS_ELEVEN
eusartDaliRxDataBits12 = EUSART_DALICFG_DALIRXDATABITS_TWELVE
eusartDaliRxDataBits13 = EUSART_DALICFG_DALIRXDATABITS_THIRTEEN
eusartDaliRxDataBits14 = EUSART_DALICFG_DALIRXDATABITS_FOURTEEN
eusartDaliRxDataBits15 = EUSART_DALICFG_DALIRXDATABITS_FIFTEEN
eusartDaliRxDataBits16 = EUSART_DALICFG_DALIRXDATABITS_SIXTEEN
eusartDaliRxDataBits17 = EUSART_DALICFG_DALIRXDATABITS_SEVENTEEN
eusartDaliRxDataBits18 = EUSART_DALICFG_DALIRXDATABITS_EIGHTEEN
eusartDaliRxDataBits19 = EUSART_DALICFG_DALIRXDATABITS_NINETEEN
eusartDaliRxDataBits20 = EUSART_DALICFG_DALIRXDATABITS_TWENTY
eusartDaliRxDataBits21 = EUSART_DALICFG_DALIRXDATABITS_TWENTYONE
eusartDaliRxDataBits22 = EUSART_DALICFG_DALIRXDATABITS_TWENTYTWO
eusartDaliRxDataBits23 = EUSART_DALICFG_DALITXDATABITS_TWENTYTHREE
eusartDaliRxDataBits24 = EUSART_DALICFG_DALIRXDATABITS_TWENTYFOUR
eusartDaliRxDataBits25 = EUSART_DALICFG_DALIRXDATABITS_TWENTYFIVE
eusartDaliRxDataBits26 = EUSART_DALICFG_DALIRXDATABITS_TWENTYSIX
eusartDaliRxDataBits27 = EUSART_DALICFG_DALIRXDATABITS_TWENTYSEVEN
eusartDaliRxDataBits28 = EUSART_DALICFG_DALIRXDATABITS_TWENTYEIGHT
eusartDaliRxDataBits29 = EUSART_DALICFG_DALIRXDATABITS_TWENTYNINE
eusartDaliRxDataBits30 = EUSART_DALICFG_DALIRXDATABITS_THIRTY
eusartDaliRxDataBits31 = EUSART_DALICFG_DALIRXDATABITS_THIRTYONE
eusartDaliRxDataBits32 = EUSART_DALICFG_DALIRXDATABITS_THIRTYTWO
}

DALI RX databits (8-32).

Typedefs#

typedef uint8_t

PRS Channel type.

Functions#

void
EUSART_UartInitHf(EUSART_TypeDef *eusart, const EUSART_UartInit_TypeDef *init)

Initialize EUSART when used in UART mode with the high frequency clock.

void
EUSART_UartInitLf(EUSART_TypeDef *eusart, const EUSART_UartInit_TypeDef *init)

Initialize EUSART when used in UART mode with the low frequency clock.

void
EUSART_IrDAInit(EUSART_TypeDef *eusart, const EUSART_IrDAInit_TypeDef *irdaInit)

Initialize EUSART when used in IrDA mode with the high or low frequency clock.

void
EUSART_SpiInit(EUSART_TypeDef *eusart, const EUSART_SpiInit_TypeDef *init)

Initialize EUSART when used in SPI mode.

void
EUSART_DaliInit(EUSART_TypeDef *eusart, const EUSART_DaliInit_TypeDef *daliInit)

Initialize EUSART when used in DALI mode with the high or low frequency clock.

void
EUSART_Reset(EUSART_TypeDef *eusart)

Configure EUSART to its reset state.

void
EUSART_Enable(EUSART_TypeDef *eusart, EUSART_Enable_TypeDef enable)

Enable/disable EUSART receiver and/or transmitter.

uint8_t
EUSART_Rx(EUSART_TypeDef *eusart)

Receive one 8 bit frame, (or part of 9 bit frame).

uint16_t
EUSART_RxExt(EUSART_TypeDef *eusart)

Receive one 8-16 bit frame with extended information.

void
EUSART_Tx(EUSART_TypeDef *eusart, uint8_t data)

Transmit one frame.

void
EUSART_TxExt(EUSART_TypeDef *eusart, uint16_t data)

Transmit one 8-9 bit frame with extended control.

uint16_t
EUSART_Spi_TxRx(EUSART_TypeDef *eusart, uint16_t data)

Transmit one 8-16 bit frame and return received data.

void
EUSART_Dali_Tx(EUSART_TypeDef *eusart, uint32_t data)

Transmit one DALI frame.

uint32_t
EUSART_Dali_Rx(EUSART_TypeDef *eusart)

Receive one 8-32 bit DALI frame.

void
EUSART_BaudrateSet(EUSART_TypeDef *eusart, uint32_t refFreq, uint32_t baudrate)

Configure the baudrate (or as close as possible to a specified baudrate).

uint32_t
EUSART_BaudrateGet(EUSART_TypeDef *eusart)

Get the current baudrate.

void
EUSART_RxBlock(EUSART_TypeDef *eusart, EUSART_BlockRx_TypeDef enable)

Enable/Disable reception operation until the configured start frame is received.

void
EUSART_TxTristateSet(EUSART_TypeDef *eusart, EUSART_TristateTx_TypeDef enable)

Enable/Disable the tristating of the transmitter output.

void
EUSART_PrsTriggerEnable(EUSART_TypeDef *eusart, const EUSART_PrsTriggerInit_TypeDef *init)

Initialize the automatic enabling of transmissions and/or reception using the PRS as a trigger.

uint32_t
EUSART_StatusGet(EUSART_TypeDef *eusart)

Get EUSART STATUS register.

void
EUSART_IntClear(EUSART_TypeDef *eusart, uint32_t flags)

Clear one or more pending EUSART interrupts.

void
EUSART_IntDisable(EUSART_TypeDef *eusart, uint32_t flags)

Disable one or more EUSART interrupts.

void
EUSART_IntEnable(EUSART_TypeDef *eusart, uint32_t flags)

Enable one or more EUSART interrupts.

uint32_t
EUSART_IntGet(EUSART_TypeDef *eusart)

Get pending EUSART interrupt flags.

uint32_t
EUSART_IntGetEnabled(EUSART_TypeDef *eusart)

Get enabled and pending EUSART interrupt flags.

void
EUSART_IntSet(EUSART_TypeDef *eusart, uint32_t flags)

Set one or more pending EUSART interrupts from SW.

Macros#

#define

Define EUSART FIFO Depth information.

#define
EUSART1_FIFO_DEPTH EUSART0_FIFO_DEPTH
#define
EUSART2_FIFO_DEPTH EUSART0_FIFO_DEPTH
#define
EUSART3_FIFO_DEPTH EUSART0_FIFO_DEPTH
#define
EUSART4_FIFO_DEPTH EUSART0_FIFO_DEPTH
#define

Default configuration for EUSART initialization structure in UART mode with high-frequency clock.

#define

Default start frame configuration, i.e. feature disabled.

#define

Default configuration for EUSART advanced initialization structure.

#define

Default configuration for EUSART initialization structure in UART mode with low-frequency clock.

#define

Default configuration for EUSART initialization structure in IrDA mode with high-frequency clock.

#define

Default configuration for EUSART initialization structure in IrDA mode with low-frequency clock.

#define

Default advanced configuration for EUSART initialization structure in SPI mode with high-frequency clock.

#define

Default configuration for EUSART initialization structure in SPI master mode with high-frequency clock.

#define

Default configuration for EUSART initialization structure in SPI slave mode with high-frequency clock.

#define

Default configuration for EUSART initialization structure in DALI mode with high-frequency clock.

#define

Default configuration for EUSART initialization structure in DALI mode with high-frequency clock.

#define

Default configuration for EUSART initialization structure in DALI mode with low-frequency clock.

#define

Default configuration for EUSART initialization structure in DALI mode with high-frequency clock.

#define

Default configuration for EUSART initialization structure in DALI mode with low-frequency clock.

Enumeration Documentation#

EUSART_Enable_TypeDef#

EUSART_Enable_TypeDef

Enable selection.

Enumerator
eusartDisable

Disable the peripheral.

eusartEnableRx

Enable receiver only, transmitter disabled.

eusartEnableTx

Enable transmitter only, receiver disabled.

eusartEnable

Enable both receiver and transmitter.


EUSART_Databits_TypeDef#

EUSART_Databits_TypeDef

Data bit selection.

Enumerator
eusartDataBits7

7 data bits.

eusartDataBits8

8 data bits.

eusartDataBits9

9 data bits.

eusartDataBits10

10 data bits, SPI mode only.

eusartDataBits11

11 data bits, SPI mode only.

eusartDataBits12

12 data bits, SPI mode only.

eusartDataBits13

13 data bits, SPI mode only.

eusartDataBits14

14 data bits, SPI mode only.

eusartDataBits15

15 data bits, SPI mode only.

eusartDataBits16

16 data bits, SPI mode only.


EUSART_Parity_TypeDef#

EUSART_Parity_TypeDef

Parity selection.

Enumerator
eusartNoParity

No parity.

eusartEvenParity

Even parity.

eusartOddParity

Odd parity.


EUSART_Stopbits_TypeDef#

EUSART_Stopbits_TypeDef

Stop bits selection.

Enumerator
eusartStopbits0p5

0.5 stop bits.

eusartStopbits1p5

1.5 stop bits.

eusartStopbits1

1 stop bits.

eusartStopbits2

2 stop bits.


EUSART_OVS_TypeDef#

EUSART_OVS_TypeDef

Oversampling selection, used for asynchronous operation.

Enumerator
eusartOVS16

16x oversampling (normal).

eusartOVS8

8x oversampling.

eusartOVS6

6x oversampling.

eusartOVS4

4x oversampling.

eusartOVS0

Oversampling disabled.


EUSART_HwFlowControl_TypeDef#

EUSART_HwFlowControl_TypeDef

HW flow control config.

Enumerator
eusartHwFlowControlNone

No HW Flow Control.

eusartHwFlowControlCts

CTS HW Flow Control.

eusartHwFlowControlRts

RTS HW Flow Control.

eusartHwFlowControlCtsAndRts

CTS and RTS HW Flow Control.


EUSART_LoopbackEnable_TypeDef#

EUSART_LoopbackEnable_TypeDef

Loopback enable.

Enumerator
eusartLoopbackEnable

Enable loopback.

eusartLoopbackDisable

Disable loopback.


EUSART_MajorityVote_TypeDef#

EUSART_MajorityVote_TypeDef

Majority vote enable.

Enumerator
eusartMajorityVoteEnable

Enable majority vote for 16x, 8x and 6x oversampling modes.

eusartMajorityVoteDisable

Disable majority vote for 16x, 8x and 6x oversampling modes.


EUSART_BlockRx_TypeDef#

EUSART_BlockRx_TypeDef

Block reception enable.

Enumerator
eusartBlockRxEnable

Block reception enable, resulting in all incoming frames being discarded.

eusartBlockRxDisable

Block reception disable, resulting in all incoming frames being loaded into the RX FIFO.


EUSART_TristateTx_TypeDef#

EUSART_TristateTx_TypeDef

TX output tristate enable.

Enumerator
eusartTristateTxEnable

Tristates the transmitter output.

eusartTristateTxDisable

Disables tristating of the transmitter output.


EUSART_IrDARxFilterEnable_TypeDef#

EUSART_IrDARxFilterEnable_TypeDef

IrDA filter enable.

Enumerator
eusartIrDARxFilterEnable

Enable filter on demodulator.

eusartIrDARxFilterDisable

Disable filter on demodulator.


EUSART_IrDAPulseWidth_Typedef#

EUSART_IrDAPulseWidth_Typedef

Pulse width selection for IrDA mode.

Enumerator
eusartIrDAPulseWidthOne

IrDA pulse width is 1/16 for OVS=X16 and 1/8 for OVS=X8.

eusartIrDAPulseWidthTwo

IrDA pulse width is 2/16 for OVS=X16 and 2/8 for OVS=X8.

eusartIrDAPulseWidthThree

IrDA pulse width is 3/16 for OVS=X16 and 3/8 for OVS=X8.

eusartIrDAPulseWidthFour

IrDA pulse width is 4/16 for OVS=X16 and 4/8 for OVS=X8.


EUSART_PrsTriggerEnable_TypeDef#

EUSART_PrsTriggerEnable_TypeDef

PRS trigger enable.

Enumerator
eusartPrsTriggerDisable

Disable trigger on both receiver and transmitter.

eusartPrsTriggerEnableRx

Enable receive trigger only, transmit disabled.

eusartPrsTriggerEnableTx

Enable transmit trigger only, receive disabled.

eusartPrsTriggerEnableRxTx

Enable trigger on both receive and transmit.


EUSART_InvertIO_TypeDef#

EUSART_InvertIO_TypeDef

IO polarity selection.

Enumerator
eusartInvertIODisable

Disable inversion on both RX and TX signals.

eusartInvertRxEnable

Invert RX signal, before receiver.

eusartInvertTxEnable

Invert TX signal, after transmitter.

eusartInvertIOEnable

Enable trigger on both receive and transmit.


EUSART_AutoTxDelay_TypeDef#

EUSART_AutoTxDelay_TypeDef

Auto TX delay transmission.

Enumerator
eusartAutoTxDelayNone

Frames are transmitted immediately.

eusartAutoTxDelaySingle

Transmission of new frames is delayed by a single bit period.

eusartAutoTxDelayDouble

Transmission of new frames is delayed by a two bit periods.

eusartAutoTxDelayTripple

Transmission of new frames is delayed by a three bit periods.


EUSART_RxFifoWatermark_TypeDef#

EUSART_RxFifoWatermark_TypeDef

RX FIFO Interrupt ans Status Watermark.

Enumerator
eusartRxFiFoWatermark1Frame
eusartRxFiFoWatermark2Frame
eusartRxFiFoWatermark3Frame
eusartRxFiFoWatermark4Frame
eusartRxFiFoWatermark5Frame
eusartRxFiFoWatermark6Frame
eusartRxFiFoWatermark7Frame
eusartRxFiFoWatermark8Frame
eusartRxFiFoWatermark9Frame
eusartRxFiFoWatermark10Frame
eusartRxFiFoWatermark11Frame
eusartRxFiFoWatermark12Frame
eusartRxFiFoWatermark13Frame
eusartRxFiFoWatermark14Frame
eusartRxFiFoWatermark15Frame
eusartRxFiFoWatermark16Frame

EUSART_TxFifoWatermark_TypeDef#

EUSART_TxFifoWatermark_TypeDef

TX FIFO Interrupt and Status Watermark.

Enumerator
eusartTxFiFoWatermark1Frame
eusartTxFiFoWatermark2Frame
eusartTxFiFoWatermark3Frame
eusartTxFiFoWatermark4Frame
eusartTxFiFoWatermark5Frame
eusartTxFiFoWatermark6Frame
eusartTxFiFoWatermark7Frame
eusartTxFiFoWatermark8Frame
eusartTxFiFoWatermark9Frame
eusartTxFiFoWatermark10Frame
eusartTxFiFoWatermark11Frame
eusartTxFiFoWatermark12Frame
eusartTxFiFoWatermark13Frame
eusartTxFiFoWatermark14Frame
eusartTxFiFoWatermark15Frame
eusartTxFiFoWatermark16Frame

EUSART_ClockMode_TypeDef#

EUSART_ClockMode_TypeDef

Clock polarity/phase mode.

Enumerator
eusartClockMode0

Clock idle low, sample on rising edge.

eusartClockMode1

Clock idle low, sample on falling edge.

eusartClockMode2

Clock idle high, sample on falling edge.

eusartClockMode3

Clock idle high, sample on rising edge.


EUSART_CsPolarity_TypeDef#

EUSART_CsPolarity_TypeDef

Chip select polarity.

Enumerator
eusartCsActiveLow

Chip select active low.

eusartCsActiveHigh

Chip select active high.


EUSART_DaliTxDatabits_TypeDef#

EUSART_DaliTxDatabits_TypeDef

DALI TX databits (8-32).

Enumerator
eusartDaliTxDataBits8

Each frame contains 8 data bits.

eusartDaliTxDataBits9

Each frame contains 9 data bits.

eusartDaliTxDataBits10

Each frame contains 10 data bits.

eusartDaliTxDataBits11

Each frame contains 11 data bits.

eusartDaliTxDataBits12

Each frame contains 12 data bits.

eusartDaliTxDataBits13

Each frame contains 13 data bits.

eusartDaliTxDataBits14

Each frame contains 14 data bits.

eusartDaliTxDataBits15

Each frame contains 15 data bits.

eusartDaliTxDataBits16

Each frame contains 16 data bits.

eusartDaliTxDataBits17

Each frame contains 17 data bits.

eusartDaliTxDataBits18

Each frame contains 18 data bits.

eusartDaliTxDataBits19

Each frame contains 19 data bits.

eusartDaliTxDataBits20

Each frame contains 20 data bits.

eusartDaliTxDataBits21

Each frame contains 21 data bits.

eusartDaliTxDataBits22

Each frame contains 22 data bits.

eusartDaliTxDataBits23

Each frame contains 23 data bits.

eusartDaliTxDataBits24

Each frame contains 24 data bits.

eusartDaliTxDataBits25

Each frame contains 25 data bits.

eusartDaliTxDataBits26

Each frame contains 26 data bits.

eusartDaliTxDataBits27

Each frame contains 27 data bits.

eusartDaliTxDataBits28

Each frame contains 28 data bits.

eusartDaliTxDataBits29

Each frame contains 29 data bits.

eusartDaliTxDataBits30

Each frame contains 30 data bits.

eusartDaliTxDataBits31

Each frame contains 31 data bits.

eusartDaliTxDataBits32

Each frame contains 32 data bits.


EUSART_DaliRxDatabits_TypeDef#

EUSART_DaliRxDatabits_TypeDef

DALI RX databits (8-32).

Enumerator
eusartDaliRxDataBits8

Each frame contains 8 data bits.

eusartDaliRxDataBits9

Each frame contains 9 data bits.

eusartDaliRxDataBits10

Each frame contains 10 data bits.

eusartDaliRxDataBits11

Each frame contains 11 data bits.

eusartDaliRxDataBits12

Each frame contains 12 data bits.

eusartDaliRxDataBits13

Each frame contains 13 data bits.

eusartDaliRxDataBits14

Each frame contains 14 data bits.

eusartDaliRxDataBits15

Each frame contains 15 data bits.

eusartDaliRxDataBits16

Each frame contains 16 data bits.

eusartDaliRxDataBits17

Each frame contains 17 data bits.

eusartDaliRxDataBits18

Each frame contains 18 data bits.

eusartDaliRxDataBits19

Each frame contains 19 data bits.

eusartDaliRxDataBits20

Each frame contains 20 data bits.

eusartDaliRxDataBits21

Each frame contains 21 data bits.

eusartDaliRxDataBits22

Each frame contains 22 data bits.

eusartDaliRxDataBits23

Each frame contains 23 data bits.

eusartDaliRxDataBits24

Each frame contains 24 data bits.

eusartDaliRxDataBits25

Each frame contains 25 data bits.

eusartDaliRxDataBits26

Each frame contains 26 data bits.

eusartDaliRxDataBits27

Each frame contains 27 data bits.

eusartDaliRxDataBits28

Each frame contains 28 data bits.

eusartDaliRxDataBits29

Each frame contains 29 data bits.

eusartDaliRxDataBits30

Each frame contains 30 data bits.

eusartDaliRxDataBits31

Each frame contains 31 data bits.

eusartDaliRxDataBits32

Each frame contains 32 data bits.


Typedef Documentation#

EUSART_PrsChannel_TypeDef#

typedef uint8_t EUSART_PrsChannel_TypeDef

PRS Channel type.


Function Documentation#

EUSART_UartInitHf#

void EUSART_UartInitHf (EUSART_TypeDef * eusart, const EUSART_UartInit_TypeDef * init)

Initialize EUSART when used in UART mode with the high frequency clock.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

const EUSART_UartInit_TypeDef *N/Ainit

A pointer to the initialization structure.

Initialize EUSART when used in UART mode with the high frequency clock.


EUSART_UartInitLf#

void EUSART_UartInitLf (EUSART_TypeDef * eusart, const EUSART_UartInit_TypeDef * init)

Initialize EUSART when used in UART mode with the low frequency clock.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

const EUSART_UartInit_TypeDef *N/Ainit

A pointer to the initialization structure.

Initialize EUSART when used in UART mode with the low frequency clock.

Note

  • (1) When EUSART oversampling is set to eusartOVS0 (Disable), the peripheral clock frequency must be at least three times higher than the chosen baud rate. In LF, max input clock is 32768 (LFXO or LFRCO), thus 32768 / 3 ~ 9600 baudrate.


EUSART_IrDAInit#

void EUSART_IrDAInit (EUSART_TypeDef * eusart, const EUSART_IrDAInit_TypeDef * irdaInit)

Initialize EUSART when used in IrDA mode with the high or low frequency clock.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

const EUSART_IrDAInit_TypeDef *N/AirdaInit

A pointer to the initialization structure.

Initialize EUSART when used in IrDA mode with the high or low frequency clock.


EUSART_SpiInit#

void EUSART_SpiInit (EUSART_TypeDef * eusart, const EUSART_SpiInit_TypeDef * init)

Initialize EUSART when used in SPI mode.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

const EUSART_SpiInit_TypeDef *N/Ainit

A pointer to the initialization structure.

Initialize EUSART when used in SPI mode.


EUSART_DaliInit#

void EUSART_DaliInit (EUSART_TypeDef * eusart, const EUSART_DaliInit_TypeDef * daliInit)

Initialize EUSART when used in DALI mode with the high or low frequency clock.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

const EUSART_DaliInit_TypeDef *N/AdaliInit

A pointer to the initialization structure.

Initialize EUSART when used in DALI mode with the high or low frequency clock.

Note

  • (1) When EUSART oversampling is set to eusartOVS0 (Disable), the peripheral clock frequency must be at least three times higher than the chosen baud rate. In LF, max input clock is 32768 (LFXO or LFRCO), thus 32768 / 3 ~ 9600 baudrate.


EUSART_Reset#

void EUSART_Reset (EUSART_TypeDef * eusart)

Configure EUSART to its reset state.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

Configure EUSART to its reset state.


EUSART_Enable#

void EUSART_Enable (EUSART_TypeDef * eusart, EUSART_Enable_TypeDef enable)

Enable/disable EUSART receiver and/or transmitter.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

EUSART_Enable_TypeDefN/Aenable

Select the status for the receiver and transmitter.

Enable/disable EUSART receiver and/or transmitter.


EUSART_Rx#

uint8_t EUSART_Rx (EUSART_TypeDef * eusart)

Receive one 8 bit frame, (or part of 9 bit frame).

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

Note

  • This function is normally used to receive one frame when operating with frame length of 8 bits. See EUSART_RxExt() for reception of 9 bit frames. Notice that possible parity/stop bits are not considered a part of the specified frame bit length.

  • This function will stall if buffer is empty until data is received.

Returns

  • Data received.

Receive one 8 bit frame, (or part of 9 bit frame).

Note

  • (1) Handles the case where the RX Fifo Watermark has been set to N frames, and when N is greater than one. Attempt to read a frame from the RX Fifo. If the read is unsuccessful (i.e. no frames in the RX fifo), the RXFU interrupt flag is set. If the flag is set, wait to read again until the RXFL status flag is set, indicating there are N frames in the RX Fifo, where N is equal to the RX watermark level. Once there are N frames in the Fifo, read and return one frame. For consecutive N-1 reads there will be data available in the Fifo. Therefore, the RXUF interrupt will not be triggered eliminating delays between reads and sending N data frames in "bursts".


EUSART_RxExt#

uint16_t EUSART_RxExt (EUSART_TypeDef * eusart)

Receive one 8-16 bit frame with extended information.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

Note

  • This function is normally used to receive one frame and additional RX status information.

  • This function will stall if buffer is empty until data is received.

Returns

  • Data received and receive status.

Receive one 8-16 bit frame with extended information.


EUSART_Tx#

void EUSART_Tx (EUSART_TypeDef * eusart, uint8_t data)

Transmit one frame.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

uint8_tN/Adata

Data to transmit.

Note

  • Depending on the frame length configuration, 8 (least significant) bits from data are transmitted. If the frame length is 9, 8 bits are transmitted from data. See EUSART_TxExt() for transmitting 9 bit frame with full control of all 9 bits.

  • This function will stall if the 4 frame FIFO is full, until the buffer becomes available.

Transmit one frame.


EUSART_TxExt#

void EUSART_TxExt (EUSART_TypeDef * eusart, uint16_t data)

Transmit one 8-9 bit frame with extended control.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

uint16_tN/Adata

Data to transmit.

Note

  • Possible parity/stop bits in asynchronous mode are not considered part of a specified frame bit length.

  • This function will stall if buffer is full until the buffer becomes available.

Transmit one 8-9 bit frame with extended control.


EUSART_Spi_TxRx#

uint16_t EUSART_Spi_TxRx (EUSART_TypeDef * eusart, uint16_t data)

Transmit one 8-16 bit frame and return received data.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

uint16_tN/Adata

Data to transmit.

Returns

  • Data received and receive status.

Note

  • SPI master mode only.

  • This function will stall if the TX buffer is full until the buffer becomes available.

Transmit one 8-16 bit frame and return received data.


EUSART_Dali_Tx#

void EUSART_Dali_Tx (EUSART_TypeDef * eusart, uint32_t data)

Transmit one DALI frame.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

uint32_tN/Adata

Data to transmit.

Note

  • Depending on the TXdatabits configuration, N (least significant) bits from data are transmitted.

  • This function will stall if the 16 frame FIFO is full, until the buffer becomes available.

Transmit one DALI frame.


EUSART_Dali_Rx#

uint32_t EUSART_Dali_Rx (EUSART_TypeDef * eusart)

Receive one 8-32 bit DALI frame.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

Note

  • This function is normally used to receive one DALI frame (RXdatabits).

  • This function will stall if the 16 frame FIFO is empty until new data is received.

Returns

  • Data received. Depending on the RXdatabits configuration, N (least significant) bits are returned.

Receive one 8-32 bit DALI frame.


EUSART_BaudrateSet#

void EUSART_BaudrateSet (EUSART_TypeDef * eusart, uint32_t refFreq, uint32_t baudrate)

Configure the baudrate (or as close as possible to a specified baudrate).

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

uint32_tN/ArefFreq

The EUSART reference clock frequency in Hz that will be used. If set to 0, the currently configured peripheral clock is used.

uint32_tN/Abaudrate

A baudrate to try to achieve.

Configure the baudrate (or as close as possible to a specified baudrate).

Note

  • (1) When the oversampling is disabled, the peripheral clock frequency must be at least three times higher than the chosen baud rate.


EUSART_BaudrateGet#

uint32_t EUSART_BaudrateGet (EUSART_TypeDef * eusart)

Get the current baudrate.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

Returns

  • The current baudrate.

Get the current baudrate.


EUSART_RxBlock#

void EUSART_RxBlock (EUSART_TypeDef * eusart, EUSART_BlockRx_TypeDef enable)

Enable/Disable reception operation until the configured start frame is received.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

EUSART_BlockRx_TypeDefN/Aenable

Select the receiver blocking status.

Enable/Disable reception operation until the configured start frame is received.


EUSART_TxTristateSet#

void EUSART_TxTristateSet (EUSART_TypeDef * eusart, EUSART_TristateTx_TypeDef enable)

Enable/Disable the tristating of the transmitter output.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

EUSART_TristateTx_TypeDefN/Aenable

Select the transmitter tristate status.

Enable/Disable the tristating of the transmitter output.


EUSART_PrsTriggerEnable#

void EUSART_PrsTriggerEnable (EUSART_TypeDef * eusart, const EUSART_PrsTriggerInit_TypeDef * init)

Initialize the automatic enabling of transmissions and/or reception using the PRS as a trigger.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

const EUSART_PrsTriggerInit_TypeDef *N/Ainit

Pointer to the initialization structure.

Note

Initialize the automatic enabling of transmissions and/or reception using the PRS as a trigger.


EUSART_StatusGet#

uint32_t EUSART_StatusGet (EUSART_TypeDef * eusart)

Get EUSART STATUS register.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

Returns

  • STATUS register value.


EUSART_IntClear#

void EUSART_IntClear (EUSART_TypeDef * eusart, uint32_t flags)

Clear one or more pending EUSART interrupts.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

uint32_tN/Aflags

Pending EUSART interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for EUSART module (EUSART_IF_nnn).


EUSART_IntDisable#

void EUSART_IntDisable (EUSART_TypeDef * eusart, uint32_t flags)

Disable one or more EUSART interrupts.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

uint32_tN/Aflags

Pending EUSART interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for EUSART module (EUSART_IF_nnn).


EUSART_IntEnable#

void EUSART_IntEnable (EUSART_TypeDef * eusart, uint32_t flags)

Enable one or more EUSART interrupts.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

uint32_tN/Aflags

Pending EUSART interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for EUSART module (EUSART_IF_nnn).


EUSART_IntGet#

uint32_t EUSART_IntGet (EUSART_TypeDef * eusart)

Get pending EUSART interrupt flags.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

Returns

  • Pending EUSART interrupt sources.


EUSART_IntGetEnabled#

uint32_t EUSART_IntGetEnabled (EUSART_TypeDef * eusart)

Get enabled and pending EUSART interrupt flags.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

Useful for handling more interrupt sources in the same interrupt handler.

Returns

  • Pending and enabled EUSART interrupt sources.


EUSART_IntSet#

void EUSART_IntSet (EUSART_TypeDef * eusart, uint32_t flags)

Set one or more pending EUSART interrupts from SW.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *N/Aeusart

Pointer to the EUSART peripheral register block.

uint32_tN/Aflags

Interrupt source(s) to set to pending. Use a bitwise logic OR combination of valid interrupt flags for EUSART module (EUSART_IF_nnn).


Macro Definition Documentation#

EUSART0_FIFO_DEPTH#

#define EUSART0_FIFO_DEPTH
Value:
16

Define EUSART FIFO Depth information.


EUSART1_FIFO_DEPTH#

#define EUSART1_FIFO_DEPTH
Value:
EUSART0_FIFO_DEPTH

EUSART2_FIFO_DEPTH#

#define EUSART2_FIFO_DEPTH
Value:
EUSART0_FIFO_DEPTH

EUSART3_FIFO_DEPTH#

#define EUSART3_FIFO_DEPTH
Value:
EUSART0_FIFO_DEPTH

EUSART4_FIFO_DEPTH#

#define EUSART4_FIFO_DEPTH
Value:
EUSART0_FIFO_DEPTH

EUSART_FIFO_DEPTH#

#define EUSART_FIFO_DEPTH
Value:
(((n) == 0) ? EUSART0_FIFO_DEPTH \
: ((n) == 1) ? EUSART1_FIFO_DEPTH \
: ((n) == 2) ? EUSART2_FIFO_DEPTH \
: ((n) == 3) ? EUSART3_FIFO_DEPTH \
: ((n) == 4) ? EUSART4_FIFO_DEPTH \
: 0x0UL)

EUSART_UART_INIT_DEFAULT_HF#

#define EUSART_UART_INIT_DEFAULT_HF
Value:
{ \
eusartEnable, /* Enable RX/TX when initialization completed. */ \
0, /* Use current configured reference clock for configuring baud rate.*/ \
115200, /* 115200 bits/s. */ \
eusartOVS16, /* Oversampling x16. */ \
eusartDataBits8, /* 8 data bits. */ \
eusartNoParity, /* No parity. */ \
eusartStopbits1, /* 1 stop bit. */ \
eusartMajorityVoteEnable, /* Majority vote enabled. */ \
eusartLoopbackDisable, /* Loop back disabled. */ \
NULL, /* Default advanced settings. */ \
}

Default configuration for EUSART initialization structure in UART mode with high-frequency clock.


EUSART_DEFAULT_START_FRAME#

#define EUSART_DEFAULT_START_FRAME
Value:
0x00u

Default start frame configuration, i.e. feature disabled.


EUSART_ADVANCED_INIT_DEFAULT#

#define EUSART_ADVANCED_INIT_DEFAULT
Value:
{ \
eusartHwFlowControlNone, /* Flow control disabled. */ \
false, /* Collision detection disabled. */ \
false, /* Data is sent with the least significant bit first. */ \
eusartInvertIODisable, /* RX and TX signal active high. */ \
false, /* No DMA wake up on reception. */ \
false, /* No DMA wake up on transmission. */ \
false, /* Halt DMA on error disabled. */ \
EUSART_DEFAULT_START_FRAME, /* No start frame. */ \
false, /* TX auto tristate disabled. */ \
false, /* Do not use PRS signal as RX signal.*/ \
(EUSART_PrsChannel_TypeDef) 0u, /* EUSART RX connected to prs channel 0. */ \
false, /* Multiprocessor mode disabled. */ \
false, /* Multiprocessor address bit : 0.*/ \
eusartAutoTxDelayNone, /* Frames are transmitted immediately */ \
eusartRxFiFoWatermark1Frame, /* RXFL status/IF set when RX FIFO has at least one frame in it */ \
eusartTxFiFoWatermark1Frame, /* TXFL status/IF set when TX FIFO has space for at least one more frame */ \
}

Default configuration for EUSART advanced initialization structure.


EUSART_UART_INIT_DEFAULT_LF#

#define EUSART_UART_INIT_DEFAULT_LF
Value:
{ \
eusartEnable, /* Enable RX/TX when initialization completed. */ \
0, /* Use current configured reference clock for configuring baud rate.*/ \
9600, /* 9600 bits/s. */ \
eusartOVS0, /* Oversampling disabled. */ \
eusartDataBits8, /* 8 data bits. */ \
eusartNoParity, /* No parity. */ \
eusartStopbits1, /* 1 stop bit. */ \
eusartMajorityVoteDisable, /* Majority vote enabled. */ \
eusartLoopbackDisable, /* Loop back disabled. */ \
NULL, /* Default advanced settings. */ \
}

Default configuration for EUSART initialization structure in UART mode with low-frequency clock.


EUSART_IRDA_INIT_DEFAULT_HF#

#define EUSART_IRDA_INIT_DEFAULT_HF
Value:
{ \
EUSART_UART_INIT_DEFAULT_HF, /* Default high frequency configuration. */ \
false, /* Disable IrDA low frequency mode. */ \
eusartIrDARxFilterDisable, /* RX Filter disabled. */ \
eusartIrDAPulseWidthOne, /* Pulse width is set to 1/16. */ \
}

Default configuration for EUSART initialization structure in IrDA mode with high-frequency clock.


EUSART_IRDA_INIT_DEFAULT_LF#

#define EUSART_IRDA_INIT_DEFAULT_LF
Value:
{ \
{ \
eusartEnableRx, /* Enable RX when initialization completed (TX not allowed). */ \
0, /* Use current configured reference clock for configuring baud rate.*/ \
9600, /* 9600 bits/s. */ \
eusartOVS0, /* Oversampling disabled. */ \
eusartDataBits8, /* 8 data bits. */ \
eusartNoParity, /* No parity. */ \
eusartStopbits1, /* 1 stop bit. */ \
eusartMajorityVoteDisable, /* Majority vote enabled. */ \
eusartLoopbackDisable, /* Loop back disabled. */ \
NULL, /* Default advanced settings. */ \
}, \
true, /* Enable IrDA low frequency mode. */ \
eusartIrDARxFilterDisable, /* RX Filter disabled. */ \
eusartIrDAPulseWidthOne, /* Pulse width is set to 1. */ \
}

Default configuration for EUSART initialization structure in IrDA mode with low-frequency clock.


EUSART_SPI_ADVANCED_INIT_DEFAULT#

#define EUSART_SPI_ADVANCED_INIT_DEFAULT
Value:
{ \
eusartCsActiveLow, /* CS active low. */ \
eusartInvertIODisable, /* RX and TX signal active High. */ \
true, /* AutoCS enabled. */ \
false, /* Data is sent with the least significant bit first. */ \
0u, /* CS setup time is 0 baud cycles */ \
0u, /* CS hold time is 0 baud cycles */ \
0u, /* Inter-frame time is 0 baud cycles */ \
false, /* AutoTX disabled. */ \
0x0000, /* Default transmitted data is 0. */ \
false, /* No DMA wake up on reception. */ \
false, /* Do not use PRS signal as RX signal. */ \
(EUSART_PrsChannel_TypeDef) 0u, /* EUSART RX tied to prs channel 0. */ \
false, /* Do not use PRS signal as SCLK signal. */ \
(EUSART_PrsChannel_TypeDef) 1u, /* EUSART SCLCK tied to prs channel 1. */ \
eusartRxFiFoWatermark1Frame, /* RXFL status/IF set when RX FIFO has at least one frame in it */ \
eusartTxFiFoWatermark1Frame, /* TXFL status/IF set when TX FIFO has space for at least one more frame */ \
true, /* The first byte sent by the slave won't be the default value if a byte is made available \
after chip select is asserted. */ \
0x04u, /* Setup window before the sampling edge of SCLK at word-boundary to avoid force load error. */ \
}

Default advanced configuration for EUSART initialization structure in SPI mode with high-frequency clock.


EUSART_SPI_MASTER_INIT_DEFAULT_HF#

#define EUSART_SPI_MASTER_INIT_DEFAULT_HF
Value:
{ \
eusartEnable, /* Enable RX/TX when initialization completed. */ \
0, /* Use current configured reference clock for configuring baud rate.*/ \
10000000, /* 10 Mbits/s. */ \
eusartDataBits8, /* 8 data bits. */ \
true, /* Master mode enabled. */ \
eusartClockMode0, /* Clock idle low, sample on rising edge. */ \
eusartLoopbackDisable, /* Loop back disabled. */ \
NULL, /* Default advanced settings. */ \
}

Default configuration for EUSART initialization structure in SPI master mode with high-frequency clock.


EUSART_SPI_SLAVE_INIT_DEFAULT_HF#

#define EUSART_SPI_SLAVE_INIT_DEFAULT_HF
Value:
{ \
eusartEnable, /* Enable RX/TX when initialization completed. */ \
0, /* Use current configured reference clock for configuring baud rate.*/ \
10000000, /* 10 Mbits/s. */ \
eusartDataBits8, /* 8 data bits. */ \
false, /* Master mode enabled. */ \
eusartClockMode0, /* Clock idle low, sample on rising edge. */ \
eusartLoopbackDisable, /* Loop back disabled. */ \
NULL, /* Default advanced settings. */ \
}

Default configuration for EUSART initialization structure in SPI slave mode with high-frequency clock.


EUSART_ADVANCED_DALI_INIT_DEFAULT#

#define EUSART_ADVANCED_DALI_INIT_DEFAULT
Value:
{ \
eusartHwFlowControlNone, /* Flow control disabled. */ \
false, /* Collision detection disabled. */ \
true, /* Data is sent with the most significant bit first. */ \
eusartInvertIODisable, /* RX and TX signal active high. */ \
false, /* No DMA wake up on reception. */ \
false, /* No DMA wake up on transmission. */ \
false, /* Halt DMA on error disabled. */ \
EUSART_DEFAULT_START_FRAME, /* No start frame. */ \
false, /* TX auto tristate disabled. */ \
false, /* Do not use PRS signal as RX signal.*/ \
(EUSART_PrsChannel_TypeDef) 0u, /* EUSART RX connected to prs channel 0. */ \
false, /* Multiprocessor mode disabled. */ \
false, /* Multiprocessor address bit : 0.*/ \
eusartAutoTxDelayNone, /* Frames are transmitted immediately */ \
eusartRxFiFoWatermark1Frame, /* RXFL status/IF set when RX FIFO has at least one frame in it */ \
eusartTxFiFoWatermark1Frame, /* TXFL status/IF set when TX FIFO has space for at least one more frame */ \
}

Default configuration for EUSART initialization structure in DALI mode with high-frequency clock.

Default configuration for EUSART advanced initialization structure.


EUSART_UART_DALI_INIT_DEFAULT_HF#

#define EUSART_UART_DALI_INIT_DEFAULT_HF
Value:
{ \
eusartEnable, /* Enable RX/TX when initialization completed. */ \
0, /* Use current configured reference clock for configuring baud rate.*/ \
1200, /* 1200 bits/s. */ \
eusartOVS16, /* Oversampling x16. */ \
eusartDataBits8, /* 8 data bits. */ \
eusartNoParity, /* No parity. */ \
eusartStopbits1, /* 1 stop bit. */ \
eusartMajorityVoteEnable, /* Majority vote enabled. */ \
eusartLoopbackDisable, /* Loop back disabled. */ \
NULL, /* Default advanced settings. */ \
}

Default configuration for EUSART initialization structure in DALI mode with high-frequency clock.


EUSART_UART_DALI_INIT_DEFAULT_LF#

#define EUSART_UART_DALI_INIT_DEFAULT_LF
Value:
{ \
eusartEnable, /* Enable RX/TX when initialization completed. */ \
0, /* Use current configured reference clock for configuring baud rate.*/ \
1200, /* 1200 bits/s. */ \
eusartOVS0, /* Oversampling disabled. */ \
eusartDataBits8, /* 8 data bits. */ \
eusartNoParity, /* No parity. */ \
eusartStopbits1, /* 1 stop bit. */ \
eusartMajorityVoteDisable, /* Majority vote enabled. */ \
eusartLoopbackDisable, /* Loop back disabled. */ \
NULL, /* Default advanced settings. */ \
}

Default configuration for EUSART initialization structure in DALI mode with low-frequency clock.


EUSART_DALI_INIT_DEFAULT_HF#

#define EUSART_DALI_INIT_DEFAULT_HF
Value:
{ \
EUSART_UART_DALI_INIT_DEFAULT_HF, \
false, /* Disable DALI low frequency mode. */ \
eusartDaliTxDataBits16, /* TX 16 data bits. */ \
eusartDaliRxDataBits8, /* RX 8 data bits. */ \
} \

Default configuration for EUSART initialization structure in DALI mode with high-frequency clock.


EUSART_DALI_INIT_DEFAULT_LF#

#define EUSART_DALI_INIT_DEFAULT_LF
Value:
{ \
EUSART_UART_DALI_INIT_DEFAULT_LF, \
true, /* Enable DALI low frequency mode. */ \
eusartDaliTxDataBits16, /* TX 16 data bits. */ \
eusartDaliRxDataBits8, /* RX 8 data bits. */ \
} \

Default configuration for EUSART initialization structure in DALI mode with low-frequency clock.