SYSTEM - System Utils#

System API.

This module contains functions to read information such as RAM and Flash size, device unique ID, chip revision, family, and part number from DEVINFO and SCB blocks. Functions to configure and read status from FPU are available for compatible devices.

Modules#

SYSTEM_ChipRevision_TypeDef

SYSTEM_CalAddrVal_TypeDef

Enumerations#

enum
systemPartFamilyFlex25 = DEVINFO_PART_FAMILY_FG | (25 << _DEVINFO_PART_FAMILYNUM_SHIFT)
systemPartFamilyUnknown = 0xFF
}

Family identifiers.

enum
fpuAccessDenied = (0x0 << 20)
fpuAccessPrivilegedOnly = (0x5 << 20)
fpuAccessReserved = (0xA << 20)
fpuAccessFull = (0xF << 20)
}

Floating point co-processor access modes.

enum
securityCapabilityUnknown
securityCapabilityNA
securityCapabilityBasic
securityCapabilityRoT
securityCapabilitySE
securityCapabilityVault
}

Family security capability.

Functions#

void
SYSTEM_ChipRevisionGet(SYSTEM_ChipRevision_TypeDef *rev)

Get a chip major/minor revision.

Get the MCU family identifier.

uint8_t

Get DEVINFO revision.

void
SYSTEM_FpuAccessModeSet(SYSTEM_FpuAccess_TypeDef accessMode)

Set floating point co-processor (FPU) access mode.

bool
SYSTEM_GetCalibrationValue(volatile uint32_t *regAddress)

Get a factory calibration value for a given peripheral register.

uint64_t

Get the unique number for this device.

uint8_t

Get the production revision for this part.

uint32_t

Get the SRAM Base Address.

uint16_t

Get the SRAM size (in KB).

uint16_t

Get the flash size (in KB).

uint32_t

Get the flash page size in bytes.

uint16_t

Get the MCU part number.

uint8_t

Get the calibration temperature (in degrees Celsius).

Enumeration Documentation#

SYSTEM_PartFamily_TypeDef#

SYSTEM_PartFamily_TypeDef

Family identifiers.

Enumerator
systemPartFamilyFlex25

EFR32 Flex Gecko Series 2 Config 5 Value Device Family.

systemPartFamilyUnknown

Unknown Device Family.


SYSTEM_FpuAccess_TypeDef#

SYSTEM_FpuAccess_TypeDef

Floating point co-processor access modes.

Enumerator
fpuAccessDenied

Access denied, any attempted access generates a NOCP UsageFault.

fpuAccessPrivilegedOnly

Privileged access only, an unprivileged access generates a NOCP UsageFault.

fpuAccessReserved

Reserved.

fpuAccessFull

Full access.


SYSTEM_SecurityCapability_TypeDef#

SYSTEM_SecurityCapability_TypeDef

Family security capability.

Enumerator
securityCapabilityUnknown

Unknown security capability.

securityCapabilityNA

Security capability not applicable.

securityCapabilityBasic

Basic security capability.

securityCapabilityRoT

Root of Trust security capability.

securityCapabilitySE

Secure Element security capability.

securityCapabilityVault

Secure Vault security capability.


Function Documentation#

SYSTEM_ChipRevisionGet#

void SYSTEM_ChipRevisionGet (SYSTEM_ChipRevision_TypeDef * rev)

Get a chip major/minor revision.

Parameters
TypeDirectionArgument NameDescription
SYSTEM_ChipRevision_TypeDef *[out]rev

A location to place the chip revision information.


SYSTEM_GetFamily#

SYSTEM_PartFamily_TypeDef SYSTEM_GetFamily (void )

Get the MCU family identifier.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • This function retrieves family ID by reading the chip's device info structure in flash memory. Users can retrieve family ID directly by reading DEVINFO->PART item and decode with mask and shift #defines defined in <part_family>_devinfo.h (refer to code below for details).

Returns

  • Family identifier of MCU.


SYSTEM_GetDevinfoRev#

uint8_t SYSTEM_GetDevinfoRev (void )

Get DEVINFO revision.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Revision of the DEVINFO contents.


SYSTEM_FpuAccessModeSet#

void SYSTEM_FpuAccessModeSet (SYSTEM_FpuAccess_TypeDef accessMode)

Set floating point co-processor (FPU) access mode.

Parameters
TypeDirectionArgument NameDescription
SYSTEM_FpuAccess_TypeDef[in]accessMode

Floating point co-processor access mode. See SYSTEM_FpuAccess_TypeDef for details.


SYSTEM_GetCalibrationValue#

bool SYSTEM_GetCalibrationValue (volatile uint32_t * regAddress)

Get a factory calibration value for a given peripheral register.

Parameters
TypeDirectionArgument NameDescription
volatile uint32_t *[in]regAddress

The peripheral calibration register address to get a calibration value for. If the calibration value is found, this register is updated with the calibration value.

Returns

  • True if a calibration value exists, false otherwise.


SYSTEM_GetSecurityCapability#

SYSTEM_SecurityCapability_TypeDef SYSTEM_GetSecurityCapability (void )

Get family security capability.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • This function retrieves the family security capability based on the device number. The device number is one letter and 3 digits: DEVICENUMBER = (alpha-'A')*1000 + numeric. i.e. 0d = "A000"; 1123d = "B123". The security capabilities are represented by SYSTEM_SecurityCapability_TypeDef.

Returns

  • Security capability of MCU.


SYSTEM_GetUnique#

uint64_t SYSTEM_GetUnique (void )

Get the unique number for this device.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Unique number for this device.


SYSTEM_GetProdRev#

uint8_t SYSTEM_GetProdRev (void )

Get the production revision for this part.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Production revision for this part.


SYSTEM_GetSRAMBaseAddress#

uint32_t SYSTEM_GetSRAMBaseAddress (void )

Get the SRAM Base Address.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • This function is used to retrieve the base address of the SRAM.

Returns

  • Base address SRAM (32-bit unsigned integer).


SYSTEM_GetSRAMSize#

uint16_t SYSTEM_GetSRAMSize (void )

Get the SRAM size (in KB).

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • This function retrieves SRAM size by reading the chip device info structure. If your binary is made for one specific device only, use SRAM_SIZE instead.

Returns

  • Size of internal SRAM (in KB).


SYSTEM_GetFlashSize#

uint16_t SYSTEM_GetFlashSize (void )

Get the flash size (in KB).

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • This function retrieves flash size by reading the chip device info structure. If your binary is made for one specific device only, use FLASH_SIZE instead.

Returns

  • Size of internal flash (in KB).


SYSTEM_GetFlashPageSize#

uint32_t SYSTEM_GetFlashPageSize (void )

Get the flash page size in bytes.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • This function retrieves flash page size by reading the chip device info structure. If your binary is made for one specific device only, use FLASH_PAGE_SIZE instead.

Returns

  • Page size of internal flash in bytes.


SYSTEM_GetPartNumber#

uint16_t SYSTEM_GetPartNumber (void )

Get the MCU part number.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • The part number of MCU.


SYSTEM_GetCalibrationTemperature#

uint8_t SYSTEM_GetCalibrationTemperature (void )

Get the calibration temperature (in degrees Celsius).

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Calibration temperature in Celsius.