Cipher#
Symmetric encryption, AEAD and MAC.
API for performing symmetric encryption, Authenticated Encryption and Additional Data (AEAD) operations, and computing Message Authentication Codes (MACs) using the Secure Engine.
Modules#
sl_se_cmac_multipart_context_t
Enumerations#
Functions#
AES-ECB block encryption/decryption.
AES-CBC buffer encryption/decryption.
AES-CFB128 buffer encryption/decryption.
AES-CFB8 buffer encryption/decryption.
AES-CTR buffer encryption/decryption.
AES-CCM buffer encryption.
AES-CCM buffer decryption.
Prepare a CCM streaming command context object.
This function feeds an input buffer into an ongoing CCM computation.
Finish a CCM streaming operation and return the resulting CCM tag.
This function performs GCM encryption or decryption of a buffer.
This function performs a GCM authenticated decryption of a buffer.
This function calculates the full generic CMAC on the input buffer with the provided key.
Prepare a CMAC streaming command context object.
This function feeds an input buffer into an ongoing CMAC computation.
Finish a CMAC streaming operation and return the resulting CMAC tag.
Prepare a GCM streaming command context object.
This function feeds an input buffer into an ongoing GCM computation.
Finish a GCM streaming operation and return the resulting GCM tag.
Compute a HMAC on a full message.
ChaCha20 buffer encryption/decryption, as defined by RFC8439 section 2.4.
ChaCha20-Poly1305 authenticated encryption with additional data, as defined by RFC8439 section 2.8.
ChaCha20-Poly1305 authenticated decryption with additional data, as defined by RFC8439 section 2.8.
Generate a Poly1305 MAC (message authentication code) for a given message using an ephemeral key derived using ChaCha20.
Macros#
Initial values for CMAC streaming context struct sl_se_cmac_streaming_context_t.
Initial values for AES-GCM streaming context struct sl_se_gcm_streaming_context_t.
Block size for the AES.
Enumeration Documentation#
sl_se_cipher_operation_t#
sl_se_cipher_operation_t
Cipher operation types.
| Enumerator | |
|---|---|
| SL_SE_ENCRYPT | |
| SL_SE_DECRYPT | |
Function Documentation#
sl_se_aes_crypt_ecb#
sl_status_t sl_se_aes_crypt_ecb (sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, sl_se_cipher_operation_t mode, size_t length, const unsigned char * input, unsigned char * output)
AES-ECB block encryption/decryption.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure.  | 
| sl_se_cipher_operation_t | [in] | mode | Crypto operation type (encryption or decryption).  | 
| size_t | [in] | length | Length of the input data.  | 
| const unsigned char * | [in] | input | Buffer holding the input data.  | 
| unsigned char * | [out] | output | Buffer holding the output data.  | 
Returns
Status code, sl_status.h.
sl_se_aes_crypt_cbc#
sl_status_t sl_se_aes_crypt_cbc (sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, sl_se_cipher_operation_t mode, size_t length, unsigned char iv, const unsigned char * input, unsigned char * output)
AES-CBC buffer encryption/decryption.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure.  | 
| sl_se_cipher_operation_t | [in] | mode | Crypto operation type (encryption or decryption).  | 
| size_t | [in] | length | Length of the input data.  | 
| unsigned char | [inout] | iv | Initialization vector (updated after use).  | 
| const unsigned char * | [in] | input | Buffer holding the input data.  | 
| unsigned char * | [out] | output | Buffer holding the output data.  | 
Note
Length should be a multiple of the block size (16 bytes).
Returns
Status code, sl_status.h.
sl_se_aes_crypt_cfb128#
sl_status_t sl_se_aes_crypt_cfb128 (sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, sl_se_cipher_operation_t mode, size_t length, uint32_t * iv_off, unsigned char iv, const unsigned char * input, unsigned char * output)
AES-CFB128 buffer encryption/decryption.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure.  | 
| sl_se_cipher_operation_t | [in] | mode | Crypto operation type (encryption or decryption).  | 
| size_t | [in] | length | Length of the input data.  | 
| uint32_t * | [inout] | iv_off | Offset in IV (updated after use).  | 
| unsigned char | [inout] | iv | Initialization vector (updated after use).  | 
| const unsigned char * | [in] | input | Buffer holding the input data.  | 
| unsigned char * | [out] | output | Buffer holding the output data.  | 
Returns
Status code, sl_status.h.
sl_se_aes_crypt_cfb8#
sl_status_t sl_se_aes_crypt_cfb8 (sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, sl_se_cipher_operation_t mode, size_t length, unsigned char iv, const unsigned char * input, unsigned char * output)
AES-CFB8 buffer encryption/decryption.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure.  | 
| sl_se_cipher_operation_t | [in] | mode | Crypto operation type (encryption or decryption).  | 
| size_t | [in] | length | Length of the input data.  | 
| unsigned char | [inout] | iv | Initialization vector (updated after use).  | 
| const unsigned char * | [in] | input | Buffer holding the input data.  | 
| unsigned char * | [out] | output | Buffer holding the output data.  | 
Returns
Status code, sl_status.h.
sl_se_aes_crypt_ctr#
sl_status_t sl_se_aes_crypt_ctr (sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, size_t length, uint32_t * nc_off, unsigned char nonce_counter, unsigned char stream_block, const unsigned char * input, unsigned char * output)
AES-CTR buffer encryption/decryption.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure.  | 
| size_t | [in] | length | Length of the input data.  | 
| uint32_t * | [in] | nc_off | The offset in the current stream_block (for resuming within current cipher stream). The offset pointer to should be 0 at the start of a stream.  | 
| unsigned char | [inout] | nonce_counter | The 128-bit nonce and counter.  | 
| unsigned char | [inout] | stream_block | The saved stream-block for resuming (updated after use).  | 
| const unsigned char * | [in] | input | Buffer holding the input data.  | 
| unsigned char * | [out] | output | Buffer holding the output data.  | 
Warnings
Avoid passing in the same buffer for nonce_counter and stream_block as the incrementation operation of nonce_counter can lead to corruption of the ciphertext
Returns
Status code, sl_status.h.
sl_se_ccm_encrypt_and_tag#
sl_status_t sl_se_ccm_encrypt_and_tag (sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, size_t length, const unsigned char * iv, size_t iv_len, const unsigned char * add, size_t add_len, const unsigned char * input, unsigned char * output, unsigned char * tag, size_t tag_len)
AES-CCM buffer encryption.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure.  | 
| size_t | [in] | length | The length of the input data in Bytes.  | 
| const unsigned char * | [in] | iv | Initialization vector (nonce).  | 
| size_t | [in] | iv_len | The length of the IV in Bytes: 7, 8, 9, 10, 11, 12, or 13.  | 
| const unsigned char * | [in] | add | The additional data field.  | 
| size_t | [in] | add_len | The length of additional data in Bytes.  | 
| const unsigned char * | [in] | input | The buffer holding the input data.  | 
| unsigned char * | [out] | output | The buffer holding the output data. Must be at least   | 
| unsigned char * | [inout] | tag | The buffer holding the tag.  | 
| size_t | [in] | tag_len | The length of the tag to generate in Bytes: 4, 6, 8, 10, 12, 14 or 16.  | 
Returns
Status code, sl_status.h.
sl_se_ccm_auth_decrypt#
sl_status_t sl_se_ccm_auth_decrypt (sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, size_t length, const unsigned char * iv, size_t iv_len, const unsigned char * add, size_t add_len, const unsigned char * input, unsigned char * output, const unsigned char * tag, size_t tag_len)
AES-CCM buffer decryption.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure.  | 
| size_t | [in] | length | The length of the input data in Bytes.  | 
| const unsigned char * | [in] | iv | Initialization vector.  | 
| size_t | [in] | iv_len | The length of the IV in Bytes: 7, 8, 9, 10, 11, 12, or 13.  | 
| const unsigned char * | [in] | add | The additional data field.  | 
| size_t | [in] | add_len | The length of additional data in Bytes.  | 
| const unsigned char * | [in] | input | The buffer holding the input data.  | 
| unsigned char * | [out] | output | The buffer holding the output data. Must be at least   | 
| const unsigned char * | [in] | tag | The buffer holding the tag.  | 
| size_t | [in] | tag_len | The length of the tag in Bytes. Must be 4, 6, 8, 10, 12, 14 or 16.  | 
Returns
Status code, sl_status.h.
sl_se_ccm_multipart_starts#
sl_status_t sl_se_ccm_multipart_starts (sl_se_ccm_multipart_context_t * ccm_ctx, sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, sl_se_cipher_operation_t mode, uint32_t total_message_length, const uint8_t * iv, size_t iv_len, const uint8_t * add, size_t add_len, size_t tag_len)
Prepare a CCM streaming command context object.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_ccm_multipart_context_t * | [in] | ccm_ctx | Pointer to a CCM streaming context object.  | 
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to a SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure.  | 
| sl_se_cipher_operation_t | [in] | mode | The operation to perform: SL_SE_ENCRYPT or SL_SE_DECRYPT.  | 
| uint32_t | [in] | total_message_length | The total length of the text to encrypt/decrypt  | 
| const uint8_t * | [in] | iv | The initialization vector (commonly referred to as nonce for CCM).  | 
| size_t | [in] | iv_len | The length of the IV.  | 
| const uint8_t * | [in] | add | The buffer holding the additional data.  | 
| size_t | [in] | add_len | The length of the additional data.  | 
| size_t | [in] | tag_len | Encryption: The length of the tag to generate. Must be 0, 4, 6, 8, 10, 12, 14 or 16. Decryption: The length of the tag to authenticate. Must be 0, 4, 6, 8, 10, 12, 14 or 16.  | 
Prepare a CCM streaming command context object to be used in subsequent CCM streaming function calls.
Returns
Status code, sl_status.h.
sl_se_ccm_multipart_update#
sl_status_t sl_se_ccm_multipart_update (sl_se_ccm_multipart_context_t * ccm_ctx, sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, size_t length, const uint8_t * input, uint8_t * output, size_t * output_length)
This function feeds an input buffer into an ongoing CCM computation.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_ccm_multipart_context_t * | [in] | ccm_ctx | Pointer to a CCM streaming context object.  | 
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to a SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure.  | 
| size_t | [in] | length | The length of the input data. This must be a multiple of 16 except in the last call before sl_se_ccm_multipart_finish().  | 
| const uint8_t * | [in] | input | Buffer holding the input data, must be at least   | 
| uint8_t * | [out] | output | Buffer for holding the output data, must be at least   | 
| size_t * | [out] | output_length | Length of data that has been encrypted/decrypted.  | 
It is called between sl_se_ccm_multipart_starts() and sl_se_ccm_multipart_finish(). Can be called repeatedly.
Returns
Status code, sl_status.h.
sl_se_ccm_multipart_finish#
sl_status_t sl_se_ccm_multipart_finish (sl_se_ccm_multipart_context_t * ccm_ctx, sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, uint8_t * tag, uint8_t tag_size, uint8_t * output, uint8_t output_size, uint8_t * output_length)
Finish a CCM streaming operation and return the resulting CCM tag.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_ccm_multipart_context_t * | [in] | ccm_ctx | Pointer to a CCM streaming context object.  | 
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure.  | 
| uint8_t * | [inout] | tag | Encryption: The buffer for holding the tag. Decryption: The tag to authenticate.  | 
| uint8_t | [in] | tag_size | The size of the tag buffer. Must be equal or greater to the length of the expected tag.  | 
| uint8_t * | [out] | output | Buffer for holding the output data.  | 
| uint8_t | [in] | output_size | Output buffer size. Must be equal or greater to the stored data from sl_se_ccm_multipart_update (maximum 16 bytes).  | 
| uint8_t * | [out] | output_length | Length of data that has been encrypted/decrypted.  | 
It is called after sl_se_ccm_multipart_update().
Returns
Returns SL_SE_INVALID_SIGNATURE if authentication step fails. Status code, sl_status.h.
sl_se_gcm_crypt_and_tag#
sl_status_t sl_se_gcm_crypt_and_tag (sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, sl_se_cipher_operation_t mode, size_t length, const unsigned char * iv, size_t iv_len, const unsigned char * add, size_t add_len, const unsigned char * input, unsigned char * output, size_t tag_len, unsigned char * tag)
This function performs GCM encryption or decryption of a buffer.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure.  | 
| sl_se_cipher_operation_t | [in] | mode | Crypto operation type (encryption or decryption). 
  | 
| size_t | [in] | length | The length of the input data, which is equal to the length of the output data.  | 
| const unsigned char * | [in] | iv | The initialization vector.  | 
| size_t | [in] | iv_len | The length of the iv. Must be 12 bytes.  | 
| const unsigned char * | [in] | add | The buffer holding the additional data.  | 
| size_t | [in] | add_len | The length of the additional data in bytes.  | 
| const unsigned char * | [in] | input | The buffer holding the input data. Its size is length bytes.  | 
| unsigned char * | [out] | output | The buffer for holding the output data. It must have room for length bytes.  | 
| size_t | [in] | tag_len | The length of the tag to generate (in bytes).  | 
| unsigned char * | [out] | tag | The buffer for holding the tag.  | 
Note
For encryption, the output buffer can be the same as the input buffer. For decryption, the output buffer cannot be the same as input buffer. If the buffers overlap, the output buffer must trail at least 8 bytes behind the input buffer.
Warnings
When this function performs a decryption, it outputs the authentication tag and does not verify that the data is authentic. You should use this function to perform encryption only. For decryption, use sl_se_gcm_auth_decrypt() instead.
Returns
SL_STATUS_OK when the command was executed successfully, otherwise an appropriate error code (sl_status.h).
sl_se_gcm_auth_decrypt#
sl_status_t sl_se_gcm_auth_decrypt (sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, size_t length, const unsigned char * iv, size_t iv_len, const unsigned char * add, size_t add_len, const unsigned char * input, unsigned char * output, size_t tag_len, const unsigned char * tag)
This function performs a GCM authenticated decryption of a buffer.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure.  | 
| size_t | [in] | length | The length of the ciphertext to decrypt, which is also the length of the decrypted plaintext.  | 
| const unsigned char * | [in] | iv | The initialization vector.  | 
| size_t | [in] | iv_len | The length of the iv. Must be 12 bytes.  | 
| const unsigned char * | [in] | add | The buffer holding the additional data.  | 
| size_t | [in] | add_len | The length of the additional data in bytes.  | 
| const unsigned char * | [in] | input | The buffer holding the tag to verify.  | 
| unsigned char * | [in] | output | The length of the tag to verify (in bytes).  | 
| size_t | [in] | tag_len | The buffer holding the ciphertext. Its size is length bytes.  | 
| const unsigned char * | [out] | tag | The buffer for holding the decrypted plaintext. It must have room for length bytes.  | 
Note
The output buffer cannot be the same as input buffer. If the buffers overlap, the output buffer must trail at least 8 bytes behind the input buffer.
Returns
SL_STATUS_OK when the command was executed successfully, otherwise an appropriate error code (sl_status.h).
sl_se_cmac#
sl_status_t sl_se_cmac (sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, const unsigned char * input, size_t input_len, unsigned char * output)
This function calculates the full generic CMAC on the input buffer with the provided key.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure.  | 
| const unsigned char * | [in] | input | Buffer holding the input data, must be at least   | 
| size_t | [in] | input_len | The length of the input data in bytes.  | 
| unsigned char * | [out] | output | Buffer holding the 16-byte output data, must be at least 16 bytes wide.  | 
Returns
Status code, sl_status.h.
sl_se_cmac_multipart_starts#
sl_status_t sl_se_cmac_multipart_starts (sl_se_cmac_multipart_context_t * cmac_ctx, sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key)
Prepare a CMAC streaming command context object.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_cmac_multipart_context_t * | [in] | cmac_ctx | Pointer to a CMAC streaming context object.  | 
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure.  | 
Prepare a CMAC streaming command context object to be used in subsequent CMAC streaming function calls.
Returns
Status code, sl_status.h.
sl_se_cmac_multipart_update#
sl_status_t sl_se_cmac_multipart_update (sl_se_cmac_multipart_context_t * cmac_ctx, sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, const uint8_t * input, size_t input_len)
This function feeds an input buffer into an ongoing CMAC computation.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_cmac_multipart_context_t * | [inout] | cmac_ctx | Pointer to a CMAC streaming context object.  | 
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure.  | 
| const uint8_t * | [in] | input | Buffer holding the input data, must be at least   | 
| size_t | [in] | input_len | The length of the input data in bytes.  | 
It is called between sl_se_cmac_multipart_starts() and sl_se_cmac_multipart_finish(). Can be called repeatedly.
Returns
Status code, sl_status.h.
sl_se_cmac_multipart_finish#
sl_status_t sl_se_cmac_multipart_finish (sl_se_cmac_multipart_context_t * cmac_ctx, sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, uint8_t * output)
Finish a CMAC streaming operation and return the resulting CMAC tag.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_cmac_multipart_context_t * | [inout] | cmac_ctx | Pointer to a CMAC streaming context object.  | 
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure.  | 
| uint8_t * | [out] | output | Buffer holding the 16-byte CMAC tag, must be at least 16 bytes wide.  | 
It is called after sl_se_cmac_multipart_update().
Returns
Status code, sl_status.h.
sl_se_gcm_multipart_starts#
sl_status_t sl_se_gcm_multipart_starts (sl_se_gcm_multipart_context_t * gcm_ctx, sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, sl_se_cipher_operation_t mode, const uint8_t * iv, size_t iv_len, const uint8_t * add, size_t add_len)
Prepare a GCM streaming command context object.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_gcm_multipart_context_t * | [inout] | gcm_ctx | Pointer to a GCM streaming context object.  | 
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure.  | 
| sl_se_cipher_operation_t | [in] | mode | The operation to perform: SL_SE_ENCRYPT or SL_SE_DECRYPT.  | 
| const uint8_t * | [in] | iv | The initialization vector.  | 
| size_t | [in] | iv_len | The length of the IV.  | 
| const uint8_t * | [in] | add | The buffer holding the additional data, or NULL if   | 
| size_t | [in] | add_len | The length of the additional data. If 0,   | 
Prepare a GCM streaming command context object to be used in subsequent GCM streaming function calls.
Returns
Status code, sl_status.h.
sl_se_gcm_multipart_update#
sl_status_t sl_se_gcm_multipart_update (sl_se_gcm_multipart_context_t * gcm_ctx, sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, size_t length, const uint8_t * input, uint8_t * output, size_t * output_length)
This function feeds an input buffer into an ongoing GCM computation.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_gcm_multipart_context_t * | [inout] | gcm_ctx | Pointer to a GCM streaming context object.  | 
| sl_se_command_context_t * | [in] | cmd_ctx | The length of the input data.  | 
| const sl_se_key_descriptor_t * | [in] | key | Buffer holding the input data, must be at least   | 
| size_t | [out] | length | Buffer for holding the output data, must be at least   | 
| const uint8_t * | [out] | input | Length of data that has been encrypted/decrypted.  | 
| uint8_t * | N/A | output | |
| size_t * | N/A | output_length | 
It is called between sl_se_gcm_multipart_starts() and sl_se_gcm_multiapart_finish(). Can be called repeatedly.
Returns
Status code, sl_status.h.
sl_se_gcm_multipart_finish#
sl_status_t sl_se_gcm_multipart_finish (sl_se_gcm_multipart_context_t * gcm_ctx, sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, uint8_t * tag, uint8_t tag_length, uint8_t * output, uint8_t output_size, uint8_t * output_length)
Finish a GCM streaming operation and return the resulting GCM tag.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_gcm_multipart_context_t * | [inout] | gcm_ctx | Pointer to a GCM streaming context object.  | 
| sl_se_command_context_t * | [inout] | cmd_ctx | Encryption: The buffer for holding the tag. Decryption: The tag to authenticate.  | 
| const sl_se_key_descriptor_t * | [in] | key | Encryption: Length of the output tag. Decryption: Length of tag to verify  | 
| uint8_t * | [out] | tag | Buffer for holding the output data.  | 
| uint8_t | [in] | tag_length | Output buffer size. Must be equal or greater to the stored data from sl_se_gcm_multipart_update (stored data is maximum 16 bytes).  | 
| uint8_t * | [out] | output | Length of data that has been encrypted/decrypted.  | 
| uint8_t | N/A | output_size | |
| uint8_t * | N/A | output_length | 
It is called after sl_se_gcm_multipart_update().
Returns
Returns SL_SE_INVALID_SIGNATURE if authentication step fails. Status code, sl_status.h.
sl_se_hmac#
sl_status_t sl_se_hmac (sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, sl_se_hash_type_t hash_type, const uint8_t * message, size_t message_len, uint8_t * output, size_t output_len)
Compute a HMAC on a full message.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure specifying the key to use in the HMAC computation.  | 
| sl_se_hash_type_t | [in] | hash_type | Which hashing algorithm to use.  | 
| const uint8_t * | [in] | message | Pointer to the message buffer to compute the hash/digest from.  | 
| size_t | [in] | message_len | Number of bytes in message.  | 
| uint8_t * | [out] | output | Pointer to memory buffer to store the final HMAC output.  | 
| size_t | [in] | output_len | The length of the HMAC output memory buffer, must be at least the size of the corresponding hash type.  | 
This function computes a Keyed-Hashed Message Authentication Code (HMAC) for the given input message. HMAC can be used with any iterative cryptographic hash function, e.g., SHA-1 in combination with a secret shared key. The cryptographic strength of HMAC depends on the properties of the underlying hash function. For instance, if the algorithm is chosen to be SHA-256, it will generate a 32 bytes HMAC. This function supports SHA-1, SHA-224, SHA-256, SHA-384 and SHA-512. The key can be of any length. If the key is shorter than the block size of the hash function the SE will append zeros to the key so the key size matches the block size of the hash function. If the key is longer than the block size of the hash function the key will be hashed to produce a key digest, then append zeros so the resulting 'hashed' key size matches the block size of the hash function. In any case the minimal recommended key length is the digest size of the hash function.
Returns
Status code, sl_status.h.
sl_se_chacha20_crypt#
sl_status_t sl_se_chacha20_crypt (sl_se_command_context_t * cmd_ctx, sl_se_cipher_operation_t mode, const sl_se_key_descriptor_t * key, size_t length, const unsigned char initial_counter, const unsigned char nonce, const unsigned char * input, unsigned char * output)
ChaCha20 buffer encryption/decryption, as defined by RFC8439 section 2.4.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| sl_se_cipher_operation_t | [in] | mode | Crypto operation type (encryption or decryption).  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure.  | 
| size_t | [in] | length | Length of the input data.  | 
| const unsigned char | [in] | initial_counter | The initial counter value as defined in RFC8439 section 2.4.  | 
| const unsigned char | [in] | nonce | The nonce, also called initialisation vector, as defined in RFC8439 section 2.4.  | 
| const unsigned char * | [in] | input | Buffer holding the input data.  | 
| unsigned char * | [out] | output | Buffer holding the output data.  | 
Returns
Status code, sl_status.h.
sl_se_chacha20_poly1305_encrypt_and_tag#
sl_status_t sl_se_chacha20_poly1305_encrypt_and_tag (sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, size_t length, const unsigned char nonce, const unsigned char * add, size_t add_len, const unsigned char * input, unsigned char * output, unsigned char * tag)
ChaCha20-Poly1305 authenticated encryption with additional data, as defined by RFC8439 section 2.8.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure.  | 
| size_t | [in] | length | The length of the input data in bytes.  | 
| const unsigned char | [in] | nonce | The nonce, also called initialisation vector, as defined in RFC8439 section 2.8.  | 
| const unsigned char * | [in] | add | The buffer holding additional authenticated data. Can be NULL if   | 
| size_t | [in] | add_len | The length of the additional authenticated data in bytes.  | 
| const unsigned char * | [in] | input | The buffer holding the plaintext input.  | 
| unsigned char * | [out] | output | The buffer holding the ciphertext output. Can be NULL, in which case the generated ciphertext will be discarded. Must be at least   | 
| unsigned char * | [out] | tag | The buffer holding the tag. This function will produce a 128-bit tag, so this buffer must be at least 16 bytes wide. Can be NULL, in which case the generated tag will be discarded.  | 
Returns
Status code, sl_status.h.
sl_se_chacha20_poly1305_auth_decrypt#
sl_status_t sl_se_chacha20_poly1305_auth_decrypt (sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, size_t length, const unsigned char nonce, const unsigned char * add, size_t add_len, const unsigned char * input, unsigned char * output, const unsigned char tag)
ChaCha20-Poly1305 authenticated decryption with additional data, as defined by RFC8439 section 2.8.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure.  | 
| size_t | [in] | length | The length of the input data in Bytes.  | 
| const unsigned char | [in] | nonce | The nonce, also called initialisation vector, as defined in RFC8439 section 2.8.  | 
| const unsigned char * | [in] | add | The buffer holding additional authenticated data. Can be NULL if   | 
| size_t | [in] | add_len | The length of the additional authenticated data in bytes.  | 
| const unsigned char * | [in] | input | The buffer holding the ciphertext to decrypt. Can be NULL if   | 
| unsigned char * | [out] | output | The buffer holding the plaintext output. Can be NULL, in which case the decrypted plaintext will be discarded, or when   | 
| const unsigned char | [in] | tag | The buffer holding the tag to verify.  | 
Returns
Status code, sl_status.h.
sl_se_poly1305_genkey_tag#
sl_status_t sl_se_poly1305_genkey_tag (sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, size_t length, const unsigned char nonce, const unsigned char * input, unsigned char * tag)
Generate a Poly1305 MAC (message authentication code) for a given message using an ephemeral key derived using ChaCha20.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure containing a ChaCha20 key.  | 
| size_t | [in] | length | The length of the input data in Bytes.  | 
| const unsigned char | [in] | nonce | The nonce, also called initialisation vector, as defined in RFC8439 section 2.6.  | 
| const unsigned char * | [in] | input | The buffer holding the input data.  | 
| unsigned char * | [out] | tag | The buffer holding the tag. This function will produce a 128-bit tag, so this buffer must be at least 16 bytes wide.  | 
Note
This function first derives a Poly1305 key based on a ChaCha20 key and nonce, which are input to this function. The key derivation adheres to RFC8439 section 2.6. The derived key is then used to calculate a MAC of the input data, according to RFC8439 section 2.5.
Returns
Status code, sl_status.h.