LED Driver#
Generic LED Driver.
Introduction#
The LED driver is a platfom level software module that manages the control of various types of LEDs. There are currently two types of LEDs supported by the LED driver:
simple_rgbw_pwm_led
The common LED functions are called through the generic LED driver, while other functions specific to a certain type of LED are called directly through their own driver.
Configuration#
All LED instances are configured with an sl_led_t struct and a type specific context struct, and sometimes additional structs. There is also a typedef sl_led_state_t to get the state of an LED. These structs are automatically generated after an LED is set up using Simplicity Studio's wizard, along with a function definition for initializing all LEDs of that type. Specific setups for the various LED types are in the following sections.
Usage#
Once the LED structs are defined, the common LED functions can be called being passed an instance of sl_led_t, which will be redirected to calling the type specific version of that function. The common functions include the following:
These functions allow for initializing the LED, turning it on and off, toggling it, and getting the current on/off state of it. Other functions are called through the specific type of LED's API directly. The usages of the different types of LEDs are described in detail in the following sections.
rgbw_led_usage
Modules#
Typedefs#
LED state.
Functions#
Initialize the LED driver.
Turn on the LED.
Turn off the LED.
Toggle the LED.
Get the current state of the LED.
Macros#
LED state off.
LED state on.
Function Documentation#
sl_led_init#
sl_status_t sl_led_init (const sl_led_t * led_handle)
Initialize the LED driver.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_led_t * | [in] | led_handle | Pointer to instance of sl_led_t to initialize |
Call this function before any other LED function. Initializes the selected LED GPIO, mode, and polarity.
Returns
Status Code:
SL_STATUS_OK
sl_led_turn_on#
void sl_led_turn_on (const sl_led_t * led_handle)
Turn on the LED.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_led_t * | [in] | led_handle | Pointer to instance of sl_led_t to turn on |
sl_led_turn_off#
void sl_led_turn_off (const sl_led_t * led_handle)
Turn off the LED.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_led_t * | [in] | led_handle | Pointer to instance of sl_led_t to turn off |