TIMER - Timer/Counter#
Timer/Counter (TIMER) Peripheral API.
The timer module consists of three main parts:
General timer configuration and enable control.
Compare/capture control.
Dead time insertion control (may not be available for all timers).
Modules#
Enumerations#
Timer compare/capture mode.
Clock select.
Input capture edge select.
Input capture event control.
Input edge action.
Timer mode.
Compare/capture output action.
Prescaler.
PRS input type.
DT (Dead Time) Fault Actions.
PRS Output configuration.
Typedefs#
Peripheral Reflex System signal.
Functions#
Initialize TIMER.
Initialize the TIMER compare/capture channel.
Initialize the TIMER DTI unit.
Reset the TIMER to the same state that it was in after a hardware reset.
Wait for pending synchronization to finish.
Validate the TIMER register block pointer.
Check whether the TIMER is valid and supports Dead Timer Insertion (DTI).
Get the Max count of the timer.
Get compare/capture value for the compare/capture channel.
Get the buffered compare/capture value for compare/capture channel.
Set the compare value buffer for the compare/capture channel when operating in compare or PWM mode.
Set the compare value for compare/capture channel when operating in compare or PWM mode.
Get the TIMER counter value.
Set the TIMER counter value.
Start/stop TIMER.
Enable or disable DTI unit.
Get DTI fault source flags status.
Clear DTI fault source flags.
Clear one or more pending TIMER interrupts.
Disable one or more TIMER interrupts.
Enable one or more TIMER interrupts.
Get pending TIMER interrupt flags.
Get enabled and pending TIMER interrupt flags.
Set one or more pending TIMER interrupts from SW.
Set the top value buffer for the timer.
Get the top value setting for the timer.
Set the top value for timer.
Macros#
Default configuration for TIMER initialization structure.
Default configuration for TIMER compare/capture initialization structure.
Default configuration for TIMER DTI initialization structure.
Enumeration Documentation#
TIMER_CCMode_TypeDef#
TIMER_CCMode_TypeDef
Timer compare/capture mode.
| Enumerator | |
|---|---|
| timerCCModeOff | Channel turned off. |
| timerCCModeCapture | Input capture. |
| timerCCModeCompare | Output compare. |
| timerCCModePWM | Pulse-Width modulation. |
TIMER_ClkSel_TypeDef#
TIMER_ClkSel_TypeDef
Clock select.
| Enumerator | |
|---|---|
| timerClkSelHFPerClk | Prescaled EM01GRPA clock. |
| timerClkSelCC1 | Compare/Capture Channel 1 Input. |
| timerClkSelCascade | Cascaded clocked by underflow or overflow by lower numbered timer. |
TIMER_Edge_TypeDef#
TIMER_Edge_TypeDef
Input capture edge select.
| Enumerator | |
|---|---|
| timerEdgeRising | Rising edges detected. |
| timerEdgeFalling | Falling edges detected. |
| timerEdgeBoth | Both edges detected. |
| timerEdgeNone | No edge detection, leave signal as is. |
TIMER_Event_TypeDef#
TIMER_Event_TypeDef
Input capture event control.
| Enumerator | |
|---|---|
| timerEventEveryEdge | PRS output pulse, interrupt flag, and DMA request set on every capture. |
| timerEventEvery2ndEdge | PRS output pulse, interrupt flag, and DMA request set on every second capture. |
| timerEventRising | PRS output pulse, interrupt flag, and DMA request set on rising edge (if input capture edge = BOTH). |
| timerEventFalling | PRS output pulse, interrupt flag, and DMA request set on falling edge (if input capture edge = BOTH). |
TIMER_InputAction_TypeDef#
TIMER_InputAction_TypeDef
Input edge action.
| Enumerator | |
|---|---|
| timerInputActionNone | No action taken. |
| timerInputActionStart | Start counter without reload. |
| timerInputActionStop | Stop counter without reload. |
| timerInputActionReloadStart | Reload and start counter. |
TIMER_Mode_TypeDef#
TIMER_Mode_TypeDef
Timer mode.
| Enumerator | |
|---|---|
| timerModeUp | Up-counting. |
| timerModeDown | Down-counting. |
| timerModeUpDown | Up/down-counting. |
| timerModeQDec | Quadrature decoder. |
TIMER_OutputAction_TypeDef#
TIMER_OutputAction_TypeDef
Compare/capture output action.
| Enumerator | |
|---|---|
| timerOutputActionNone | No action. |
| timerOutputActionToggle | Toggle on event. |
| timerOutputActionClear | Clear on event. |
| timerOutputActionSet | Set on event. |
TIMER_Prescale_TypeDef#
TIMER_Prescale_TypeDef
Prescaler.
| Enumerator | |
|---|---|
| timerPrescale1 | Divide by 1. |
| timerPrescale2 | Divide by 2. |
| timerPrescale4 | Divide by 4. |
| timerPrescale8 | Divide by 8. |
| timerPrescale16 | Divide by 16. |
| timerPrescale32 | Divide by 32. |
| timerPrescale64 | Divide by 64. |
| timerPrescale128 | Divide by 128. |
| timerPrescale256 | Divide by 256. |
| timerPrescale512 | Divide by 512. |
| timerPrescale1024 | Divide by 1024. |
TIMER_PrsInput_TypeDef#
TIMER_PrsInput_TypeDef
PRS input type.
| Enumerator | |
|---|---|
| timerPrsInputNone | No PRS input. |
| timerPrsInputSync | Synchronous PRS selected. |
| timerPrsInputAsyncLevel | Asynchronous level PRS selected. |
| timerPrsInputAsyncPulse | Asynchronous pulse PRS selected. |
TIMER_DtiFaultAction_TypeDef#
TIMER_DtiFaultAction_TypeDef
DT (Dead Time) Fault Actions.
| Enumerator | |
|---|---|
| timerDtiFaultActionNone | No action on fault. |
| timerDtiFaultActionInactive | Set outputs inactive. |
| timerDtiFaultActionClear | Clear outputs. |
| timerDtiFaultActionTristate | Tristate outputs. |
TIMER_PrsOutput_t#
TIMER_PrsOutput_t
PRS Output configuration.
| Enumerator | |
|---|---|
| timerPrsOutputPulse | Pulse PRS output from a channel. |
| timerPrsOutputLevel | PRS output follows CC out level. |
| timerPrsOutputDefault | Default PRS output behavior. |
Typedef Documentation#
Function Documentation#
TIMER_Init#
void TIMER_Init (TIMER_TypeDef * timer, const TIMER_Init_TypeDef * init)
Initialize TIMER.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | A pointer to the TIMER peripheral register block. |
| const TIMER_Init_TypeDef * | [in] | init | A pointer to the TIMER initialization structure. |
Notice that the counter top must be configured separately with, for instance TIMER_TopSet(). In addition, compare/capture and dead-time insertion initialization must be initialized separately if used, which should probably be done prior to using this function if configuring the TIMER to start when initialization is completed.
TIMER_InitCC#
void TIMER_InitCC (TIMER_TypeDef * timer, unsigned int ch, const TIMER_InitCC_TypeDef * init)
Initialize the TIMER compare/capture channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | A pointer to the TIMER peripheral register block. |
| unsigned int | [in] | ch | A compare/capture channel to initialize for. |
| const TIMER_InitCC_TypeDef * | [in] | init | A pointer to the TIMER initialization structure. |
Notice that if operating the channel in compare mode, the CCV and CCVB register must be set separately, as required.
TIMER_InitDTI#
void TIMER_InitDTI (TIMER_TypeDef * timer, const TIMER_InitDTI_TypeDef * init)
Initialize the TIMER DTI unit.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | A pointer to the TIMER peripheral register block. |
| const TIMER_InitDTI_TypeDef * | [in] | init | A pointer to the TIMER DTI initialization structure. |
TIMER_Reset#
void TIMER_Reset (TIMER_TypeDef * timer)
Reset the TIMER to the same state that it was in after a hardware reset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | A pointer to the TIMER peripheral register block. |
Note
The ROUTE register is NOT reset by this function to allow for a centralized setup of this feature.
TIMER_SyncWait#
void TIMER_SyncWait (TIMER_TypeDef * timer)
Wait for pending synchronization to finish.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer |
TIMER_Valid#
bool TIMER_Valid (const TIMER_TypeDef * ref)
Validate the TIMER register block pointer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const TIMER_TypeDef * | [in] | ref | Pointer to the TIMER peripheral register block. |
Returns
True if ref points to a valid timer, false otherwise.
TIMER_SupportsDTI#
bool TIMER_SupportsDTI (const TIMER_TypeDef * ref)
Check whether the TIMER is valid and supports Dead Timer Insertion (DTI).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const TIMER_TypeDef * | [in] | ref | Pointer to the TIMER peripheral register block. |
Returns
True if ref points to a valid timer that supports DTI, false otherwise.
TIMER_MaxCount#
uint32_t TIMER_MaxCount (const TIMER_TypeDef * ref)
Get the Max count of the timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const TIMER_TypeDef * | [in] | ref | Pointer to the TIMER peripheral register block. |
Returns
The max count value of the timer. This is 0xFFFF for 16 bit timers and 0xFFFFFFFF for 32 bit timers.
TIMER_CaptureGet#
uint32_t TIMER_CaptureGet (TIMER_TypeDef * timer, unsigned int ch)
Get compare/capture value for the compare/capture channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | Pointer to the TIMER peripheral register block. |
| unsigned int | [in] | ch | Compare/capture channel to access. |
Returns
Current capture value.
TIMER_CaptureBufGet#
uint32_t TIMER_CaptureBufGet (TIMER_TypeDef * timer, unsigned int ch)
Get the buffered compare/capture value for compare/capture channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | Pointer to the TIMER peripheral register block. |
| unsigned int | [in] | ch | Compare/capture channel to access. |
Returns
Current buffered capture value.
TIMER_CompareBufSet#
void TIMER_CompareBufSet (TIMER_TypeDef * timer, unsigned int ch, uint32_t val)
Set the compare value buffer for the compare/capture channel when operating in compare or PWM mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | Pointer to the TIMER peripheral register block. |
| unsigned int | [in] | ch | Compare/capture channel to access. |
| uint32_t | [in] | val | Value to set in compare value buffer register. |
The compare value buffer holds the value which will be written to TIMERn_CCx_CCV on an update event if the buffer has been updated since the last event.
TIMER_CompareSet#
void TIMER_CompareSet (TIMER_TypeDef * timer, unsigned int ch, uint32_t val)
Set the compare value for compare/capture channel when operating in compare or PWM mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | Pointer to the TIMER peripheral register block. |
| unsigned int | [in] | ch | Compare/capture channel to access. |
| uint32_t | [in] | val | Value to set in compare value register. |
TIMER_CounterGet#
uint32_t TIMER_CounterGet (TIMER_TypeDef * timer)
Get the TIMER counter value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | Pointer to TIMER peripheral register block. |
Returns
Current TIMER counter value.
TIMER_CounterSet#
void TIMER_CounterSet (TIMER_TypeDef * timer, uint32_t val)
Set the TIMER counter value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | Pointer to the TIMER peripheral register block. |
| uint32_t | [in] | val | Value to set counter to. |
TIMER_Enable#
void TIMER_Enable (TIMER_TypeDef * timer, bool enable)
Start/stop TIMER.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | Pointer to the TIMER peripheral register block. |
| bool | [in] | enable | Set to true to enable counting; set to false otherwise. |
TIMER_EnableDTI#
void TIMER_EnableDTI (TIMER_TypeDef * timer, bool enable)
Enable or disable DTI unit.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | Pointer to the TIMER peripheral register block. |
| bool | [in] | enable | Set to true to enable DTI unit; set to false otherwise. |
TIMER_GetDTIFault#
uint32_t TIMER_GetDTIFault (TIMER_TypeDef * timer)
Get DTI fault source flags status.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | Pointer to the TIMER peripheral register block. |
Note
Event bits are not cleared by this function.
Returns
Status of the DTI fault source flags. Returns one or more valid DTI fault source flags (TIMER_DTFAULT_nnn) OR'ed together.
TIMER_ClearDTIFault#
void TIMER_ClearDTIFault (TIMER_TypeDef * timer, uint32_t flags)
Clear DTI fault source flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | Pointer to the TIMER peripheral register block. |
| uint32_t | [in] | flags | DTI fault source(s) to clear. Use one or more valid DTI fault source flags (TIMER_DTFAULT_nnn) OR'ed together. |
TIMER_IntClear#
void TIMER_IntClear (TIMER_TypeDef * timer, uint32_t flags)
Clear one or more pending TIMER interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | Pointer to the TIMER peripheral register block. |
| uint32_t | [in] | flags | Pending TIMER interrupt source(s) to clear. Use one or more valid interrupt flags for the TIMER module (TIMER_IF_nnn) OR'ed together. |
TIMER_IntDisable#
void TIMER_IntDisable (TIMER_TypeDef * timer, uint32_t flags)
Disable one or more TIMER interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | Pointer to the TIMER peripheral register block. |
| uint32_t | [in] | flags | TIMER interrupt source(s) to disable. Use one or more valid interrupt flags for the TIMER module (TIMER_IF_nnn) OR'ed together. |
TIMER_IntEnable#
void TIMER_IntEnable (TIMER_TypeDef * timer, uint32_t flags)
Enable one or more TIMER interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | Pointer to the TIMER peripheral register block. |
| uint32_t | [in] | flags | TIMER interrupt source(s) to enable. Use one or more valid interrupt flags for the TIMER module (TIMER_IF_nnn) OR'ed together. |
Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using TIMER_IntClear() prior to enabling the interrupt.
TIMER_IntGet#
uint32_t TIMER_IntGet (TIMER_TypeDef * timer)
Get pending TIMER interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | Pointer to the TIMER peripheral register block. |
Note
Event bits are not cleared by this function.
Returns
TIMER interrupt source(s) pending. Returns one or more valid interrupt flags for the TIMER module (TIMER_IF_nnn) OR'ed together.
TIMER_IntGetEnabled#
uint32_t TIMER_IntGetEnabled (TIMER_TypeDef * timer)
Get enabled and pending TIMER interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | Pointer to the TIMER peripheral register block. |
Useful for handling more interrupt sources in the same interrupt handler.
Note
Interrupt flags are not cleared by this function.
Returns
Pending and enabled TIMER interrupt sources. The return value is the bitwise AND combination of
the OR combination of enabled interrupt sources in TIMERx_IEN_nnn register (TIMERx_IEN_nnn) and
the OR combination of valid interrupt flags of the TIMER module (TIMERx_IF_nnn).
TIMER_IntSet#
void TIMER_IntSet (TIMER_TypeDef * timer, uint32_t flags)
Set one or more pending TIMER interrupts from SW.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | Pointer to the TIMER peripheral register block. |
| uint32_t | [in] | flags | TIMER interrupt source(s) to set to pending. Use one or more valid interrupt flags for the TIMER module (TIMER_IF_nnn) OR'ed together. |
TIMER_TopBufSet#
void TIMER_TopBufSet (TIMER_TypeDef * timer, uint32_t val)
Set the top value buffer for the timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | Pointer to the TIMER peripheral register block. |
| uint32_t | [in] | val | Value to set in top value buffer register. |
When top value buffer register is updated, value is loaded into top value register at the next wrap around. This feature is useful in order to update top value safely when timer is running.
TIMER_TopGet#
uint32_t TIMER_TopGet (TIMER_TypeDef * timer)
Get the top value setting for the timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | Pointer to the TIMER peripheral register block. |
Returns
Current top value.
TIMER_TopSet#
void TIMER_TopSet (TIMER_TypeDef * timer, uint32_t val)
Set the top value for timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TIMER_TypeDef * | [in] | timer | Pointer to the TIMER peripheral register block. |
| uint32_t | [in] | val | Value to set in top value register. |