SegmentLcd#
Modules#
Functions#
Defines prototype for all segments in display.
Enable all segments.
Turn all segments on alpha characters in display off.
Segment LCD Initialization routine for EFM32 STK display.
Write number on numeric part on Segment LCD display.
Write temperature on Segment LCD display.
Turn all segments on numeric digits in display off.
Light up or shut off various symbols on Segment LCD.
Write hexadecimal number on numeric part on Segment LCD display.
Function Documentation#
sl_segment_lcd_all_off#
void sl_segment_lcd_all_off (void )
Defines prototype for all segments in display.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
ENUMS ************************************
Defines segment lcd block modes FUNCTIONS ***********************************
Disable all segments
sl_segment_lcd_all_on#
void sl_segment_lcd_all_on (void )
Enable all segments.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
sl_segment_lcd_disable#
void sl_segment_lcd_disable (void )
Turn all segments on alpha characters in display off.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
Disables LCD controller
sl_segment_lcd_init#
void sl_segment_lcd_init (bool use_boost)
Segment LCD Initialization routine for EFM32 STK display.
Type | Direction | Argument Name | Description |
---|---|---|---|
bool | [in] | use_boost | Set to use voltage boost |
sl_segment_lcd_number#
void sl_segment_lcd_number (int value)
Write number on numeric part on Segment LCD display.
Type | Direction | Argument Name | Description |
---|---|---|---|
int | [in] | value | Numeric value to put on display, in range -999 to +9999 |
sl_segment_lcd_temp_display#
void sl_segment_lcd_temp_display (int32_t temp_data)
Write temperature on Segment LCD display.
Type | Direction | Argument Name | Description |
---|---|---|---|
int32_t | [in] | temp_data | value to put on display, in range -40000 to +125000 |
The following function are written to handle the cases when the sensor measures negative temperature values, three digit temperature values, and temperature values from 0-100 degrees Celsius. Keep in mind, the Si7021 part has an operating temperature range of -40 to +125 degrees Celsius. The temp_data variable stores a temperature read by the Si7021 that is multiplied by a factor of 1000. In order to display the temperature correctly in the negative and three digit cases, the temp_data variable must be divided by 10 to remove one digit from the variable. Without this, the value of temp_data passed to the SegmentLCD_Number() function may be higher than the max value the Segment LCD could display.
sl_segment_lcd_number_off#
void sl_segment_lcd_number_off (void )
Turn all segments on numeric digits in display off.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
sl_segment_lcd_symbol#
void sl_segment_lcd_symbol (sl_segment_lcd_symbol_t s, int on)
Light up or shut off various symbols on Segment LCD.
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_segment_lcd_symbol_t | [in] | s | Which symbol to turn on or off |
int | [in] | on | Zero is off, non-zero is on |
sl_segment_lcd_unsigned_hex#
void sl_segment_lcd_unsigned_hex (uint32_t value)
Write hexadecimal number on numeric part on Segment LCD display.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint32_t | [in] | value | Numeric value to put on display |