A BUTTON instance.

BUTTON Instance structure.

Public Attributes#

void *

The context for this BUTTON instance.

sl_status_t(*

Member function to initialize BUTTON instance.

void(*

Member function to poll BUTTON.

void(*

Member function to enable BUTTON.

void(*

Member function to disable BUTTON.

Member function to retrieve BUTTON state.

Public Attribute Documentation#

context#

void* sl_button_t::context

The context for this BUTTON instance.


Definition at line 67 of file platform/driver/button/inc/sl_button.h

init#

sl_status_t(* sl_button_t::init) (const sl_button_t *handle)

Member function to initialize BUTTON instance.


Definition at line 68 of file platform/driver/button/inc/sl_button.h

poll#

void(* sl_button_t::poll) (const sl_button_t *handle)

Member function to poll BUTTON.


Definition at line 69 of file platform/driver/button/inc/sl_button.h

enable#

void(* sl_button_t::enable) (const sl_button_t *handle)

Member function to enable BUTTON.


Definition at line 70 of file platform/driver/button/inc/sl_button.h

disable#

void(* sl_button_t::disable) (const sl_button_t *handle)

Member function to disable BUTTON.


Definition at line 71 of file platform/driver/button/inc/sl_button.h

get_state#

sl_button_state_t(* sl_button_t::get_state) (const sl_button_t *handle)

Member function to retrieve BUTTON state.


Definition at line 72 of file platform/driver/button/inc/sl_button.h