A Cycle Counter Instance.
Public Attributes#
uint32_t
Cycle counter at start of recording.
uint32_t
Cycles elapsed in last recording.
uint32_t
Max recorded cycles since last reset or init.
Public Attribute Documentation#
start#
uint32_t sl_cycle_counter_handle_t::start
Cycle counter at start of recording.
Definition at line
103
of file platform/driver/cycle_counter/inc/sl_cycle_counter.h
cycles#
uint32_t sl_cycle_counter_handle_t::cycles
Cycles elapsed in last recording.
Definition at line
104
of file platform/driver/cycle_counter/inc/sl_cycle_counter.h
max#
uint32_t sl_cycle_counter_handle_t::max
Max recorded cycles since last reset or init.
Definition at line
105
of file platform/driver/cycle_counter/inc/sl_cycle_counter.h