ACMP initialization structure.
Public Attributes#
Bias current.
Input range.
ACMP accuracy mode.
Hysteresis level.
Inactive value emitted by ACMP during warmup.
VDD division factor.
If true, ACMP is enabled after configuration.
Public Attribute Documentation#
biasProg#
uint32_t ACMP_Init_TypeDef::biasProg
Bias current.
See the ACMP chapter about bias and response time in the reference manual for details. Valid values are in the range 0-7.
764
of file platform/emlib/inc/em_acmp.h
inputRange#
ACMP_InputRange_TypeDef ACMP_Init_TypeDef::inputRange
Input range.
Adjust this setting to optimize the performance for a given input voltage range.
779
of file platform/emlib/inc/em_acmp.h
accuracy#
ACMP_Accuracy_TypeDef ACMP_Init_TypeDef::accuracy
ACMP accuracy mode.
Select the accuracy mode that matches the required current usage and accuracy requirement. Low accuracy consumes less current while high accuracy consumes more current.
787
of file platform/emlib/inc/em_acmp.h
hysteresisLevel#
ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel
Hysteresis level.
804
of file platform/emlib/inc/em_acmp.h
inactiveValue#
bool ACMP_Init_TypeDef::inactiveValue
Inactive value emitted by ACMP during warmup.
820
of file platform/emlib/inc/em_acmp.h
vrefDiv#
uint32_t ACMP_Init_TypeDef::vrefDiv
VDD division factor.
VREFOUT = VREFIN * (VREFDIV / 63). Valid values are in the 0-63 range.
831
of file platform/emlib/inc/em_acmp.h
enable#
bool ACMP_Init_TypeDef::enable
If true, ACMP is enabled after configuration.
839
of file platform/emlib/inc/em_acmp.h