Dimensions of the display.

Public Attributes#

uint16_t

Horizontal size of the display, in pixels.

uint16_t

Vertical size of the display, in pixels.

uint16_t

X coordinate of the top left corner of the clipping area.

uint16_t

Y coordinate of the top left corner of the clipping area.

uint16_t

Width of the clipping area.

uint16_t

Height of the clipping area.

Public Attribute Documentation#

xSize#

uint16_t DMD_DisplayGeometry::xSize

Horizontal size of the display, in pixels.


Definition at line 121 of file platform/middleware/glib/dmd/dmd.h

ySize#

uint16_t DMD_DisplayGeometry::ySize

Vertical size of the display, in pixels.


Definition at line 123 of file platform/middleware/glib/dmd/dmd.h

xClipStart#

uint16_t DMD_DisplayGeometry::xClipStart

X coordinate of the top left corner of the clipping area.


Definition at line 125 of file platform/middleware/glib/dmd/dmd.h

yClipStart#

uint16_t DMD_DisplayGeometry::yClipStart

Y coordinate of the top left corner of the clipping area.


Definition at line 127 of file platform/middleware/glib/dmd/dmd.h

clipWidth#

uint16_t DMD_DisplayGeometry::clipWidth

Width of the clipping area.


Definition at line 129 of file platform/middleware/glib/dmd/dmd.h

clipHeight#

uint16_t DMD_DisplayGeometry::clipHeight

Height of the clipping area.


Definition at line 131 of file platform/middleware/glib/dmd/dmd.h