Information about a memory error.
Public Attributes#
uint16_t
X coordinate of the address where the error happened.
uint16_t
Y coordinate of the address where the error happened.
uint8_t
The color that was written to the memory address.
uint8_t
The color that was read from the memory address.
Public Attribute Documentation#
x#
uint16_t DMD_MemoryError::x
X coordinate of the address where the error happened.
Definition at line
139
of file platform/middleware/glib/dmd/dmd.h
y#
uint16_t DMD_MemoryError::y
Y coordinate of the address where the error happened.
Definition at line
141
of file platform/middleware/glib/dmd/dmd.h
writtenColor#
uint8_t DMD_MemoryError::writtenColor[3]
The color that was written to the memory address.
Definition at line
143
of file platform/middleware/glib/dmd/dmd.h
readColor#
uint8_t DMD_MemoryError::readColor[3]
The color that was read from the memory address.
Definition at line
145
of file platform/middleware/glib/dmd/dmd.h