System Initialization and Action Processing#

System Initialization and Action Processing.

System Init#

System Init provides a function for initializing the system and the products:

This function calls a set of functions that are automatically generated and located in autogen/sl_event_handler.c. Handlers can be registered for the following events using the Event Handler API provided by the Event Handler component:

  • platform_init -> sl_platform_init()

  • driver_init -> sl_driver_init()

  • service_init -> sl_service_init()

  • stack_init -> sl_stack_init()

  • internal_app_init -> sl_internal_app_init()

These events are fired in the order listed above when sl_system_init() is called.

System Kernel#

System Kernel component provides a function for starting the kernel:

This function calls a functions that is automatically generated and located in $autogen/sl_event_handler.c. Handlers can be registered for the following events using the Event Handler API provided by the Event Handler component:

  • kernel_start -> sl_kernel_start()

The event is fired when sl_system_kernel_start() is called.

System Process Action#

System Process Action component provides a function for running the products from a super loop:

This function calls a set of functions that are automatically generated and located in $autogen/sl_event_handler.c. Handlers can be registered for the following events using the Event Handler API provided by the Event Handler component:

  • platform_process_action -> sl_platform_process_action()

  • service_process_action -> sl_service_process_action()

  • stack_process_action -> sl_stack_process_action()

  • internal_app_process_action -> sl_internal_process_action()

These events are fired in the order listed above when sl_system_process_action() is called.

Usage example:

#if defined(SL_COMPONENT_CATALOG_PRESENT)
#include "sl_component_catalog.h"
#endif
#include "sl_system_init.h"
#include "sl_power_manager.h"
#include "app.h"
#if defined(SL_CATALOG_KERNEL_PRESENT)
#include "sl_system_kernel.h"
#else
#include "sl_system_process_action.h"
#endif

int main(void)
{
  // Initialize Silicon Labs device, system, service(s) and protocol stack(s).
  // Note that if the kernel is present, processing task(s) will be created by
  // this call.
  sl_system_init();

  // Initialize the application.
  app_init();

#if defined(SL_CATALOG_KERNEL_PRESENT)
  // Start the kernel. Task(s) created in app_init() will start running.
  sl_system_kernel_start();
#else
  do {
    // Do not remove this call: Silicon Labs components process action routine
    // must be called from the super loop.
    sl_system_process_action();

    // Application process.
    app_process_action();

    // Let the CPU go to sleep if the system allow it.
    sl_power_manager_sleep();
  } while (1);
#endif // SL_CATALOG_KERNEL_PRESENT
}

Functions#

void

System processing action.

void

Start the kernel.

void

Initialize Silicon Labs products.

Function Documentation#

sl_system_process_action#

void sl_system_process_action (void )

System processing action.

Parameters
TypeDirectionArgument NameDescription
voidN/A

sl_system_kernel_start#

void sl_system_kernel_start (void )

Start the kernel.

Parameters
TypeDirectionArgument NameDescription
voidN/A

sl_system_init#

void sl_system_init (void )

Initialize Silicon Labs products.

Parameters
TypeDirectionArgument NameDescription
voidN/A