Attestation#
System and configuration attestation.
API for retrieveing attestation tokens from the SE.
Functions#
Get the PSA initial attest token from the SE.
Get the size of a PSA initial attest token with the given nonce.
Get an attested (signed) security configuration token from the SE.
Get the size of a security configuration token.
Macros#
32 byte challenge size
48 byte challenge size
64 byte challenge size
Function Documentation#
sl_se_attestation_get_psa_iat_token#
sl_status_t sl_se_attestation_get_psa_iat_token (sl_se_command_context_t * cmd_ctx, const uint8_t * auth_challenge, size_t challenge_size, uint8_t * token_buf, size_t token_buf_size, size_t * token_size)
Get the PSA initial attest token from the SE.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const uint8_t * | [in] | auth_challenge | Buffer with a challenge object selected by the caller.  | 
| size_t | [in] | challenge_size | Size of the challenge object in bytes. Must be either 32, 48 or 64.  | 
| uint8_t * | [out] | token_buf | Buffer where the output token will be stored.  | 
| size_t | [in] | token_buf_size | Size of token_buf in bytes. Must be at least the size found by calling sl_se_attestation_get_psa_iat_token_size with equivalent arguments, and padded to word alignment.  | 
| size_t * | [out] | token_size | Number of bytes actually used in token_buf.  | 
Warnings
Once a nonce/challenge has been used, the same challenge should not be used ever again, to prevent replay attacks.
The output will be length-extended to the next word-multiple.
Returns
Status code, sl_status.h.
sl_se_attestation_get_psa_iat_token_size#
sl_status_t sl_se_attestation_get_psa_iat_token_size (sl_se_command_context_t * cmd_ctx, size_t challenge_size, size_t * token_size)
Get the size of a PSA initial attest token with the given nonce.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| size_t | [in] | challenge_size | Size of the challenge object in bytes. Must be either 32, 48 or 64.  | 
| size_t * | [out] | token_size | Pointer to output word. Result is stored here.  | 
Returns
Status code, sl_status.h.
sl_se_attestation_get_config_token#
sl_status_t sl_se_attestation_get_config_token (sl_se_command_context_t * cmd_ctx, const uint8_t * auth_challenge, size_t challenge_size, uint8_t * token_buf, size_t token_buf_size, size_t * token_size)
Get an attested (signed) security configuration token from the SE.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| const uint8_t * | [in] | auth_challenge | Buffer with a challenge object selected by the caller.  | 
| size_t | [in] | challenge_size | Size of the challenge object in bytes. Must be 32.  | 
| uint8_t * | [out] | token_buf | Buffer where the output token will be stored.  | 
| size_t | [in] | token_buf_size | Size of token_buf in bytes. Must be at least the size found by calling sl_se_attestation_get_config_token_size with equivalent arguments, and padded to word alignment.  | 
| size_t * | [out] | token_size | Number of bytes actually used in token_buf.  | 
Warnings
Once a nonce/challenge has been used, the same challenge should not be used ever again, to prevent replay attacks.
The output will be length-extended to the next word-multiple.
Returns
Status code, sl_status.h.
sl_se_attestation_get_config_token_size#
sl_status_t sl_se_attestation_get_config_token_size (sl_se_command_context_t * cmd_ctx, size_t challenge_size, size_t * token_size)
Get the size of a security configuration token.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object.  | 
| size_t | [in] | challenge_size | Size of the challenge object in bytes. Must be 32.  | 
| size_t * | [out] | token_size | Pointer to output word. Result is stored here.  | 
Returns
Status code, sl_status.h.