Signature#
Digital Signature Algorithms (ECDSA, EdDSA).
API for using digital signatures with the SE.
Functions#
This function computes Elliptic-Curve Cryptography (ECC) digital signatures of a message.
This function verifies Elliptic-Curve Cryptography (ECC) digital signatures of a message.
Function Documentation#
sl_se_ecc_sign#
sl_status_t sl_se_ecc_sign (sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, sl_se_hash_type_t hash_alg, bool hashed_message, const unsigned char * message, size_t message_len, unsigned char * signature, size_t signature_len)
This function computes Elliptic-Curve Cryptography (ECC) digital signatures of a message.
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure. |
sl_se_hash_type_t | [in] | hash_alg | Which hashing algorithm to use. Ignored for EdDSA keys, since EdDSA always uses SHA-512 for Ed25519 and SHA-3 for Ed448. |
bool | [in] | hashed_message | The input message is a message digest. Ignored for EdDSA keys, and treated as false. |
const unsigned char * | [in] | message | The message to be used to compute the signature. |
size_t | [in] | message_len | The length of message. |
unsigned char * | [out] | signature | The computed signature. |
size_t | [in] | signature_len | The length of the computed signature. |
Note
Edwards-curve Digital Signature Algorithm (EdDSA) generates a message digest using the input message for computing signatures. The input parameters
hash_alg
andhashed_message
do not apply for EdDSA.
P-521 Elliptic Curve for Elliptic Curve Digital Signature Algorithm (ECDSA) expects a 544 bits (68 bytes) buffer for storing private keys, and a 1088 bits (136 bytes) buffer for storing public keys and signatures. The first 23 bits of d, Qx, Qy, R and S are padding bits to comply word-aligned addressing.
Returns
SL_STATUS_OK when the command was executed successfully, otherwise an appropiate error code (sl_status.h).
sl_se_ecc_verify#
sl_status_t sl_se_ecc_verify (sl_se_command_context_t * cmd_ctx, const sl_se_key_descriptor_t * key, sl_se_hash_type_t hash_alg, bool hashed_message, const unsigned char * message, size_t message_len, const unsigned char * signature, size_t signature_len)
This function verifies Elliptic-Curve Cryptography (ECC) digital signatures of a message.
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
const sl_se_key_descriptor_t * | [in] | key | Pointer to sl_se_key_descriptor_t structure. |
sl_se_hash_type_t | [in] | hash_alg | Which hashing algorithm to use. Ignored for EdDSA keys, since EdDSA always uses SHA-512 for Ed25519 and SHA-3 for Ed448. |
bool | [in] | hashed_message | The input message is a message digest. Ignored for EdDSA keys, and treated as false. |
const unsigned char * | [in] | message | The message to be used to compute signatures. |
size_t | [in] | message_len | The length of message. |
const unsigned char * | [in] | signature | The signature to be verified. |
size_t | [in] | signature_len | The length of signature. |
Note
The input parameters
hash_alg
andhashed_message
do not apply for Edwards-curve Digital Signature Algorithm (EdDSA).
P-521 Elliptic Curve for Elliptic Curve Digital Signature Algorithm (ECDSA) expects a 544 bits (68 bytes) buffer for storing private keys, and a 1088 bits (136 bytes) buffer for storing public keys and signatures. The first 23 bits of d, Qx, Qy, R and S are padding bits to comply word-aligned addressing.
Returns
SL_STATUS_OK if the signature is successfully verified, otherwise an appropiate error code (sl_status.h).