SE status.

Public Attributes#

uint32_t

Boot status code / error code (Bits [7:0]).

uint32_t

SE firmware version.

uint32_t

Host firmware version (if available).

bool

Secure boot enabled.

bool

Active mode enabled.

uint32_t

Recorded tamper status. Reset on status read.

uint32_t

Currently active tamper sources.

Public Attribute Documentation#

boot_status#

uint32_t sl_se_status_t::boot_status

Boot status code / error code (Bits [7:0]).


Definition at line 304 of file platform/security/sl_component/se_manager/inc/sl_se_manager_types.h

se_fw_version#

uint32_t sl_se_status_t::se_fw_version

SE firmware version.


Definition at line 306 of file platform/security/sl_component/se_manager/inc/sl_se_manager_types.h

host_fw_version#

uint32_t sl_se_status_t::host_fw_version

Host firmware version (if available).


Definition at line 308 of file platform/security/sl_component/se_manager/inc/sl_se_manager_types.h

debug_status#

sl_se_debug_status_t sl_se_status_t::debug_status

Debug lock status.


Definition at line 310 of file platform/security/sl_component/se_manager/inc/sl_se_manager_types.h

secure_boot_enabled#

bool sl_se_status_t::secure_boot_enabled

Secure boot enabled.


Definition at line 312 of file platform/security/sl_component/se_manager/inc/sl_se_manager_types.h

active_mode_enabled#

bool sl_se_status_t::active_mode_enabled

Active mode enabled.


Definition at line 314 of file platform/security/sl_component/se_manager/inc/sl_se_manager_types.h

tamper_status#

uint32_t sl_se_status_t::tamper_status

Recorded tamper status. Reset on status read.


Definition at line 316 of file platform/security/sl_component/se_manager/inc/sl_se_manager_types.h

tamper_status_raw#

uint32_t sl_se_status_t::tamper_status_raw

Currently active tamper sources.


Definition at line 318 of file platform/security/sl_component/se_manager/inc/sl_se_manager_types.h