VDAC - Voltage DAC#

Digital to Analog Voltage Converter (VDAC) Peripheral API.

This module contains functions to control the VDAC peripheral of Silicon Labs' 32-bit MCUs and SoCs. VDAC converts digital values to analog signals at up to 500 ksps with 12-bit accuracy. VDAC is designed for low energy consumption, but can also provide very good performance.

The following steps are necessary for basic operation:

Clock enable:

CMU_ClockEnable(cmuClock_VDAC0, true);

Initialize the VDAC with default settings and modify selected fields:

VDAC_Init_TypeDef vdacInit          = VDAC_INIT_DEFAULT;
VDAC_InitChannel_TypeDef vdacChInit = VDAC_INITCHANNEL_DEFAULT;

// Set prescaler to get 1 MHz VDAC clock frequency.
vdacInit.prescaler = VDAC_PrescaleCalc(1000000, true, 0); // function call for series 0/1
VDAC_Init(VDAC0, &vdacInit);

vdacChInit.enable = true;
VDAC_InitChannel(VDAC0, &vdacChInit, 0);

Perform a conversion:

VDAC_ChannelOutputSet(VDAC0, 0, 250);

Note

  • The output stage of a VDAC channel consists of an on-chip operational amplifier (OPAMP) in the OPAMP module. This OPAMP is highly configurable; and to exploit the VDAC functionality fully, configure the OPAMP using the OPAMP API. Using the OPAMP API also loads OPAMP calibration values. The default (reset) settings of OPAMP is sufficient for many applications.

Modules#

VDAC_Init_TypeDef

VDAC_InitChannel_TypeDef

Enumerations#

enum
vdacRefresh2 = _VDAC_CFG_REFRESHPERIOD_CYCLES2
vdacRefresh4 = _VDAC_CFG_REFRESHPERIOD_CYCLES4
vdacRefresh8 = _VDAC_CFG_REFRESHPERIOD_CYCLES8
vdacRefresh16 = _VDAC_CFG_REFRESHPERIOD_CYCLES16
vdacRefresh32 = _VDAC_CFG_REFRESHPERIOD_CYCLES32
vdacRefresh64 = _VDAC_CFG_REFRESHPERIOD_CYCLES64
vdacRefresh128 = _VDAC_CFG_REFRESHPERIOD_CYCLES128
vdacRefresh256 = _VDAC_CFG_REFRESHPERIOD_CYCLES256
}

Channel refresh period.

enum
vdacCycles2 = _VDAC_CFG_TIMEROVRFLOWPERIOD_CYCLES2
vdacCycles4 = _VDAC_CFG_TIMEROVRFLOWPERIOD_CYCLES4
vdacCycles8 = _VDAC_CFG_TIMEROVRFLOWPERIOD_CYCLES8
vdacCycles16 = _VDAC_CFG_TIMEROVRFLOWPERIOD_CYCLES16
vdacCycles32 = _VDAC_CFG_TIMEROVRFLOWPERIOD_CYCLES32
vdacCycles64 = _VDAC_CFG_TIMEROVRFLOWPERIOD_CYCLES64
}

Timer overflow period.

enum
vdacRef1V25 = _VDAC_CFG_REFRSEL_V125
vdacRef2V5 = _VDAC_CFG_REFRSEL_V25
vdacRefAvdd = _VDAC_CFG_REFRSEL_VDD
vdacRefExtPin = _VDAC_CFG_REFRSEL_EXT
}

Reference voltage for VDAC.

enum
vdacRefreshSrcNone = _VDAC_CH0CFG_REFRESHSOURCE_NONE
vdacRefreshSrcRefreshTimer = _VDAC_CH0CFG_REFRESHSOURCE_REFRESHTIMER
vdacRefreshSrcSyncPrs = _VDAC_CH0CFG_REFRESHSOURCE_SYNCPRS
vdacRefreshSrcAsyncPrs = _VDAC_CH0CFG_REFRESHSOURCE_ASYNCPRS
}

Refresh source for VDAC.

enum
vdacTrigModeNone = _VDAC_CH0CFG_TRIGMODE_NONE
vdacTrigModeSw = _VDAC_CH0CFG_TRIGMODE_SW
vdacTrigModeSyncPrs = _VDAC_CH0CFG_TRIGMODE_SYNCPRS
vdacTrigModeLesense = _VDAC_CH0CFG_TRIGMODE_LESENSE
vdacTrigModeInternalTimer = _VDAC_CH0CFG_TRIGMODE_INTERNALTIMER
vdacTrigModeAsyncPrs = _VDAC_CH0CFG_TRIGMODE_ASYNCPRS
}

Channel conversion trigger mode.

enum
vdacPowerModeHighPower = _VDAC_CH0CFG_POWERMODE_HIGHPOWER
vdacPowerModeLowPower = _VDAC_CH0CFG_POWERMODE_LOWPOWER
}

Channel power mode.

enum
vdacChPortNone = _VDAC_OUTCTRL_ABUSPORTSELCH0_NONE
vdacChPortA = _VDAC_OUTCTRL_ABUSPORTSELCH0_PORTA
vdacChPortB = _VDAC_OUTCTRL_ABUSPORTSELCH0_PORTB
vdacChPortC = _VDAC_OUTCTRL_ABUSPORTSELCH0_PORTC
vdacChPortD = _VDAC_OUTCTRL_ABUSPORTSELCH0_PORTD
}

VDAC channel Abus port selection.

Functions#

void
VDAC_ChannelOutputSet(VDAC_TypeDef *vdac, unsigned int channel, uint32_t value)

Set the output signal of a VDAC channel to a given value.

void
VDAC_Enable(VDAC_TypeDef *vdac, unsigned int ch, bool enable)

Enable/disable the VDAC channel.

void
VDAC_Init(VDAC_TypeDef *vdac, const VDAC_Init_TypeDef *init)

Initialize VDAC.

void
VDAC_InitChannel(VDAC_TypeDef *vdac, const VDAC_InitChannel_TypeDef *init, unsigned int ch)

Initialize a VDAC channel.

void
VDAC_SineModeStart(VDAC_TypeDef *vdac, bool start)

Start/stop Sinemode.

void
VDAC_Channel0OutputSet(VDAC_TypeDef *vdac, uint32_t value)

Set the output signal of VDAC channel 0 to a given value.

void
VDAC_Channel1OutputSet(VDAC_TypeDef *vdac, uint32_t value)

Set the output signal of VDAC channel 1 to a given value.

void
VDAC_IntClear(VDAC_TypeDef *vdac, uint32_t flags)

Clear one or more pending VDAC interrupts.

void
VDAC_IntDisable(VDAC_TypeDef *vdac, uint32_t flags)

Disable one or more VDAC interrupts.

void
VDAC_IntEnable(VDAC_TypeDef *vdac, uint32_t flags)

Enable one or more VDAC interrupts.

uint32_t
VDAC_IntGet(VDAC_TypeDef *vdac)

Get pending VDAC interrupt flags.

uint32_t
VDAC_IntGetEnabled(VDAC_TypeDef *vdac)

Get enabled and pending VDAC interrupt flags.

void
VDAC_IntSet(VDAC_TypeDef *vdac, uint32_t flags)

Set one or more pending VDAC interrupts from SW.

uint32_t
VDAC_GetStatus(VDAC_TypeDef *vdac)

Get the VDAC Status register.

uint32_t
VDAC_PrescaleCalc(VDAC_TypeDef *vdac, uint32_t vdacFreq)

Calculate the prescaler value used to determine VDAC clock.

void
VDAC_Reset(VDAC_TypeDef *vdac)

Reset VDAC to same state that it was in after a hardwares reset.

Macros#

#define

Default configuration for VDAC initialization structure.

#define

Sine mode configuration for VDAC initialization structure.

#define

Default configuration for VDAC channel initialization structure.

Enumeration Documentation#

VDAC_Refresh_TypeDef#

VDAC_Refresh_TypeDef

Channel refresh period.

Enumerator
vdacRefresh2

Refresh every 2 clock cycles.

vdacRefresh4

Refresh every 4 clock cycles.

vdacRefresh8

Refresh every 8 clock cycles.

vdacRefresh16

Refresh every 16 clock cycles.

vdacRefresh32

Refresh every 32 clock cycles.

vdacRefresh64

Refresh every 64 clock cycles.

vdacRefresh128

Refresh every 128 clock cycles.

vdacRefresh256

Refresh every 256 clock cycles.


VDAC_TimerOverflow_TypeDef#

VDAC_TimerOverflow_TypeDef

Timer overflow period.

Enumerator
vdacCycles2

Overflows every 2 clock cycles.

vdacCycles4

Overflows every 4 clock cycles.

vdacCycles8

Overflows every 8 clock cycles.

vdacCycles16

Overflows every 16 clock cycles.

vdacCycles32

Overflows every 32 clock cycles.

vdacCycles64

Overflows every 64 clock cycles.


VDAC_Ref_TypeDef#

VDAC_Ref_TypeDef

Reference voltage for VDAC.

Enumerator
vdacRef1V25

Internal 1.25 V band gap reference.

vdacRef2V5

Internal 2.5 V band gap reference.

vdacRefAvdd

AVDD reference.

vdacRefExtPin

External pin reference.


VDAC_RefreshSource_TypeDef#

VDAC_RefreshSource_TypeDef

Refresh source for VDAC.

Enumerator
vdacRefreshSrcNone

No refresh source.

vdacRefreshSrcRefreshTimer

Refresh triggered by refresh timer overflow.

vdacRefreshSrcSyncPrs

Refresh triggered by sync PRS.

vdacRefreshSrcAsyncPrs

Refresh triggered by async PRS.


VDAC_TrigMode_TypeDef#

VDAC_TrigMode_TypeDef

Channel conversion trigger mode.

Enumerator
vdacTrigModeNone

No conversion trigger source selected.

vdacTrigModeSw

Channel is triggered by CHnDATA or COMBDATA write.

vdacTrigModeSyncPrs

Channel is triggered by Sync PRS input.

vdacTrigModeLesense

Channel is triggered by LESENSE.

vdacTrigModeInternalTimer

Channel is triggered by Internal Timer.

vdacTrigModeAsyncPrs

Channel is triggered by Async PRS input.


VDAC_PowerMode_TypeDef#

VDAC_PowerMode_TypeDef

Channel power mode.

Enumerator
vdacPowerModeHighPower

High power buffer mode.

vdacPowerModeLowPower

Low power buffer mode.


VDAC_ChPortSel_t#

VDAC_ChPortSel_t

VDAC channel Abus port selection.

Enumerator
vdacChPortNone

No GPIO selected.

vdacChPortA

Port A selected.

vdacChPortB

Port B selected.

vdacChPortC

Port C selected.

vdacChPortD

Port D selected.


Function Documentation#

VDAC_ChannelOutputSet#

void VDAC_ChannelOutputSet (VDAC_TypeDef * vdac, unsigned int channel, uint32_t value)

Set the output signal of a VDAC channel to a given value.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.

unsigned int[in]channel

A channel number to set the output of.

uint32_t[in]value

A value to write to the channel output register CHnDATA.

This function sets the output signal of a VDAC channel by writing value to the corresponding CHnDATA register.


VDAC_Enable#

void VDAC_Enable (VDAC_TypeDef * vdac, unsigned int ch, bool enable)

Enable/disable the VDAC channel.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.

unsigned int[in]ch

A channel to enable/disable.

bool[in]enable

True to enable VDAC channel, false to disable.


VDAC_Init#

void VDAC_Init (VDAC_TypeDef * vdac, const VDAC_Init_TypeDef * init)

Initialize VDAC.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.

const VDAC_Init_TypeDef *[in]init

A pointer to the VDAC initialization structure.

Initializes the common parts for both channels. This function will also load calibration values from the Device Information (DI) page into the VDAC calibration register. To complete a VDAC setup, channel control configuration must also be done. See VDAC_InitChannel().

Note

  • This function will disable both channels prior to configuration.


VDAC_InitChannel#

void VDAC_InitChannel (VDAC_TypeDef * vdac, const VDAC_InitChannel_TypeDef * init, unsigned int ch)

Initialize a VDAC channel.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.

const VDAC_InitChannel_TypeDef *[in]init

A pointer to the VDAC channel initialization structure.

unsigned int[in]ch

A channel number to initialize.


VDAC_SineModeStart#

void VDAC_SineModeStart (VDAC_TypeDef * vdac, bool start)

Start/stop Sinemode.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

Pointer to VDAC peripheral register block.

bool[in]start

True to start the Sine mode, false to stop it.

This function sends the sine mode start/stop signal to the DAC.


VDAC_Channel0OutputSet#

void VDAC_Channel0OutputSet (VDAC_TypeDef * vdac, uint32_t value)

Set the output signal of VDAC channel 0 to a given value.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

Pointer to VDAC peripheral register block.

uint32_t[in]value

Value to write to channel 0 output register CH0DATA.

This function sets the output signal of VDAC channel 0 by writing value to the CH0DATA register.


VDAC_Channel1OutputSet#

void VDAC_Channel1OutputSet (VDAC_TypeDef * vdac, uint32_t value)

Set the output signal of VDAC channel 1 to a given value.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

Pointer to VDAC peripheral register block.

uint32_t[in]value

Value to write to channel 1 output register CH1DATA.

This function sets the output signal of VDAC channel 1 by writing value to the CH1DATA register.


VDAC_IntClear#

void VDAC_IntClear (VDAC_TypeDef * vdac, uint32_t flags)

Clear one or more pending VDAC interrupts.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

Pointer to VDAC peripheral register block.

uint32_t[in]flags

Pending VDAC interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the VDAC module (VDAC_IF_nnn).


VDAC_IntDisable#

void VDAC_IntDisable (VDAC_TypeDef * vdac, uint32_t flags)

Disable one or more VDAC interrupts.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

Pointer to VDAC peripheral register block.

uint32_t[in]flags

VDAC interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the VDAC module (VDAC_IF_nnn).


VDAC_IntEnable#

void VDAC_IntEnable (VDAC_TypeDef * vdac, uint32_t flags)

Enable one or more VDAC interrupts.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

Pointer to VDAC peripheral register block.

uint32_t[in]flags

VDAC interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the VDAC module (VDAC_IF_nnn).

Note

  • Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using VDAC_IntClear() prior to enabling the interrupt.


VDAC_IntGet#

uint32_t VDAC_IntGet (VDAC_TypeDef * vdac)

Get pending VDAC interrupt flags.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

Pointer to VDAC peripheral register block.

Note

  • The event bits are not cleared by the use of this function.

Returns

  • VDAC interrupt sources pending. Use a bitwise logic OR combination of valid interrupt flags for the VDAC module (VDAC_IF_nnn).


VDAC_IntGetEnabled#

uint32_t VDAC_IntGetEnabled (VDAC_TypeDef * vdac)

Get enabled and pending VDAC interrupt flags.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

Pointer to VDAC peripheral register block.

Useful for handling more interrupt sources in the same interrupt handler.

Note

  • Interrupt flags are not cleared by the use of this function.

Returns

  • Pending and enabled VDAC interrupt sources. The return value is the bitwise AND combination of

    • the OR combination of enabled interrupt sources in VDACx_IEN_nnn register (VDACx_IEN_nnn) and

    • the OR combination of valid interrupt flags of the VDAC module (VDACx_IF_nnn).


VDAC_IntSet#

void VDAC_IntSet (VDAC_TypeDef * vdac, uint32_t flags)

Set one or more pending VDAC interrupts from SW.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

Pointer to VDAC peripheral register block.

uint32_t[in]flags

VDAC interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the VDAC module (VDAC_IF_nnn).


VDAC_GetStatus#

uint32_t VDAC_GetStatus (VDAC_TypeDef * vdac)

Get the VDAC Status register.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

Pointer to VDAC peripheral register block.

Returns

  • Current STATUS register value.


VDAC_PrescaleCalc#

uint32_t VDAC_PrescaleCalc (VDAC_TypeDef * vdac, uint32_t vdacFreq)

Calculate the prescaler value used to determine VDAC clock.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

Pointer to VDAC peripheral register block.

uint32_t[in]vdacFreq

VDAC frequency target. The frequency will automatically be adjusted to be below maximum allowed VDAC clock.

The VDAC clock is given by the input clock divided by the prescaler+1.

VDAC_CLK = IN_CLK / (prescale + 1)

The maximum VDAC clock is 1 MHz.

Note

  • If the requested VDAC frequency is low and the maximum prescaler value can't adjust the actual VDAC frequency lower than requested, the maximum prescaler value is returned resulting in a higher VDAC frequency than requested.

Returns

  • A prescaler value to use for VDAC to achieve a clock value less than or equal to vdacFreq.


VDAC_Reset#

void VDAC_Reset (VDAC_TypeDef * vdac)

Reset VDAC to same state that it was in after a hardwares reset.

Parameters
TypeDirectionArgument NameDescription
VDAC_TypeDef *[in]vdac

A pointer to the VDAC peripheral register block.


Macro Definition Documentation#

VDAC_INIT_DEFAULT#

#define VDAC_INIT_DEFAULT
Value:
{ \
_VDAC_CFG_WARMUPTIME_DEFAULT, /* Number of prescaled DAC_CLK for Vdac to warmup. */ \
false, /* Continue while debugging. */ \
false, /* On demand clock. */ \
false, /* DMA wake up. */ \
false, /* Bias keep warm. */ \
vdacRefresh2, /* Refresh every 2th cycle. */ \
vdacCycles2, /* Internal overflow every 2th cycle. */ \
0, /* No prescaling. */ \
vdacRef1V25, /* 1.25 V internal low noise reference. */ \
false, /* Do not reset prescaler on CH 0 start. */ \
false, /* Sine wave is stopped at the sample its currently outputting. */ \
false, /* Disable sine mode. */ \
false, /* Differential mode. */ \
}

Default configuration for VDAC initialization structure.


VDAC_INIT_SINE_GENERATION_MODE#

#define VDAC_INIT_SINE_GENERATION_MODE
Value:
{ \
_VDAC_CFG_WARMUPTIME_DEFAULT, /* Number of prescaled DAC_CLK for Vdac to warmup. */ \
false, /* Continue while debugging. */ \
true, /* On demand clock. */ \
false, /* DMA wake up. */ \
false, /* Bias keep warm. */ \
vdacRefresh8, /* Refresh every 8th cycle. */ \
vdacCycles2, /* Internal overflow every 8th cycle. */ \
0, /* No prescaling. */ \
vdacRef1V25, /* 1.25 V internal low noise reference. */ \
false, /* Do not reset prescaler on CH 0 start. */ \
false, /* Sine wave is stopped at the sample its currently outputting. */ \
true, /* Enable sine mode. */ \
false, /* Differential mode. */ \
}

Sine mode configuration for VDAC initialization structure.


VDAC_INITCHANNEL_DEFAULT#

#define VDAC_INITCHANNEL_DEFAULT
Value:
{ \
false, /* Leave channel disabled when initialization is done. */ \
false, /* Turn off between sample off conversions.*/ \
true, /* Enable High cap mode. */ \
0, /* FIFO data low watermark at 0. */ \
vdacRefreshSrcNone, /* Channel refresh source. */ \
vdacTrigModeSw, /* Conversion trigged by CH0DATA or COMBDATA write. */ \
vdacPowerModeHighPower, /* High power mode enabled. */ \
false, /* Continuous conversion mode. */ \
0, /* ABUS pin selected. */ \
vdacChPortNone, /* No Analog bus port selected. */ \
false, /* Output not shorted */ \
false, /* Alternative output disabled. */ \
true, /* Main output enabled. */ \
0, /* Hold out time. Previously called settle time */ \
}

Default configuration for VDAC channel initialization structure.