Utilities#
Device initialisation, debug lock, upgrade functionality, user data...
API for managing the Secure Engine or Root code on a device. Upload and read device configuration.
Modules#
Enumerations#
OTP key types.
Typedefs#
SE tamper signal levels.
SE tamper signals.
SE tamper filter timeout period.
Number of tamper counts to trigger the filter signal.
SE certificate types.
SE Debug lock flags.
SE challenge storage.
Functions#
Validate SE firmware image.
Apply SE firmware image.
Get upgrade status of SE firmware image.
Validate Host firmware image.
Apply Host firmware image.
Get upgrade status of Host firmware image.
Initialize key to be stored in the SE OTP flash.
Read a public key stored in the SE.
Initialize and commit SE OTP configuration to OTP.
Read the OTP firmware version of the SE module.
Read SE OTP configuration.
Read the SE firmware version.
Returns the current debug lock configuration.
Enables the debug lock for the part.
Writes data to User Data section in MTP.
Erases User Data section in MTP.
Returns the current boot status, versions and system configuration.
Read the serial number of the SE module.
Read the EMU->RSTCAUSE after a tamper reset.
Read the latest cached tamper reset cause.
Enables the secure debug functionality.
Disables the secure debug functionality.
Set debug options.
Performs a device mass erase and debug unlock.
Disabled device erase functionality.
Request challenge from SE which can be used to open debug access.
Invalidate current challenge and make a new challenge.
Unlock debug access using certificate and signed challenge.
Temporarily disable tamper configuration using certificate and signed challenge.
Read size of stored certificates in SE.
Read stored certificates in SE.
Enter SE active mode.
Exit SE active mode.
Macros#
Default configuration for OTP initialisation structure.
SE Challenge size.
Certificate key size.
Certificate signature size.
Batch ID certificate.
SE ID certificate.
Host ID certificate.
Enumeration Documentation#
sl_se_device_key_type_t#
sl_se_device_key_type_t
OTP key types.
| Enumerator | |
|---|---|
| SL_SE_KEY_TYPE_IMMUTABLE_BOOT | |
| SL_SE_KEY_TYPE_IMMUTABLE_AUTH | |
| SL_SE_KEY_TYPE_IMMUTABLE_AES_128 | |
| SL_SE_KEY_TYPE_IMMUTABLE_ATTESTATION | |
| SL_SE_KEY_TYPE_IMMUTABLE_SE_ATTESTATION | |
Typedef Documentation#
sl_se_tamper_filter_period_t#
typedef uint8_t sl_se_tamper_filter_period_t
SE tamper filter timeout period.
sl_se_tamper_filter_threshold_t#
typedef uint8_t sl_se_tamper_filter_threshold_t
Number of tamper counts to trigger the filter signal.
sl_se_challenge_t#
typedef uint8_t sl_se_challenge_t[SL_SE_CHALLENGE_SIZE] [SL_SE_CHALLENGE_SIZE]
SE challenge storage.
Function Documentation#
sl_se_check_se_image#
sl_status_t sl_se_check_se_image (sl_se_command_context_t * cmd_ctx, void * image_addr)
Validate SE firmware image.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| void * | [in] | image_addr | Pointer to SE image to validate. | 
Validate SE firmware image located at given address. This function is typically used before calling sl_se_apply_se_image.
Returns
- One of the following status codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
 
sl_se_apply_se_image#
sl_status_t sl_se_apply_se_image (sl_se_command_context_t * cmd_ctx, void * image_addr)
Apply SE firmware image.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| void * | [in] | image_addr | Pointer to SE image to apply. | 
Apply SE firmware image located at given address.
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
 
sl_se_get_upgrade_status_se_image#
sl_status_t sl_se_get_upgrade_status_se_image (sl_se_command_context_t * cmd_ctx, uint32_t * status, uint32_t * prev_version)
Get upgrade status of SE firmware image.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| uint32_t * | [in] | status | Pointer to 32-bit word where to return upgrade status. | 
| uint32_t * | [in] | prev_version | Pointer to 32-bit word where to return previous version. | 
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
 
sl_se_check_host_image#
sl_status_t sl_se_check_host_image (sl_se_command_context_t * cmd_ctx, void * image_addr, uint32_t size)
Validate Host firmware image.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| void * | [in] | image_addr | Pointer to Host image to validate. | 
| uint32_t | [in] | size | Size of Host image to validate. | 
Validate Host firmware image located at given address. This function is typically used before calling sl_se_apply_host_image.
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
 
sl_se_apply_host_image#
sl_status_t sl_se_apply_host_image (sl_se_command_context_t * cmd_ctx, void * image_addr, uint32_t size)
Apply Host firmware image.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| void * | [in] | image_addr | Pointer to Host image to apply. | 
| uint32_t | [in] | size | Size of Host image to apply. | 
Apply Host firmware image located at given address.
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
 
sl_se_get_upgrade_status_host_image#
sl_status_t sl_se_get_upgrade_status_host_image (sl_se_command_context_t * cmd_ctx, uint32_t * status, uint32_t * prev_version)
Get upgrade status of Host firmware image.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| uint32_t * | [in] | status | Pointer to 32-bit word where to return upgrade status. | 
| uint32_t * | [in] | prev_version | Pointer to 32-bit word where to return previous version. | 
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
 
sl_se_init_otp_key#
sl_status_t sl_se_init_otp_key (sl_se_command_context_t * cmd_ctx, sl_se_device_key_type_t key_type, void * key, uint32_t num_bytes)
Initialize key to be stored in the SE OTP flash.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| sl_se_device_key_type_t | [in] | key_type | ID of key type to initialize. | 
| void * | [in] | key | Pointer to a buffer that contains the key. Public keys must be word aligned and have a length of 64 bytes. AES-128 keys must be word aligned and have length of 16 bytes. | 
| uint32_t | [in] | num_bytes | Length of key buffer in bytes (16 or 64 bytes). | 
Initialize key stored in the SE. The command can be used to write (sl_se_device_key_type_t):
- SL_SE_KEY_TYPE_IMMUTABLE_BOOT 
- SL_SE_KEY_TYPE_IMMUTABLE_AUTH 
- SL_SE_KEY_TYPE_IMMUTABLE_AES_128 
Note
- These keys can not be overwritten, so this command can only be issued once per key per part. 
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
 
sl_se_read_pubkey#
sl_status_t sl_se_read_pubkey (sl_se_command_context_t * cmd_ctx, sl_se_device_key_type_t key_type, void * key, uint32_t num_bytes)
Read a public key stored in the SE.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| sl_se_device_key_type_t | [in] | key_type | ID of key type to read. | 
| void * | [out] | key | Pointer to a buffer to contain the returned public key. Must be word aligned and have a length of 64 bytes. | 
| uint32_t | [in] | num_bytes | Length of pubkey buffer (64 bytes). | 
Read out a public key stored in the SE. The command can be used to read (sl_se_device_key_type_t):
- SL_SE_KEY_TYPE_IMMUTABLE_BOOT 
- SL_SE_KEY_TYPE_IMMUTABLE_AUTH 
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
 
sl_se_init_otp#
sl_status_t sl_se_init_otp (sl_se_command_context_t * cmd_ctx, sl_se_otp_init_t * otp_init)
Initialize and commit SE OTP configuration to OTP.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| sl_se_otp_init_t * | [in] | otp_init | Pointer to OTP initialization structure. | 
Warnings
- When this function succeeds the configuration is committed to OTP and cannot be changed. 
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
- SL_STATUS_ABORTwhen the operation is not attempted.
 
sl_se_get_otp_version#
sl_status_t sl_se_get_otp_version (sl_se_command_context_t * cmd_ctx, uint32_t * version)
Read the OTP firmware version of the SE module.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| uint32_t * | [out] | version | Pointer to uint32_t word where version shall be returned. | 
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_OPERATIONwhen the SE command ID is not recognized
- SL_STATUS_INVALID_CREDENTIALSwhen the command is not authorized
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
 
sl_se_read_otp#
sl_status_t sl_se_read_otp (sl_se_command_context_t * cmd_ctx, sl_se_otp_init_t * otp_settings)
Read SE OTP configuration.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| sl_se_otp_init_t * | [out] | otp_settings | Pointer to OTP initialization structure. | 
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_COMMANDif OTP configuration isn't initialized
- SL_STATUS_ABORTwhen the operation is not attempted.
 
sl_se_get_se_version#
sl_status_t sl_se_get_se_version (sl_se_command_context_t * cmd_ctx, uint32_t * version)
Read the SE firmware version.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| uint32_t * | [out] | version | Pointer to uint32_t word where version shall be returned. | 
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_OWNERSHIPwhen the ownership is already taken
- SL_STATUS_INVALID_OPERATIONwhen the SE command ID is not recognized
- SL_STATUS_INVALID_CREDENTIALSwhen the command is not authorized
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
 
sl_se_get_debug_lock_status#
sl_status_t sl_se_get_debug_lock_status (sl_se_command_context_t * cmd_ctx, sl_se_debug_status_t * status)
Returns the current debug lock configuration.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| sl_se_debug_status_t * | [out] | status | Pointer to sl_se_debug_status_t structure to be filled out with the current status of the debug configuration. | 
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
 
sl_se_apply_debug_lock#
sl_status_t sl_se_apply_debug_lock (sl_se_command_context_t * cmd_ctx)
Enables the debug lock for the part.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
The debug port will be closed and the only way to open it is through device erase (if enabled) or through secure debug unlock (if enabled).
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
 
sl_se_write_user_data#
sl_status_t sl_se_write_user_data (sl_se_command_context_t * cmd_ctx, uint32_t offset, void * data, uint32_t num_bytes)
Writes data to User Data section in MTP.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| uint32_t | [in] | offset | Offset to the flash word to write to. Must be aligned to words. | 
| void * | [in] | data | Data to write to flash. | 
| uint32_t | [in] | num_bytes | Number of bytes to write to flash. NB: Must be divisable by four. | 
Write data must be aligned to word size and contain a number of bytes that is divisable by four. Note
- It is recommended to erase the flash page before performing a write. 
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_OPERATIONwhen the SE command ID is not recognized
- SL_STATUS_INVALID_CREDENTIALSwhen the command is not authorized
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
 
sl_se_erase_user_data#
sl_status_t sl_se_erase_user_data (sl_se_command_context_t * cmd_ctx)
Erases User Data section in MTP.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_OPERATIONwhen the SE command ID is not recognized
- SL_STATUS_INVALID_CREDENTIALSwhen the command is not authorized
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
 
sl_se_get_status#
sl_status_t sl_se_get_status (sl_se_command_context_t * cmd_ctx, sl_se_status_t * status)
Returns the current boot status, versions and system configuration.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| sl_se_status_t * | [out] | status | SE_Status_t containing current SE status. | 
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKupon command completion. Errors are encoded in the different parts of the returned status object.
- SL_STATUS_INVALID_OPERATIONwhen the SE command ID is not recognized
- SL_STATUS_INVALID_CREDENTIALSwhen the command is not authorized
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
 
sl_se_get_serialnumber#
sl_status_t sl_se_get_serialnumber (sl_se_command_context_t * cmd_ctx, void * serial)
Read the serial number of the SE module.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| void * | [out] | serial | Pointer to array of size 16 bytes. | 
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_OPERATIONwhen the SE command ID is not recognized
- SL_STATUS_INVALID_CREDENTIALSwhen the command is not authorized
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
 
sl_se_get_reset_cause#
sl_status_t sl_se_get_reset_cause (sl_se_command_context_t * cmd_ctx, uint32_t * reset_cause)
Read the EMU->RSTCAUSE after a tamper reset.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| uint32_t * | [out] | reset_cause | Pointer to uint32_t word where reset cause shall be returned. | 
This function should be called if EMU->RSTCAUSE has been cleared upon boot.
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_OPERATIONwhen the SE command ID is not recognized
 
sl_se_get_tamper_reset_cause#
sl_status_t sl_se_get_tamper_reset_cause (sl_se_command_context_t * cmd_ctx, bool * was_tamper_reset, uint32_t * reset_cause)
Read the latest cached tamper reset cause.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| bool * | [out] | was_tamper_reset | Pointer to bool that indicates if a tamper event occurred. If the cached value is 0 this will be false, true otherwise. | 
| uint32_t * | [out] | reset_cause | Pointer to a uint32_t where the cached reset cause value should be returned. | 
The returned value is the index of the tamper source that caused a reset. Requires SE version 2.2.1 or above.
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_OPERATIONwhen the SE command ID is not recognized
- SL_STATUS_INVALID_PARAMETERwhen cmd_ctx or reset_cause is NULL
 
sl_se_enable_secure_debug#
sl_status_t sl_se_enable_secure_debug (sl_se_command_context_t * cmd_ctx)
Enables the secure debug functionality.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
Enables the secure debug functionality that can be used to open a locked debug port through the Get challenge and Open debug commands. This command can only be executed before the debug port is locked, and after a secure debug public key has been installed in the SE.
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
 
sl_se_disable_secure_debug#
sl_status_t sl_se_disable_secure_debug (sl_se_command_context_t * cmd_ctx)
Disables the secure debug functionality.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
Disables the secure debug functionality that can be used to open a locked debug port.
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
 
sl_se_set_debug_options#
sl_status_t sl_se_set_debug_options (sl_se_command_context_t * cmd_ctx, const sl_se_debug_options_t * debug_options)
Set debug options.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| const sl_se_debug_options_t * | [in] | debug_options | Pointer to debug options structure. | 
This function makes it possible to configure the Trust-Zone access permissions of the debug interface. For details please refer to sl_se_debug_options_t.
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
 
sl_se_erase_device#
sl_status_t sl_se_erase_device (sl_se_command_context_t * cmd_ctx)
Performs a device mass erase and debug unlock.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
Performs a device mass erase and resets the debug configuration to its initial unlocked state. Only available before DEVICE_ERASE_DISABLE has been executed.
Note
- This command clears and verifies the complete flash and ram of the system, excluding the user data pages and one-time programmable commissioning information in the secure engine. 
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_COMMANDif device erase is disabled.
 
sl_se_disable_device_erase#
sl_status_t sl_se_disable_device_erase (sl_se_command_context_t * cmd_ctx)
Disabled device erase functionality.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
This command disables the device erase command. It does not lock the debug interface to the part, but it is a permanent action for the part. If device erase is disabled and the device is debug locked, there is no way to permanently unlock the part. If secure debug unlock is enabled, secure debug unlock can still be used to temporarily open the debug port.
Warnings
- This command permanently disables the device erase functionality! 
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
 
sl_se_get_challenge#
sl_status_t sl_se_get_challenge (sl_se_command_context_t * cmd_ctx, sl_se_challenge_t challenge)
Request challenge from SE which can be used to open debug access.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| sl_se_challenge_t | [out] | challenge | SE challenge storage. | 
This command requests a challenge (16 bytes) which can be used to generate a certificate in order to open debug access, sl_se_open_debug.
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
 
sl_se_roll_challenge#
sl_status_t sl_se_roll_challenge (sl_se_command_context_t * cmd_ctx)
Invalidate current challenge and make a new challenge.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
This command requests the SE to invalidate it's current challenge (16bytes) and generate a new challenge.
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
 
sl_se_open_debug#
sl_status_t sl_se_open_debug (sl_se_command_context_t * cmd_ctx, void * cert, uint32_t len, const sl_se_debug_options_t * debug_options)
Unlock debug access using certificate and signed challenge.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| void * | [in] | cert | Certificate for debug unlock and signed challenge. | 
| uint32_t | [in] | len | Length of certificate in number of bytes. | 
| const sl_se_debug_options_t * | [in] | debug_options | Debug options to open/unlock. | 
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_OPERATIONwhen the SE command ID is not recognized
- SL_STATUS_INVALID_CREDENTIALSwhen the command is not authorized
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
 
sl_se_disable_tamper#
sl_status_t sl_se_disable_tamper (sl_se_command_context_t * cmd_ctx, void * cert, uint32_t len, sl_se_tamper_signals_t tamper_signals)
Temporarily disable tamper configuration using certificate and signed challenge.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| void * | [in] | cert | Certificate for disabling tamper and signed challenge. | 
| uint32_t | [in] | len | Length of certificate in number of bytes. | 
| sl_se_tamper_signals_t | [in] | tamper_signals | Tamper signals to disable. Each signal represented by a bit. | 
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_OPERATIONwhen the SE command ID is not recognized
- SL_STATUS_INVALID_CREDENTIALSwhen the command is not authorized
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
 
sl_se_read_cert_size#
sl_status_t sl_se_read_cert_size (sl_se_command_context_t * cmd_ctx, sl_se_cert_size_type_t * cert_size)
Read size of stored certificates in SE.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| sl_se_cert_size_type_t * | [inout] | cert_size | Size of the certificates stored in SE. | 
Returns
- Status code, sl_status.h. 
sl_se_read_cert#
sl_status_t sl_se_read_cert (sl_se_command_context_t * cmd_ctx, sl_se_cert_type_t cert_type, void * cert, uint32_t num_bytes)
Read stored certificates in SE.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
| sl_se_cert_type_t | [in] | cert_type | Type of the certificate stored in SE. | 
| void * | [inout] | cert | Buffer to read certificate. | 
| uint32_t | [in] | num_bytes | Length of certificate in number of bytes. | 
Returns
- Status code, status 
sl_se_enter_active_mode#
sl_status_t sl_se_enter_active_mode (sl_se_command_context_t * cmd_ctx)
Enter SE active mode.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
SE will enter active mode. This will ensure SE is not powered down between operations, at the expense of increased power consumption.
Warnings
- Active mode will prevent entry to EM2/3/4. To allow energy mode entry, exit active mode through sl_se_exit_active_mode(). 
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
- SL_STATUS_COMMAND_IS_INVALIDwhen already in active mode
 
sl_se_exit_active_mode#
sl_status_t sl_se_exit_active_mode (sl_se_command_context_t * cmd_ctx)
Exit SE active mode.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. | 
SE will exit active mode.
Returns
- One of the following sl_status_t codes: - SL_STATUS_OKwhen the command was executed successfully
- SL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
- SL_STATUS_COMMAND_IS_INVALIDwhen already not in active mode