Deprecated Functions#

Deprecated Functions.

Functions#

SE_readPubkey(uint32_t key_type, void *pubkey, uint32_t numBytes, bool signature)

Function Documentation#

SE_readPubkey#

SE_Response_t SE_readPubkey (uint32_t key_type, void * pubkey, uint32_t numBytes, bool signature)
Parameters
TypeDirectionArgument NameDescription
uint32_t[in]key_type

ID of key type to read.

void *[out]pubkey

Pointer to a buffer to contain the returned public key. Must be word aligned and have a length of 64 bytes.

uint32_t[in]numBytes

Length of pubkey buffer (64 bytes).

bool[in]signature

If true, the function will return the signature programmed for the specified public key instead of the public key itself.

Read pubkey or pubkey signature.

Read out a public key stored in the SE, or its signature. The command can be used to read:

  • SE_KEY_TYPE_BOOT

  • SE_KEY_TYPE_AUTH

Returns

  • One of the SE_RESPONSE return codes.

Return values

  • SE_RESPONSE_OK: when the command was executed successfully

  • SE_RESPONSE_TEST_FAILED: when the pubkey is not set

  • SE_RESPONSE_INVALID_PARAMETER: when an invalid type is passed