DALI Initialization structure.
Public Attributes#
bool
Enable the DALI low frequency mode.
Number of TX data bits in frame.
Number of RX data bits in frame.
General EUSART initialization structure.
Public Attribute Documentation#
dali_low_frequency_enable#
bool sl_hal_eusart_dali_config_t::dali_low_frequency_enable
Enable the DALI low frequency mode.
tx_data_bits#
sl_hal_eusart_dali_data_bits_t sl_hal_eusart_dali_config_t::tx_data_bits
Number of TX data bits in frame.
rx_data_bits#
sl_hal_eusart_dali_data_bits_t sl_hal_eusart_dali_config_t::rx_data_bits
Number of RX data bits in frame.
eusart_init#
sl_hal_eusart_uart_config_t sl_hal_eusart_dali_config_t::eusart_init
General EUSART initialization structure.