SPI Advanced initialization structure.

Public Attributes#

bool

Enable automatic chip select. CS is managed by the peripheral.

bool

If true, data will be sent with most significant bit first.

bool

Enable the automatic wake up from EM2 to EM1 for DMA RX operation.

bool

Enable AUTOTX mode.

bool

Force load the first FIFO value.

bool

Enable EUSART capability to use a PRS channel as an input data line for the receiver.

bool

Enable EUSART capability to use a PRS channel as an input SPI Clock.

uint8_t

PRS Channel used to transmit data from PRS to the EUSART.

uint8_t

Enable EUSART capability to use a PRS channel as an input SPI Clock.

uint8_t

Setup window in bus clock cycles before the sampling edge of SCLK at word-boundary to avoid force load error.

Enable inversion of RX and/or TX signals.

Auto CS setup time (before transmission) in baud cycles.

Auto CS hold time (after transmission) in baud cycles.

uint16_t

Default transmitted data when the TXFIFO is empty.

Interrupt and status level of the Receive FIFO.

Interrupt and status level of the Transmit FIFO.

Public Attribute Documentation#

auto_cs_enable#

bool sl_hal_eusart_spi_advanced_config_t::auto_cs_enable

Enable automatic chip select. CS is managed by the peripheral.


msb_first#

bool sl_hal_eusart_spi_advanced_config_t::msb_first

If true, data will be sent with most significant bit first.


dma_wakeup_on_rx#

bool sl_hal_eusart_spi_advanced_config_t::dma_wakeup_on_rx

Enable the automatic wake up from EM2 to EM1 for DMA RX operation.

Only applicable to EM2 (low frequency) capable EUSART instances.


auto_tx_enable#

bool sl_hal_eusart_spi_advanced_config_t::auto_tx_enable

Enable AUTOTX mode.

Transmits as long as the RX FIFO is not full. Generates underflow interrupt if the TX FIFO is empty.


force_load#

bool sl_hal_eusart_spi_advanced_config_t::force_load

Force load the first FIFO value.


prs_rx_enable#

bool sl_hal_eusart_spi_advanced_config_t::prs_rx_enable

Enable EUSART capability to use a PRS channel as an input data line for the receiver.

PRS channel and RX GPIO must be configured separately using PRS/GPIO API.


prs_clock_enable#

bool sl_hal_eusart_spi_advanced_config_t::prs_clock_enable

Enable EUSART capability to use a PRS channel as an input SPI Clock.

Slave mode only.


prs_rx_channel#

uint8_t sl_hal_eusart_spi_advanced_config_t::prs_rx_channel

PRS Channel used to transmit data from PRS to the EUSART.


prs_clock_channel#

uint8_t sl_hal_eusart_spi_advanced_config_t::prs_clock_channel

Enable EUSART capability to use a PRS channel as an input SPI Clock.

Slave mode only.


setup_window#

uint8_t sl_hal_eusart_spi_advanced_config_t::setup_window

Setup window in bus clock cycles before the sampling edge of SCLK at word-boundary to avoid force load error.


invert_io#

sl_hal_eusart_invert_io_t sl_hal_eusart_spi_advanced_config_t::invert_io

Enable inversion of RX and/or TX signals.


cs_polarity#

sl_hal_eusart_cs_polarity_t sl_hal_eusart_spi_advanced_config_t::cs_polarity

Chip select polarity.


auto_cs_setup_time#

sl_hal_eusart_cs_time_t sl_hal_eusart_spi_advanced_config_t::auto_cs_setup_time

Auto CS setup time (before transmission) in baud cycles.


auto_cs_hold_time#

sl_hal_eusart_cs_time_t sl_hal_eusart_spi_advanced_config_t::auto_cs_hold_time

Auto CS hold time (after transmission) in baud cycles.


auto_inter_frame_time#

sl_hal_eusart_inter_character_space_t sl_hal_eusart_spi_advanced_config_t::auto_inter_frame_time

Inter-frame time in baud cycles.


default_tx_data#

uint16_t sl_hal_eusart_spi_advanced_config_t::default_tx_data

Default transmitted data when the TXFIFO is empty.


rx_fifo_watermark#

sl_hal_eusart_fifo_interrupt_watermark_t sl_hal_eusart_spi_advanced_config_t::rx_fifo_watermark

Interrupt and status level of the Receive FIFO.


tx_fifo_watermark#

sl_hal_eusart_fifo_interrupt_watermark_t sl_hal_eusart_spi_advanced_config_t::tx_fifo_watermark

Interrupt and status level of the Transmit FIFO.