ADC - Analog to Digital Converter#
Introduction#
This module provides a hardware abstraction layer (HAL) interface to the ADC peripheral. It allows the user to initialize and configure the ADC to perform one or more conversions triggered immediately or continuously. The ADC stores its conversion results as a FIFO. Additionally, the ADC can be triggered by an external event or by a timer event.
For more details on the ADC initialization and configuration options available, please refer to the following structures and their corresponding attributes:
Example#
The following code snippet is an example of how to configure the ADC peripheral to perform a single immediate conversion:
{
// Enable ADC bus clock.
sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_ADC0);
// Get clock branch frequency to configure the ADC.
sl_clock_branch_t clock_branch;
uint32_t branch_clock_freq;
clock_branch = sl_device_peripheral_get_clock_branch(SL_PERIPHERAL_ADC0);
sl_clock_manager_get_clock_branch_frequency(clock_branch, &branch_clock_freq);
sl_hal_adc_scan_entry_t entry = SL_HAL_ADC_SCAN_ENTRY_DEFAULT;
entry.pos_port = SL_HAL_ADC_PORT_POS_PORTA;
entry.pos_pin = 0;
sl_hal_adc_init_t init = SL_HAL_ADC_INIT_DEFAULT;
init.scan_trigger = SL_HAL_ADC_TRIGGER_IMMEDIATE;
init.scan_trigger_action = SL_HAL_ADC_TRIGGER_ACTION_ONCE;
sl_hal_adc_config_t config = SL_HAL_ADC_CONFIG_DEFAULT;
config.acquisition_time = 16;
init.entries[SL_HAL_ADC_CHANNEL_ID_0] = entry;
sl_hal_adc_reset(ADC0);
sl_hal_adc_enable_interrupts(ADC0, ADC_IF_SCANENTRYDONE);
init.config[SL_HAL_ADC_CONFIG_ID_0] = config;
sl_hal_adc_init(ADC0, &init, branch_clock_freq);
sl_hal_adc_enable(ADC0);
sl_hal_adc_flush_fifo(ADC0);
while (sl_hal_adc_get_status(ADC0) & ADC_STATUS_SCANFIFOFLUSHING) ;
uint32_t scan_mask = 1U << SL_HAL_ADC_CONFIG_ID_0;
sl_hal_adc_set_scan_mask(ADC0, scan_mask);
sl_hal_adc_result_t result;
// Trigger scan and pull results from fifo.
sl_hal_adc_start(ADC0);
while (!sl_hal_adc_get_enabled_pending_interrupts(ADC0)) ;
result = sl_hal_adc_pull(ADC0);
sl_hal_adc_clear_interrupts(ADC0, ADC_IF_SCANENTRYDONE);
}
Hardware Limitations and Workarounds#
Continuous Single Channel Conversion Generates Invalid Accumulation Results#
Description#
When the ADC continuously scans a single channel under certain conditions, the conversion results are incorrectly accumulated.
The conversion result is invalid if all of the following conditions are met:
One channel is being converted in the scan sequence.
ADC is performing continuous conversions
ADC init structure's
scan_trigger_actionis set toSL_HAL_ADC_TRIGGER_ACTION_CONTINUOUS.
ADC is accumulating 4 or more conversions per output
ADC configuration structure's
averageis set toSL_HAL_ADC_AVERAGE_X4or higher.
Scan repetition delay is disabled
ADC init structure's
repetition_delayis set toSL_HAL_ADC_DELAY_NO.
The internal ADC clocks CLK_CORE_ADC and CLK_SRC_ADC are equal
The prescaler
adcprescaleis set to 0 (divide by 1).If sl_hal_adc_set_clock_prescalers is not set explicitly after initializing the ADC with sl_hal_adc_init, the default prescaler values will be calculated by sl_hal_adc_init based on the branch clock frequency.
Workaround#
There are two workarounds:
Enable scan repetition delay by setting the ADC init structure's
repetition_delayto any option other thanSL_HAL_ADC_DELAY_NO.Configure CLK_SRC_ADC to be twice the frequency of CLK_CORE_ADC
By setting
adcprescaleto 1 explicitly with the sl_hal_adc_set_clock_prescalers function.Or by using a branch clock frequency of 34 - 40Mhz, 68 - 80Mhz, 102 - 120Mhz or 136 - 160Mhz, when calling sl_hal_adc_init to guarantee that the calculated
adcprescaleis 1 (See the note in sl_hal_adc_init).
Modules#
Enumerations#
Warm-up mode.
Voltage reference.
First clock divider.
ADC scan trigger.
ADC scan trigger action.
Delay value between one sequence of the table and the next start of sequence.
Analog gain.
Number of samples used for averaging.
Alignment of output data written into FIFO.
Data valid level before requesting DMA transfer.
Port (A, B, C, D) or special signal assigned to the negative input of the ADC.
Port (A, B, C, D) or special signal assigned to the positive input of the ADC.
Configuration identifier.
Channel identifier.
Functions#
Initialize the ADC.
Reset the ADC.
Set a new Scan Table mask.
Get the working scan table mask.
Update an entry in the scan table.
Pull the value at the top of the FIFO.
Peek at the top of the FIFO without removing the data.
Get the ADC's current FIFO count.
Get the ADC's internal reference voltage in millivolts.
Calculate and return the clock frequency of the ADC's local timer.
Set the timer period to periodically trigger a timer event.
Set both ADC prescalers.
Enable the ADC.
Disable the ADC.
Start the ADC.
Stop the ADC.
Enable the ADC's local timer.
Disable the ADC's local timer and resets the counter.
Flush the scan FIFO.
Wait for ongoing sync of register(s) to the low-frequency domain to complete.
Wait for disabling to finish.
Return the content of the status register.
Enable one or more ADC interrupts.
Disable one or more ADC interrupts.
Clear one or more pending ADC interrupts.
Set one or more pending ADC interrupts from software.
Get pending ADC interrupt flags.
Get enabled and pending ADC interrupt flags.
Macros#
Validation of the ADC register block pointer reference for assert statements.
Default ADC initialization structure.
Default ADC config structure.
Default ADC scan entry structure.
Enumeration Documentation#
sl_hal_adc_warmup_mode_t#
sl_hal_adc_warmup_mode_t
Warm-up mode.
| Enumerator | |
|---|---|
| SL_HAL_ADC_WARMUP_NORMAL | Shut down the ADC after conversions have completed. |
| SL_HAL_ADC_WARMUP_KEEPWARM | Keep the ADC fully powered after conversions have completed. |
| SL_HAL_ADC_WARMUP_KEEPSTANDBY | Allow the ADC to have 1us warmup instead of 5us after the first conversion. |
sl_hal_adc_voltage_reference_t#
sl_hal_adc_voltage_reference_t
Voltage reference.
| Enumerator | |
|---|---|
| SL_HAL_ADC_REFERENCE_VREFINT | Internal voltage reference. |
| SL_HAL_ADC_REFERENCE_VREFPL | External reference pin low voltage (1.05-1.25). |
| SL_HAL_ADC_REFERENCE_VREFPH | External reference pin high voltage (>1.25). |
| SL_HAL_ADC_REFERENCE_VDDA | Analog voltage supply. |
| SL_HAL_ADC_REFERENCE_VREFPBUF | External reference pin buffered. |
sl_hal_adc_high_speed_clock_rate_t#
sl_hal_adc_high_speed_clock_rate_t
First clock divider.
| Enumerator | |
|---|---|
| SL_HAL_ADC_HSCLKRATE_DIV1 | Use clk_per directly. |
| SL_HAL_ADC_HSCLKRATE_DIV2 | Divide clk_per by 2. |
| SL_HAL_ADC_HSCLKRATE_DIV3 | Divide clk_per by 3. |
| SL_HAL_ADC_HSCLKRATE_DIV4 | Divide clk_per by 4. |
| SL_HAL_ADC_HSCLKRATE_DIV5 | Divide clk_per by 5. |
| SL_HAL_ADC_HSCLKRATE_DIV6 | Divide clk_per by 6. |
| SL_HAL_ADC_HSCLKRATE_DIV7 | Divide clk_per by 7. |
| SL_HAL_ADC_HSCLKRATE_DIV8 | Divide clk_per by 8. |
sl_hal_adc_trigger_t#
sl_hal_adc_trigger_t
ADC scan trigger.
| Enumerator | |
|---|---|
| SL_HAL_ADC_TRIGGER_IMMEDIATE | Start scan queue immediately. |
| SL_HAL_ADC_TRIGGER_TIMER | Timer starts scan queue. |
| SL_HAL_ADC_TRIGGER_PRSCLKGRP | PRS0 from timer in same clock group starts scan queue. |
| SL_HAL_ADC_TRIGGER_PRSPOS | PRS0 positive edge starts scan queue. |
| SL_HAL_ADC_TRIGGER_PRSNEG | PRS0 negative edge starts scan queue. |
sl_hal_adc_trigger_action_t#
sl_hal_adc_trigger_action_t
ADC scan trigger action.
| Enumerator | |
|---|---|
| SL_HAL_ADC_TRIGGER_ACTION_ONCE | Once per trigger. |
| SL_HAL_ADC_TRIGGER_ACTION_CONTINUOUS | Continuously after trigger. |
sl_hal_adc_repetition_delay_t#
sl_hal_adc_repetition_delay_t
Delay value between one sequence of the table and the next start of sequence.
| Enumerator | |
|---|---|
| SL_HAL_ADC_DELAY_NO | No delay. |
| SL_HAL_ADC_DELAY_CYCLES_2 | 2 conversion clock cycles. |
| SL_HAL_ADC_DELAY_CYCLES_4 | 4 conversion clock cycles. |
| SL_HAL_ADC_DELAY_CYCLES_8 | 8 conversion clock cycles. |
| SL_HAL_ADC_DELAY_CYCLES_16 | 16 conversion clock cycles. |
| SL_HAL_ADC_DELAY_CYCLES_32 | 32 conversion clock cycles. |
| SL_HAL_ADC_DELAY_CYCLES_64 | 64 conversion clock cycles. |
| SL_HAL_ADC_DELAY_CYCLES_128 | 128 conversion clock cycles. |
| SL_HAL_ADC_DELAY_CYCLES_256 | 256 conversion clock cycles. |
| SL_HAL_ADC_DELAY_CYCLES_512 | 512 conversion clock cycles. |
| SL_HAL_ADC_DELAY_CYCLES_1024 | 1024 conversion clock cycles. |
sl_hal_adc_analog_gain_t#
sl_hal_adc_analog_gain_t
Analog gain.
| Enumerator | |
|---|---|
| SL_HAL_ADC_ANALOG_GAIN_0_3125 | Gain for sampling cap of 0.3125x. |
| SL_HAL_ADC_ANALOG_GAIN_0_5 | Gain for sampling cap of 0.5x. |
| SL_HAL_ADC_ANALOG_GAIN_1 | Gain for sampling cap of 1x. |
| SL_HAL_ADC_ANALOG_GAIN_2 | Gain for sampling cap of 2x. |
| SL_HAL_ADC_ANALOG_GAIN_4 | Gain for sampling cap of 3x. |
sl_hal_adc_samples_t#
sl_hal_adc_samples_t
Number of samples used for averaging.
| Enumerator | |
|---|---|
| SL_HAL_ADC_AVERAGE_X1 | 1 sample for each conversion result. |
| SL_HAL_ADC_AVERAGE_X2 | 2 samples for each conversion result. |
| SL_HAL_ADC_AVERAGE_X4 | 4 samples for each conversion result. |
| SL_HAL_ADC_AVERAGE_X8 | 8 samples for each conversion result. |
| SL_HAL_ADC_AVERAGE_X16 | 16 samples for each conversion result. |
| SL_HAL_ADC_AVERAGE_X32 | 32 samples for each conversion result. |
| SL_HAL_ADC_AVERAGE_X64 | 64 samples for each conversion result. |
| SL_HAL_ADC_AVERAGE_X128 | 128 samples for each conversion result. |
| SL_HAL_ADC_AVERAGE_X256 | 256 samples for each conversion result. |
| SL_HAL_ADC_AVERAGE_X512 | 512 samples for each conversion result. |
| SL_HAL_ADC_AVERAGE_X1024 | 1024 samples for each conversion result. |
sl_hal_adc_alignment_t#
sl_hal_adc_alignment_t
Alignment of output data written into FIFO.
| Enumerator | |
|---|---|
| SL_HAL_ADC_ALIGNMENT_RIGHT_16 | ID[7:0], SIGN_EXT, DATA[15:0]. |
| SL_HAL_ADC_ALIGNMENT_RIGHT_12 | ID[7:0], SIGN_EXT, DATA[11:0]. |
| SL_HAL_ADC_ALIGNMENT_RIGHT_8 | ID[7:0], SIGN_EXT, DATA[7:0]. |
| SL_HAL_ADC_ALIGNMENT_LEFT_16 | DATA[15:0], 00000000, ID[7:0]. |
| SL_HAL_ADC_ALIGNMENT_LEFT_12 | DATA[11:0], 000000000000, ID[7:0]. |
| SL_HAL_ADC_ALIGNMENT_LEFT_8 | DATA[7:0], 0000000000000000, ID[7:0]. |
sl_hal_adc_data_valid_t#
sl_hal_adc_data_valid_t
Data valid level before requesting DMA transfer.
| Enumerator | |
|---|---|
| SL_HAL_ADC_DATA_VALID_1 | 1 valid entry to set SCANFIFODVL interrupt. |
| SL_HAL_ADC_DATA_VALID_2 | 2 valid entries to set SCANFIFODVL interrupt. |
| SL_HAL_ADC_DATA_VALID_3 | 3 valid entries to set SCANFIFODVL interrupt. |
| SL_HAL_ADC_DATA_VALID_4 | 4 valid entries to set SCANFIFODVL interrupt. |
| SL_HAL_ADC_DATA_VALID_5 | 5 valid entries to set SCANFIFODVL interrupt. |
| SL_HAL_ADC_DATA_VALID_6 | 6 valid entries to set SCANFIFODVL interrupt. |
| SL_HAL_ADC_DATA_VALID_7 | 7 valid entries to set SCANFIFODVL interrupt. |
| SL_HAL_ADC_DATA_VALID_8 | 8 valid entries to set SCANFIFODVL interrupt. |
| SL_HAL_ADC_DATA_VALID_9 | 9 valid entries to set SCANFIFODVL interrupt. |
| SL_HAL_ADC_DATA_VALID_10 | 10 valid entries to set SCANFIFODVL interrupt. |
| SL_HAL_ADC_DATA_VALID_11 | 11 valid entries to set SCANFIFODVL interrupt. |
| SL_HAL_ADC_DATA_VALID_12 | 12 valid entries to set SCANFIFODVL interrupt. |
| SL_HAL_ADC_DATA_VALID_13 | 13 valid entries to set SCANFIFODVL interrupt. |
| SL_HAL_ADC_DATA_VALID_14 | 14 valid entries to set SCANFIFODVL interrupt. |
| SL_HAL_ADC_DATA_VALID_15 | 15 valid entries to set SCANFIFODVL interrupt. |
| SL_HAL_ADC_DATA_VALID_16 | 16 valid entries to set SCANFIFODVL interrupt. |
sl_hal_adc_port_negative_t#
sl_hal_adc_port_negative_t
Port (A, B, C, D) or special signal assigned to the negative input of the ADC.
| Enumerator | |
|---|---|
| SL_HAL_ADC_PORT_NEG_GND | Ground. |
| SL_HAL_ADC_PORT_NEG_PORTA | Port A. |
| SL_HAL_ADC_PORT_NEG_PORTB | Port B. |
| SL_HAL_ADC_PORT_NEG_PORTC | Port C. |
| SL_HAL_ADC_PORT_NEG_PORTD | Port D. |
sl_hal_adc_port_positive_t#
sl_hal_adc_port_positive_t
Port (A, B, C, D) or special signal assigned to the positive input of the ADC.
| Enumerator | |
|---|---|
| SL_HAL_ADC_PORT_POS_GND | Ground. |
| SL_HAL_ADC_PORT_POS_SUPPLY | Supply. |
| SL_HAL_ADC_PORT_POS_PORTA | Port A. |
| SL_HAL_ADC_PORT_POS_PORTB | Port B. |
| SL_HAL_ADC_PORT_POS_PORTC | Port C. |
| SL_HAL_ADC_PORT_POS_PORTD | Port D. |
sl_hal_adc_config_id_t#
sl_hal_adc_config_id_t
Configuration identifier.
| Enumerator | |
|---|---|
| SL_HAL_ADC_CONFIG_ID_0 | |
| SL_HAL_ADC_CONFIG_ID_1 | |
| SL_HAL_ADC_CONFIG_ID_MAX | |
sl_hal_adc_channel_id_t#
sl_hal_adc_channel_id_t
Channel identifier.
| Enumerator | |
|---|---|
| SL_HAL_ADC_CHANNEL_ID_0 | |
| SL_HAL_ADC_CHANNEL_ID_1 | |
| SL_HAL_ADC_CHANNEL_ID_2 | |
| SL_HAL_ADC_CHANNEL_ID_3 | |
| SL_HAL_ADC_CHANNEL_ID_4 | |
| SL_HAL_ADC_CHANNEL_ID_5 | |
| SL_HAL_ADC_CHANNEL_ID_6 | |
| SL_HAL_ADC_CHANNEL_ID_7 | |
| SL_HAL_ADC_CHANNEL_ID_8 | |
| SL_HAL_ADC_CHANNEL_ID_9 | |
| SL_HAL_ADC_CHANNEL_ID_10 | |
| SL_HAL_ADC_CHANNEL_ID_11 | |
| SL_HAL_ADC_CHANNEL_ID_12 | |
| SL_HAL_ADC_CHANNEL_ID_13 | |
| SL_HAL_ADC_CHANNEL_ID_14 | |
| SL_HAL_ADC_CHANNEL_ID_15 | |
| SL_HAL_ADC_CHANNEL_ID_MAX | |
Function Documentation#
sl_hal_adc_init#
void sl_hal_adc_init (ADC_TypeDef * adc, const sl_hal_adc_init_t * init, uint32_t branch_clock_freq)
Initialize the ADC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
| const sl_hal_adc_init_t * | [in] | init | A pointer to the ADC initialization structure. |
| uint32_t | [in] | branch_clock_freq | Incoming peripheral frequency. Should be retrieved using the Clock Manager service. |
Note
The ADC peripheral's internal clock prescalers and timebase will be set to sensible defaults according to the input parameter branch_clock_freq provided. These default prescalers can be modified using sl_hal_adc_set_clock_prescalers. The branch_clock_freq can be obtained for adc0 using the Device Manager and Clock Manager services as such:
{ #include "sl_clock_manager.h" #include "sl_device_peripheral.h" sl_clock_branch_t clock_branch; clock_branch = sl_device_peripheral_get_clock_branch(SL_PERIPHERAL_ADC0); uint32_t branch_clock_freq; sl_clock_manager_get_clock_branch_frequency(clock_branch, &branch_clock_freq); }For SiXG301, due to hardware limitations, the ADC cannot be configured for hardware averaging if the adcprescale is 0 (divide by 1). If hardware averaging is desired, then an adc0 branch_clock_freq of 34 - 40Mhz, 68 - 80Mhz, 102 - 120Mhz or 136 - 160Mhz can be used to guarantee that the calculated adcprescale is 1.
sl_hal_adc_reset#
void sl_hal_adc_reset (ADC_TypeDef * adc)
Reset the ADC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
sl_hal_adc_set_scan_mask#
void sl_hal_adc_set_scan_mask (ADC_TypeDef * adc, uint32_t mask)
Set a new Scan Table mask.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
| uint32_t | [in] | mask | New scan table mask. |
Note
The working scan table is updated when it's not being scanned. Each bit in the mask corresponds to a given ADC channel, and setting a given bit to 1 will enable the conversion of the respective ADC channel.
sl_hal_adc_get_scan_mask#
uint32_t sl_hal_adc_get_scan_mask (ADC_TypeDef * adc)
Get the working scan table mask.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
Returns
The working scan table mask.
sl_hal_adc_update_scan_entry#
void sl_hal_adc_update_scan_entry (ADC_TypeDef * adc, uint8_t id, const sl_hal_adc_scan_entry_t * entry)
Update an entry in the scan table.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
| uint8_t | [in] | id | ID of scan table entry to add. |
| const sl_hal_adc_scan_entry_t * | [in] | entry | A pointer to a Scan Table entry structure. |
sl_hal_adc_pull#
sl_hal_adc_result_t sl_hal_adc_pull (const ADC_TypeDef * adc)
Pull the value at the top of the FIFO.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
FIFO count reduced.
Returns
The data at the top of the FIFO.
sl_hal_adc_peek#
sl_hal_adc_result_t sl_hal_adc_peek (const ADC_TypeDef * adc)
Peek at the top of the FIFO without removing the data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
Returns
The data at the top of the FIFO.
Note
The FIFO's count remains unchanged.
sl_hal_adc_get_fifo_count#
uint32_t sl_hal_adc_get_fifo_count (const ADC_TypeDef * adc)
Get the ADC's current FIFO count.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
Returns
The ADC's current FIFO count.
sl_hal_adc_get_internal_reference_voltage#
uint32_t sl_hal_adc_get_internal_reference_voltage (const ADC_TypeDef * adc)
Get the ADC's internal reference voltage in millivolts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
Returns
The ADC's internal reference voltage in millivolts.
sl_hal_adc_get_timer_frequency#
uint32_t sl_hal_adc_get_timer_frequency (const ADC_TypeDef * adc, uint32_t branch_clock_freq)
Calculate and return the clock frequency of the ADC's local timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
| uint32_t | [in] | branch_clock_freq | Incoming peripheral frequency. Should be retrieved using the Clock Manager service. |
Returned value is based on the clock branch selected for the ADC peripheral and the current hsclkrate prescaler.
Returns
The clock frequency of the ADC's local timer.
Note
The local timer can be used to trigger conversions periodically by setting the timer period with sl_hal_adc_set_timer_period.
The branch_clock_freq can be obtained for adc0 using the Device Manager and Clock Manager services as such:
#include "sl_clock_manager.h"
#include "sl_device_peripheral.h"
sl_clock_branch_t clock_branch;
clock_branch = sl_device_peripheral_get_clock_branch(SL_PERIPHERAL_ADC0);
uint32_t branch_clock_freq;
sl_clock_manager_get_clock_branch_frequency(clock_branch, &branch_clock_freq);
sl_hal_adc_set_timer_period#
void sl_hal_adc_set_timer_period (ADC_TypeDef * adc, uint16_t timer_period)
Set the timer period to periodically trigger a timer event.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
| uint16_t | [in] | timer_period | The number of clock cycles between ADC timer events. |
Timer events can be used to trigger an ADC scan.
Note
The ADC's local timer must be disabled before calling this function.
sl_hal_adc_set_clock_prescalers#
void sl_hal_adc_set_clock_prescalers (ADC_TypeDef * adc, uint32_t branch_clock_freq, uint8_t hsclkrate, uint8_t adcprescale)
Set both ADC prescalers.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
| uint32_t | [in] | branch_clock_freq | Incoming peripheral frequency. Should be retrieved using the Clock Manager service. |
| uint8_t | [in] | hsclkrate | This prescaler divides the branch clock frequency and the resulting clock is ADC_SRC_CLK. This clocks the ADC peripheral's local timer. The value can be set to an integer value from 0 to 5. The branch clock frequency is divided by (hsclkrate + 1). ADC_SRC_CLK must be less than 40MHz. |
| uint8_t | [in] | adcprescale | This prescaler divides the ADC_SRC_CLK and the resulting clock is ADC_CORE_CLK. This clocks the core functionality of the ADC peripheral. The value can be set to 0 (no divider) or 1 (divide by 2). The operating frequency of ADC_CORE_CLK is between 17MHz and 22MHz. |
Re-calculates and updates the timebase.
Note
The ADC must be disabled before making changes to the clock prescalers. The branch_clock_freq can be obtained for adc0 using the Device Manager and Clock Manager services as such:
{ #include "sl_clock_manager.h" #include "sl_device_peripheral.h" sl_clock_branch_t clock_branch; clock_branch = sl_device_peripheral_get_clock_branch(SL_PERIPHERAL_ADC0); uint32_t branch_clock_freq; sl_clock_manager_get_clock_branch_frequency(clock_branch, &branch_clock_freq); }
sl_hal_adc_enable#
void sl_hal_adc_enable (ADC_TypeDef * adc)
Enable the ADC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
sl_hal_adc_disable#
void sl_hal_adc_disable (ADC_TypeDef * adc)
Disable the ADC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
sl_hal_adc_start#
void sl_hal_adc_start (ADC_TypeDef * adc)
Start the ADC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
Note
Enables the scan sequence and will start a scan if using the immediate trigger mode.
sl_hal_adc_stop#
void sl_hal_adc_stop (ADC_TypeDef * adc)
Stop the ADC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
sl_hal_adc_enable_timer#
void sl_hal_adc_enable_timer (ADC_TypeDef * adc)
Enable the ADC's local timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
sl_hal_adc_disable_timer#
void sl_hal_adc_disable_timer (ADC_TypeDef * adc)
Disable the ADC's local timer and resets the counter.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
sl_hal_adc_flush_fifo#
void sl_hal_adc_flush_fifo (ADC_TypeDef * adc)
Flush the scan FIFO.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
Note
The ADC must be enabled. The operation is completed when SCANFIFOFLUSHING STATUS bit is low. The Scan queue should be disabled. Any incoming scan queue data will be discarded during the flush.
sl_hal_adc_wait_sync#
void sl_hal_adc_wait_sync (ADC_TypeDef * adc)
Wait for ongoing sync of register(s) to the low-frequency domain to complete.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
sl_hal_adc_wait_ready#
void sl_hal_adc_wait_ready (ADC_TypeDef * adc)
Wait for disabling to finish.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
sl_hal_adc_get_status#
uint32_t sl_hal_adc_get_status (ADC_TypeDef * adc)
Return the content of the status register.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | A pointer to the ADC peripheral register block. |
Returns
Status register.
sl_hal_adc_enable_interrupts#
void sl_hal_adc_enable_interrupts (ADC_TypeDef * adc, uint32_t flags)
Enable one or more ADC interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | Pointer to the ADC peripheral register block. |
| uint32_t | [in] | flags | Pending ADC interrupt source to enable. Use a bitwise logic OR combination of valid interrupt flags for ADC module (ADC_IEN_nnn). |
sl_hal_adc_disable_interrupts#
void sl_hal_adc_disable_interrupts (ADC_TypeDef * adc, uint32_t flags)
Disable one or more ADC interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | Pointer to the ADC peripheral register block. |
| uint32_t | [in] | flags | Pending ADC interrupt source to disable. Use a bitwise logic OR combination of valid interrupt flags for ADC module (ADC_IEN_nnn). |
sl_hal_adc_clear_interrupts#
void sl_hal_adc_clear_interrupts (ADC_TypeDef * adc, uint32_t flags)
Clear one or more pending ADC interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | Pointer to the ADC peripheral register block. |
| uint32_t | [in] | flags | Pending ADC interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for ADC module (ADC_IEN_nnn). |
sl_hal_adc_set_interrupts#
void sl_hal_adc_set_interrupts (ADC_TypeDef * adc, uint32_t flags)
Set one or more pending ADC interrupts from software.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | Pointer to the ADC peripheral register block. |
| uint32_t | [in] | flags | Interrupt source(s) to set to pending. Use a bitwise logic OR combination of valid interrupt flags for ADC module (ADC_IEN_nnn). |
sl_hal_adc_get_pending_interrupts#
uint32_t sl_hal_adc_get_pending_interrupts (ADC_TypeDef * adc)
Get pending ADC interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | Pointer to the ADC peripheral register block. |
Returns
Pending ADC interrupt sources.
sl_hal_adc_get_enabled_pending_interrupts#
uint32_t sl_hal_adc_get_enabled_pending_interrupts (ADC_TypeDef * adc)
Get enabled and pending ADC interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ADC_TypeDef * | [in] | adc | Pointer to the ADC peripheral register block. |
Useful for handling more interrupt sources in the same interrupt handler.
Returns
Pending and enabled ADC interrupt sources.
Macro Definition Documentation#
SL_HAL_ADC_REF_VALID#
#define SL_HAL_ADC_REF_VALIDValue:
(ref)
Validation of the ADC register block pointer reference for assert statements.
SL_HAL_ADC_INIT_DEFAULT#
#define SL_HAL_ADC_INIT_DEFAULTValue:
Default ADC initialization structure.
SL_HAL_ADC_CONFIG_DEFAULT#
#define SL_HAL_ADC_CONFIG_DEFAULTValue:
Default ADC config structure.
SL_HAL_ADC_SCAN_ENTRY_DEFAULT#
#define SL_HAL_ADC_SCAN_ENTRY_DEFAULTValue:
Default ADC scan entry structure.