ACMP initialization structure.
Public Attributes#
uint32_t
Controls the bias current.
uint32_t
Controls the VDD division factor. VREFOUT = VREFIN * (VREFDIV / 63).
Selects the input range.
Selects the ACMP accuracy mode.
Selects the hysteresis level on rising edge.
Selects the hysteresis level on falling edge.
bool
Inactive value emitted by ACMP during warmup.
Public Attribute Documentation#
vref_div#
uint32_t sl_hal_acmp_init_t::vref_div
Controls the VDD division factor. VREFOUT = VREFIN * (VREFDIV / 63).
hysteresis_rise#
sl_hal_acmp_hysteresis_t sl_hal_acmp_init_t::hysteresis_rise
Selects the hysteresis level on rising edge.
hysteresis_fall#
sl_hal_acmp_hysteresis_t sl_hal_acmp_init_t::hysteresis_fall
Selects the hysteresis level on falling edge.