LESENSE timing control descriptor structure.

Public Attributes#

uint8_t

Set number of LFACLK cycles to delay sensor interaction on each channel. Valid range: 0-3 (2 bit).

bool

Set to true to delay startup of AUXHFRCO until the system enters excite phase.

Public Attribute Documentation#

start_delay#

uint8_t sl_hal_lesense_timing_descriptor_t::start_delay

Set number of LFACLK cycles to delay sensor interaction on each channel. Valid range: 0-3 (2 bit).


delay_aux_startup#

bool sl_hal_lesense_timing_descriptor_t::delay_aux_startup

Set to true to delay startup of AUXHFRCO until the system enters excite phase.

This will reduce the time AUXHFRCO is enabled and reduce power usage.