Static Token Key Space Regions#
MACRO's for Static Token Key Space Regions.
Applicable for both static device and static secure tokens for series 3 devices.
CTM has reserved dedicated token key ranges for each domain, with a total of 128 token keys allocated per domain. The token key ranges are defined as follows:
0x000 to 0x07F used for defining tokens for the Common domain.
0x080 to 0x0FF used for defining tokens for the Zigbee domain.
0x100 to 0x17F used for defining tokens for the Thread domain.
0x180 to 0x1FF used for defining tokens for the Connect domain.
0x200 to 0x27F used for defining tokens for the Bluetooth domain.
0x280 to 0x2FF used for defining tokens for the Z-Wave domain.
0x300 to 0x37F used for defining tokens for the Bluetooth Mesh domain.
0x380 to 0x3FF used for defining tokens for the Matter domain.
0x400 to 0x47F used for defining tokens for the Wi-Sun domain.
0x480 to 0x4FF used for defining tokens for the Sidewalk domain.
0x500 to 0x57F used for defining tokens for the Wi-Fi domain.
0x580 to 0x5FF reserved for future use.
0x600 to 0x67F used for defining tokens for the User domain.
0x680 to 0xFFF reserved for future use.
A new token added for series 3 devices must follow the domain-specific token Id ranges mentioned above. And the new tokens must not conflict with the existing tokens. Below is an example of how to define a new token:
@code{.c}
// Defining a new static device token for the Matter domain:
#define TOKEN_MFG_MATTER_NEW_STATIC_DEVICE_TOKEN (SL_TOKEN_STATIC_DEVICE_TOKENS | SL_TOKEN_DOMAIN_STATIC_MATTER | 0x0)
#define TOKEN_MFG_MATTER_NEW_STATIC_DEVICE_TOKEN_SIZE (2u) // 2 bytes
// Defining a new static secure token for the Matter domain:
#define TOKEN_MFG_MATTER_NEW_STATIC_SECURE_TOKEN (SL_TOKEN_STATIC_SECURE_DATA_TOKENS | SL_TOKEN_DOMAIN_STATIC_MATTER | 0x0)
#define TOKEN_MFG_MATTER_NEW_STATIC_SECURE_TOKEN_SIZE (2u) // 2 bytes
@endcode
Note
The token IDs listed below are reserved and must not be used to define tokens for any specific domain. For example, the token TOKEN_MFG_CTUNE (a static device token) is reserved with Id 0x100 and must not be reused to define a static device token for the Thread domain. Similarly, the token TOKEN_MFG_CBKE_DATA (a static secure token) is reserved with Id 0x204 and must not be reused to define a static secure token for the Bluetooth domain. These reservations exist because there are already deployed devices using these token Id values, which are distributed across the overall token Id space. Reusing these Id's would create compatibility issues with existing devices.
Reserved token IDs by type (do not use below IDs for defining new tokens for the respective domains):
Static device token (Domain : Token IDs)
Static secure token (Domain : Token IDs)
Common : 0x002, 0x00C, 0x020, 0x030, 0x034, 0x038, 0x064
Bluetooth : 0x204, 0x260, 0x270
Zigbee : 0x09C
Z-Wave : 0x298
Thread : 0x100
Connect : 0x1f0
Macros#
Macro Definition Documentation#
SL_TOKEN_DOMAIN_STATIC_COMMON#
#define SL_TOKEN_DOMAIN_STATIC_COMMONValue:
(0x000)
Static Token Domain for Common tokens.
SL_TOKEN_DOMAIN_STATIC_ZIGBEE#
#define SL_TOKEN_DOMAIN_STATIC_ZIGBEEValue:
(0x080)
Static Token Domain for Zigbee tokens.
SL_TOKEN_DOMAIN_STATIC_THREAD#
#define SL_TOKEN_DOMAIN_STATIC_THREADValue:
(0x100)
Static Token Domain for Thread tokens.
SL_TOKEN_DOMAIN_STATIC_CONNECT#
#define SL_TOKEN_DOMAIN_STATIC_CONNECTValue:
(0x180)
Static Token Domain for Connect tokens.
SL_TOKEN_DOMAIN_STATIC_BT#
#define SL_TOKEN_DOMAIN_STATIC_BTValue:
(0x200)
Static Token Domain for Bluetooth tokens.
SL_TOKEN_DOMAIN_STATIC_ZWAVE#
#define SL_TOKEN_DOMAIN_STATIC_ZWAVEValue:
(0x280)
Static Token Domain for Z-Wave tokens.
SL_TOKEN_DOMAIN_STATIC_BT_MESH#
#define SL_TOKEN_DOMAIN_STATIC_BT_MESHValue:
(0x300)
Static Token Domain for Bluetooth Mesh tokens.
SL_TOKEN_DOMAIN_STATIC_MATTER#
#define SL_TOKEN_DOMAIN_STATIC_MATTERValue:
(0x380)
Static Token Domain for Matter tokens.
SL_TOKEN_DOMAIN_STATIC_WI_SUN#
#define SL_TOKEN_DOMAIN_STATIC_WI_SUNValue:
(0x400)
Static Token Domain for Wi-Sun tokens.
SL_TOKEN_DOMAIN_STATIC_SIDEWALK#
#define SL_TOKEN_DOMAIN_STATIC_SIDEWALKValue:
(0x480)
Static Token Domain for Sidewalk tokens.
SL_TOKEN_DOMAIN_STATIC_WI_FI#
#define SL_TOKEN_DOMAIN_STATIC_WI_FIValue:
(0x500)
Static Token Domain for Wi-Fi tokens.
SL_TOKEN_DOMAIN_STATIC_USER#
#define SL_TOKEN_DOMAIN_STATIC_USERValue:
(0x600)
Static Token Domain for User tokens.