Simplicity SDK Platform - Bootloader Version 3.3.2 - Release Notes (Oct 14, 2026)#
Simplicity SDK Platform Version 6.1.2
The Gecko Bootloader is a common bootloader framework used across modern Silicon Labs MCUs and wireless SoCs. It offers configurable features such as device initialization and secure firmware updates.
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Added in 3.3.2#
None
Added in 3.3.1#
None
Added in 3.3.0#
Updated the default Series 3 bootloader clock configuration to use SoCPLL at 145 MHz sourced from HFRCO.
Added support for dynamic application image selection in dual-application bootloaders using a flash-based switch mechanism.
API Changes#
Changed in 3.3.2#
None
Changed in 3.3.1#
None
Changed in 3.3.0#
Updated bootloader return types from
int32_ttobtl_ret_tfor IAR build compatibility.
Bug Fixes#
Fixed in 3.3.2#
Fixed an issue in Delta DFU where the bootloader read metadata from Slot 0 instead of the firmware slot being updated.
Fixed GBL tag-order handling when an SE upgrade was combined with an unencrypted application and SE upgrade no-staging was enabled.
Added the missing documentation entry for the bootloader_app_properties component.
Fixed in 3.3.1#
Fixed a UsageFault that could occur during bootloader image verification and image information parsing.
Fixed GCC Link Time Optimization (LTO) build issues affecting Series 2 and Series 3 bootloader core configurations.
Fixed a GCC LTO build issue in the bootloader apploader configuration.
Fixed bootloader component dependency metadata for TrustZone-aware configurations.
Fixed an SMP-related issue in the bootloader code identified during Sonar and build validation.
Fixed in 3.3.0#
Fixed a bootloader hard fault caused by invalid bootload information read from external flash.
Fixed a crash caused by invalid application properties pointers during application version checks.
Fixed internal storage slot overlap with NVM on 768 kB devices.
Fixed IAR build failures for Series 2 bootloader applications when glitch mitigation is disabled.
Chip Enablement#
Added in 3.3.2#
Added bootloader support for BRD2608B, BRD2602B, BRD2600C, and BRD2603C.
Added support for the bootloader-spi-ezsp application on xG2B OPNs and radio boards.
Added in 3.3.1#
None
Added in 3.3.0#
None
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
New Features#
Added in 3.3.1#
None
Added in 3.3.0#
Added a new Switch Multi-Protocol (SMP) feature that enables dual-application bootloaders to dynamically select and boot either App 1 or App 2 using a two-page flash-based switch mechanism.
Enhancements#
Added in 3.3.1#
None
Added in 3.3.0#
Added GCC Link Time Optimization (LTO) build support for Series 2 and Series 3 bootloader applications.
Updated the default Series 3 (SiWx301) bootloader clock configuration to use SoCPLL at 145 MHz sourced from HFRCO for improved out-of-box bootloader performance.
Removed Features#
None
Deprecated Features#
None
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
None
Modified APIs#
Modified in 3.3.1#
None
Modified in 3.3.0#
Modified API Signature | Previous API Signature |
|---|---|
|
|
|
|
|
|
Removed APIs#
None
Deprecated APIs#
None
Bug Fixes#
Fixed in 3.3.2#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1787166 | Fixed an issue where Delta DFU initialization loaded metadata from Slot 0 instead of the firmware slot being updated, causing a second slot to inherit Slot 0’s address and length. | None | Series 2 devices using Delta DFU with more than one firmware slot |
| 1671058 | Fixed an issue where the GBL parser returned an invalid tag-order error when an SE firmware upgrade was combined with an unencrypted application and SE upgrade no-staging was enabled. | None | Series 2 devices using SE upgrade no-staging with an unencrypted application image |
| 1757351 | Added the missing documentation entry for the bootloader_app_properties component so that its public properties provide a Help link. | None | None |
Fixed in 3.3.1#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1680408 | Fixed an issue that could trigger a UsageFault while the bootloader verified an image or parsed image metadata, improving reliability during image validation and startup. | None | None |
| 1649284 | Fixed build issues when compiling Series 2 and Series 3 bootloader core configurations with GCC LTO enabled. | None | None |
| 1666290 | Fixed a GCC LTO compatibility issue that prevented bootloader apploader configurations from building successfully. | None | None |
| 1672058 | Updated bootloader component dependency metadata to correctly support TrustZone-aware configurations during project setup. | None | None |
| 1657262 | Fixed an issue in the SMP-related bootloader code to improve reliability and maintainability. | None | None |
Fixed in 3.3.0#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1569692 | Resolved an issue where invalid BootloadInfo length values read from external SPI flash could cause the CRC validation routine to access memory outside valid bounds, resulting in a hard fault during firmware update operations. The bootloader now validates bootload information header fields before performing CRC checks to prevent invalid memory access. | None |
None |
| 1543959 | Updated bootload_checkApplicationPropertiesMagic() for Series 2 bootloaders to validate that the application properties pointer lies within the configured application space and flash bounds. Out-of-range pointers are now rejected to prevent crashes during application version checks. | None |
None |
| 1569149 | Reduced the internal storage slot size in the bootloader-storage-internal-single-768k sample from 368 kB to 352 kB to prevent overlap with NVM regions on 768 kB devices. | None |
None |
| 1596059 | Resolved an issue where Series 2 bootloader applications could fail to build with the IAR toolchain when glitch mitigation was disabled. The fix aligns the bootload_verifyApplication return type with the expected interface definition. | None |
None |
Chip Enablement#
Added in 3.3.2#
Added bootloader support for BRD2608B, BRD2602B, BRD2600C, and BRD2603C.
Added support for the bootloader-spi-ezsp application on xG2B OPNs and radio boards.
Added in 3.3.1#
None
Added in 3.3.0#
None
Application Example Changes#
New Examples | Modified Examples | Removed Examples | Deprecated Examples
New Examples#
None
Modified Examples#
None
Removed Examples#
None
Deprecated Examples#
None
Known Issues and Limitation#
Issues in 3.3.1#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1752568 | After a full or partial application OTA DFU on the BRD4407A, the device does not advertise after reboot when built with the LLVM toolchain. The OTA transfer completes successfully, but advertising does not resume. This issue does not affect builds that use the GCC toolchain. | None | None |
Issues in 3.3.0#
None