Simplicity SDK Platform - Micrium OS Version 6.1.2 - Release Notes (Oct 14, 2026)#
Simplicity SDK Platform Version 6.1.2
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
None.
API Changes#
None.
Bug Fixes#
Fixed in 6.1.2#
None.
Fixed in 6.1.1#
Corrected the option names
BSP_LF_CLK_SELandCPU_CFG_CACHE_MGMT_ENin the Studio configuration UI.
Fixed in 6.1.0#
Fixed an
OSTimeDly()overflow that could cause TimeTask to run continuously after approximately 36.4 hours.
Chip Enablement#
None.
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
New Features#
None.
Enhancements#
None.
Removed Features#
None.
Deprecated Features#
None.
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
None.
Modified APIs#
None.
Removed APIs#
None.
Deprecated APIs#
None.
Bug Fixes#
Fixed in 6.1.1#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1672985 | Corrected the option names BSP_LF_CLK_SEL and CPU_CFG_CACHE_MGMT_EN in the Studio configuration UI. |
None | Series 2 Devices |
Fixed in 6.1.0#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1596809 | Fixed an issue with OSTimeDly() where an overflow would cause TimeTask to run continuously after approximately 36.4 hours. |
None | Series 2 Devices |
Chip Enablement#
None.
Application Example Changes#
New Examples | Modified Examples | Removed Examples | Deprecated Examples
New Examples#
None.
Modified Examples#
None.
Removed Examples#
None.
Deprecated Examples#
None.
Known Issues and Limitations#
None.