You are viewing documentation for version:
PDFDimensions of the display.
Public Attributes#
uint16_t
Horizontal size of the display, in pixels.
uint16_t
Vertical size of the display, in pixels.
uint16_t
X coordinate of the top left corner of the clipping area.
uint16_t
Y coordinate of the top left corner of the clipping area.
uint16_t
Width of the clipping area.
uint16_t
Height of the clipping area.
Public Attribute Documentation#
xSize#
uint16_t DMD_DisplayGeometry::xSize
Horizontal size of the display, in pixels.
ySize#
uint16_t DMD_DisplayGeometry::ySize
Vertical size of the display, in pixels.
xClipStart#
uint16_t DMD_DisplayGeometry::xClipStart
X coordinate of the top left corner of the clipping area.
yClipStart#
uint16_t DMD_DisplayGeometry::yClipStart
Y coordinate of the top left corner of the clipping area.
clipWidth#
uint16_t DMD_DisplayGeometry::clipWidth
Width of the clipping area.
clipHeight#
uint16_t DMD_DisplayGeometry::clipHeight
Height of the clipping area.