You are viewing documentation for version:
ACMP initialization structure. 
Public Attributes#
uint32_t
Controls the bias current. 
uint32_t
Controls the VDD division factor. VREFOUT = VREFIN * (VREFDIV / 63). 
Selects the ACMP accuracy mode. 
Selects the hysteresis level. 
bool
Inactive value emitted by ACMP during warmup. 
Public Attribute Documentation#
bias_prog#
uint32_t sl_hal_acmp_init_t::bias_prog
Controls the bias current. 
vref_div#
uint32_t sl_hal_acmp_init_t::vref_div
Controls the VDD division factor. VREFOUT = VREFIN * (VREFDIV / 63). 
input_range#
sl_hal_acmp_input_range_t sl_hal_acmp_init_t::input_range
Selects the input range. 
accuracy#
sl_hal_acmp_accuracy_t sl_hal_acmp_init_t::accuracy
Selects the ACMP accuracy mode. 
hysteresis#
sl_hal_acmp_hysteresis_t sl_hal_acmp_init_t::hysteresis
Selects the hysteresis level. 
inactive_value#
bool sl_hal_acmp_init_t::inactive_value
Inactive value emitted by ACMP during warmup.