Channel descriptor structure.
Public Attributes#
Set to enable scan channel CHx.
Set to enable CHx pin.
Enable/disable channel interrupts after configuring all the sensor channel parameters.
Configure channel pin mode for the excitation phase of the scan sequence.
Configure channel pin idle setup in LESENSE idle phase.
Set to use alternate excite pin for excitation.
Set to enable result from this channel being shifted into the decoder register.
Set to invert result bit stored in the SCANRES register.
Set to store counter value in the RAM (accessible via RESDATA) and make the comparison result available in the SCANRES register.
Select clock used for the excitation timing.
Select clock used for the sample delay timing.
Configure the excitation time.
Configure the sample delay.
Configure the measure delay.
Configure the ACMP threshold or the DAC data.
Select if the ACMP output, the ADC output or the counter output should be used in comparison.
Configure the interrupt generation mode for the CHx interrupt flag.
Configure the decision threshold for the sensor data comparison. Valid range: 0-65535 (16 bits).
Select the mode for counter comparison.
Select the sensor evaluation mode.
Offset for IADC/ACMP interaction.
Public Attribute Documentation#
enable_interrupt#
bool sl_hal_lesense_channel_descriptor_t::enable_interrupt
Enable/disable channel interrupts after configuring all the sensor channel parameters.
excitation_mode#
sl_hal_lesense_pin_excitation_phase_t sl_hal_lesense_channel_descriptor_t::excitation_mode
Configure channel pin mode for the excitation phase of the scan sequence.
Note: OPAOUT is only available on channels 2, 3, 4, and 5.
idle_mode#
sl_hal_lesense_pin_idle_mode_t sl_hal_lesense_channel_descriptor_t::idle_mode
Configure channel pin idle setup in LESENSE idle phase.
pin_alternate_excite#
bool sl_hal_lesense_channel_descriptor_t::pin_alternate_excite
Set to use alternate excite pin for excitation.
shift_register#
bool sl_hal_lesense_channel_descriptor_t::shift_register
Set to enable result from this channel being shifted into the decoder register.
invert_register#
bool sl_hal_lesense_channel_descriptor_t::invert_register
Set to invert result bit stored in the SCANRES register.
store_counter#
sl_hal_lesense_store_sample_data_t sl_hal_lesense_channel_descriptor_t::store_counter
Set to store counter value in the RAM (accessible via RESDATA) and make the comparison result available in the SCANRES register.
excitation_clock#
sl_hal_lesense_excitation_clock_t sl_hal_lesense_channel_descriptor_t::excitation_clock
Select clock used for the excitation timing.
sample_clock#
sl_hal_lesense_excitation_clock_t sl_hal_lesense_channel_descriptor_t::sample_clock
Select clock used for the sample delay timing.
excitation_time#
uint8_t sl_hal_lesense_channel_descriptor_t::excitation_time
Configure the excitation time.
Excitation will last excitation_time+1 excitation clock. cycles. Valid range: 0-63 (6 bits).
sample_delay#
uint8_t sl_hal_lesense_channel_descriptor_t::sample_delay
Configure the sample delay.
Sampling will occur after sample_delay+1 sample clock cycles. Valid range: 0-127 (7 bits) or 0-255 (8 bits) depending on device.
measure_delay#
uint16_t sl_hal_lesense_channel_descriptor_t::measure_delay
Configure the measure delay.
Sensor measuring is delayed for measDelay excitation clock cycles. Valid range: 0-127 (7 bits) or 0-1023 (10 bits) depending on device.
acmp_threshold#
uint16_t sl_hal_lesense_channel_descriptor_t::acmp_threshold
Configure the ACMP threshold or the DAC data.
If dac_channel0_data is set to SL_HAL_LESENSE_DAC_CH_DATA, acmp_threshold defines the 12-bit DAC data in the data register of DAC interface (DACn_CH0DATA). In this case, the valid range is: 0-4095 (12 bits). If dac_channel0_data is set to SL_HAL_LESENSE_DAC_THRES, acmp_threshold defines the 6-bit Vdd scaling factor of ACMP negative input (VDDLEVEL in ACMP_INPUTSEL register). In this case, the valid range is: 0-63 (6 bits).
sample_mode#
sl_hal_lesense_channel_sample_t sl_hal_lesense_channel_descriptor_t::sample_mode
Select if the ACMP output, the ADC output or the counter output should be used in comparison.
interrupt_mode#
sl_hal_lesense_channel_interrupt_t sl_hal_lesense_channel_descriptor_t::interrupt_mode
Configure the interrupt generation mode for the CHx interrupt flag.
count_threshold#
uint16_t sl_hal_lesense_channel_descriptor_t::count_threshold
Configure the decision threshold for the sensor data comparison. Valid range: 0-65535 (16 bits).
compare_mode#
sl_hal_lesense_compare_counter_t sl_hal_lesense_channel_descriptor_t::compare_mode
Select the mode for counter comparison.
evaluation_mode#
sl_hal_lesense_sensor_evaluation_t sl_hal_lesense_channel_descriptor_t::evaluation_mode
Select the sensor evaluation mode.
offset#
uint8_t sl_hal_lesense_channel_descriptor_t::offset
Offset for IADC/ACMP interaction.
ACMP: determines which port I/O pins on the external override interface to access. IADC: determines which IADC scanner channels is sampled.