LEDDRV - LED Pre-Driver#


Example#

This example shows how to configure and use the LEDDRV peripheral for driving LED lights using both single and dual drive modes.

#include "sl_hal_leddrv.h"
#include "sl_clock_manager.h"

// Example function showing how to initialize and use the LEDDRV for LED control
void leddrv_example(void)
{
  // Enable clock to the LEDDRV peripheral
  sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_LEDDRV0);
  sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_GPIO);

  // Configure LEDDRV peripheral
  sl_hal_leddrv_init_t init = {
    .dual_drive_mode_enable = true,             // Enable dual drive mode
    .direct_drive_mode_enable = false,          // Disable direct drive mode
    .peak_current_foldback_enable = true,       // Enable peak current foldback
    .disable_ocflag_hardware_control = false,   // Enable overcurrent flag hardware control
    .enable_forced_calibration = false,         // Don't force enable (use internal enable)
    .time_on_max = SL_HAL_LEDDRV_TIME_MAX_12P8US,  // Set max on time to 12.8us
    .time_off_max = SL_HAL_LEDDRV_TIME_MAX_38P4US, // Set max off time to 38.4us
    .ipeak_detect_ref_adjust = SL_HAL_LEDDRV_IPEAK_DETECT_REF_ADJUST_300MV,
    .overcurrent_ref_adjust = SL_HAL_LEDDRV_IPEAK_OVERCURRENT_REF_ADJUST_800MV,
    .ton_cal_mode = SL_HAL_LEDDRV_TON_CAL_MODE_BOTH_CHANNELS,
    .fixed_ton_sel_lsb = SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_5MV,
    // Configure GPIO pins for LEDDRV - only Port C or D can be used
    .vac_gpio_select = { SL_HAL_LEDDRV_PORT_SELECT_PORT_C, 0 },
    .current_sense0_gpio_select = { SL_HAL_LEDDRV_PORT_SELECT_PORT_C, 1 },
    .drain_sense0_gpio_select = { SL_HAL_LEDDRV_PORT_SELECT_PORT_C, 2 },
    .current_sense1_gpio_select = { SL_HAL_LEDDRV_PORT_SELECT_PORT_C, 3 },
    .drain_sense1_gpio_select = { SL_HAL_LEDDRV_PORT_SELECT_PORT_C, 4 }
  };

  // Initialize the LEDDRV with the configuration
  sl_hal_leddrv_init(LEDDRV0, &init);

  // Enable the LEDDRV peripheral
  sl_hal_leddrv_enable(LEDDRV0);

  // Configure interrupts if needed
  sl_hal_leddrv_clear_interrupts(LEDDRV0, _LEDDRV_IEN_MASK);
  sl_hal_leddrv_enable_interrupts(LEDDRV0, LEDDRV_IEN_OCDET0);  // Enable overcurrent detection interrupt

  // Wait for a while to let the LEDDRV operate
  // In a real application, this would be replaced with application code
  // or you would respond to interrupts
  for (volatile int i = 0; i < 1000; i++) {}

  // Check for any overcurrent conditions
  uint32_t status = sl_hal_leddrv_get_status(LEDDRV0);
  if (status & LEDDRV_STATUS_OCFLAG0) {
    // Handle overcurrent condition on channel 0
    sl_hal_leddrv_clear_ocflag_channel0(LEDDRV0);
  }

  // Clean up and disable LEDDRV when done
  sl_hal_leddrv_disable_interrupts(LEDDRV0, _LEDDRV_IEN_MASK);
  sl_hal_leddrv_disable(LEDDRV0);
  sl_hal_leddrv_wait_ready(LEDDRV0);

  // Disable clocks to save power
  sl_clock_manager_disable_bus_clock(SL_BUS_CLOCK_LEDDRV0);
  sl_clock_manager_disable_bus_clock(SL_BUS_CLOCK_GPIO);
}

Modules#

sl_hal_leddrv_gpio_select_t

sl_hal_leddrv_init_t

Enumerations#

enum
SL_HAL_LEDDRV_TIME_MAX_DISABLE = 0
SL_HAL_LEDDRV_TIME_MAX_6P4US
SL_HAL_LEDDRV_TIME_MAX_12P8US
SL_HAL_LEDDRV_TIME_MAX_19P2US
SL_HAL_LEDDRV_TIME_MAX_25P6US
SL_HAL_LEDDRV_TIME_MAX_32P0US
SL_HAL_LEDDRV_TIME_MAX_38P4US
SL_HAL_LEDDRV_TIME_MAX_44P8US
}

Used for Max On time and max Off time of LEDDRV.

enum
SL_HAL_LEDDRV_TON_CAL_MODE_CURRENT_CHANNEL_ONLY = 0
SL_HAL_LEDDRV_TON_CAL_MODE_BOTH_CHANNELS
SL_HAL_LEDDRV_TON_CAL_MODE_ON_FORCE
SL_HAL_LEDDRV_TON_CAL_MODE_FIXED
}

Time On calibration channel mode.

enum
SL_HAL_LEDDRV_IPEAK_DETECT_REF_ADJUST_200MV = 0
SL_HAL_LEDDRV_IPEAK_DETECT_REF_ADJUST_300MV
SL_HAL_LEDDRV_IPEAK_DETECT_REF_ADJUST_400MV
SL_HAL_LEDDRV_IPEAK_DETECT_REF_ADJUST_500MV
}

Peak current detect reference adjust value.

enum
SL_HAL_LEDDRV_IPEAK_OVERCURRENT_REF_ADJUST_400MV = 0
SL_HAL_LEDDRV_IPEAK_OVERCURRENT_REF_ADJUST_600MV
SL_HAL_LEDDRV_IPEAK_OVERCURRENT_REF_ADJUST_800MV
SL_HAL_LEDDRV_IPEAK_OVERCURRENT_REF_ADJUST_1000MV
}

Over current reference adjust.

enum
SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_0MV = 0
SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_1MV
SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_2MV
SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_3MV
SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_4MV
SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_5MV
SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_6MV
SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_7MV
SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_8MV
SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_9MV
SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_10MV
SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_11MV
SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_12MV
SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_13MV
SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_14MV
SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_15MV
}

Fixed Ton Select LSBs.

enum
SL_HAL_LEDDRV_PORT_SELECT_NONE = 0
SL_HAL_LEDDRV_PORT_SELECT_PORT_C
SL_HAL_LEDDRV_PORT_SELECT_PORT_D
}

Port selection for LEDDRV gpio selection (only ports C/D allowed).

Functions#

void
sl_hal_leddrv_init(LEDDRV_TypeDef *leddrv, const sl_hal_leddrv_init_t *init)

Initialize LEDDRV.

void
sl_hal_leddrv_wait_ready(LEDDRV_TypeDef *leddrv)

Wait for disabling to finish.

void
sl_hal_leddrv_enable(LEDDRV_TypeDef *leddrv)

Enable LEDDRV.

void
sl_hal_leddrv_disable(LEDDRV_TypeDef *leddrv)

Disable LEDDRV.

void
sl_hal_leddrv_enable_dual_drive_mode(LEDDRV_TypeDef *leddrv)

Enable LEDDRV dual drive mode.

void

Disable LEDDRV dual drive mode.

void

Enable LEDDRV peak current foldback mode.

void

Disable LEDDRV peak current foldback mode.

void

Enable LEDDRV direct drive mode.

void

Disable LEDDRV direct drive mode.

void

Enable LEDDRV Hardware overcurrent control.

void

Disable LEDDRV Hardware overcurrent control.

void

Set LEDDRV Ton calibration trigger.

void

Clear LEDDRV Ton calibration trigger.

void
sl_hal_leddrv_clear_ocflag_channel0(LEDDRV_TypeDef *leddrv)

Clear LEDDRV Overcurrent Flag on channel 0.

void
sl_hal_leddrv_clear_ocflag_channel1(LEDDRV_TypeDef *leddrv)

Clear LEDDRV Overcurrent Flag on channel 1.

void
sl_hal_leddrv_reset(LEDDRV_TypeDef *leddrv)

Reset the LEDDRV.

uint32_t
sl_hal_leddrv_get_status(LEDDRV_TypeDef *leddrv)

Gets LEDDRV STATUS register value.

void
sl_hal_leddrv_clear_interrupts(LEDDRV_TypeDef *leddrv, uint32_t flags)

Clear one or more pending LEDDRV interrupts.

void
sl_hal_leddrv_set_interrupts(LEDDRV_TypeDef *leddrv, uint32_t flags)

Set one or more pending LEDDRV interrupts from SW.

void
sl_hal_leddrv_disable_interrupts(LEDDRV_TypeDef *leddrv, uint32_t flags)

Disable one or more LEDDRV interrupts.

void
sl_hal_leddrv_enable_interrupts(LEDDRV_TypeDef *leddrv, uint32_t flags)

Enable one or more LEDDRV interrupts.

uint32_t
sl_hal_leddrv_get_pending_interrupts(LEDDRV_TypeDef *leddrv)

Get pending LEDDRV interrupt flags.

uint32_t
sl_hal_leddrv_get_enabled_interrupts(LEDDRV_TypeDef *leddrv)

Get enabled LEDDRV interrupt flags.

uint32_t

Get enabled and pending LEDDRV interrupt flags.

Macros#

#define

Check if LEDDRV instance is valid.

#define

Default configuration for LEDDRV port/pin structure.

#define

Default configuration for LEDDRV initialization structure.

Enumeration Documentation#

sl_hal_leddrv_time_max_t#

sl_hal_leddrv_time_max_t

Used for Max On time and max Off time of LEDDRV.

Enumerator
SL_HAL_LEDDRV_TIME_MAX_DISABLE

Max On/Off time is disabled.

SL_HAL_LEDDRV_TIME_MAX_6P4US

Max On/Off time is 6.4 us.

SL_HAL_LEDDRV_TIME_MAX_12P8US

Max On/Off time is 12.8 us.

SL_HAL_LEDDRV_TIME_MAX_19P2US

Max On/Off time is 19.2 us.

SL_HAL_LEDDRV_TIME_MAX_25P6US

Max On/Off time is 25.6 us.

SL_HAL_LEDDRV_TIME_MAX_32P0US

Max On/Off time is 32.0 us.

SL_HAL_LEDDRV_TIME_MAX_38P4US

Max On/Off time is 38.4 us.

SL_HAL_LEDDRV_TIME_MAX_44P8US

Max On/Off time is 44.8 us.


sl_hal_leddrv_ton_cal_mode_t#

sl_hal_leddrv_ton_cal_mode_t

Time On calibration channel mode.

Enumerator
SL_HAL_LEDDRV_TON_CAL_MODE_CURRENT_CHANNEL_ONLY

Current channel only.

SL_HAL_LEDDRV_TON_CAL_MODE_BOTH_CHANNELS

Both channels.

SL_HAL_LEDDRV_TON_CAL_MODE_ON_FORCE

Calibration On force.

SL_HAL_LEDDRV_TON_CAL_MODE_FIXED

Calibration is Fixed.


sl_hal_leddrv_ipeak_detect_ref_adjust_t#

sl_hal_leddrv_ipeak_detect_ref_adjust_t

Peak current detect reference adjust value.

Enumerator
SL_HAL_LEDDRV_IPEAK_DETECT_REF_ADJUST_200MV

ipeak detect reference adjust 200 mV.

SL_HAL_LEDDRV_IPEAK_DETECT_REF_ADJUST_300MV

ipeak detect reference adjust 300 mV.

SL_HAL_LEDDRV_IPEAK_DETECT_REF_ADJUST_400MV

ipeak detect reference adjust 400 mV.

SL_HAL_LEDDRV_IPEAK_DETECT_REF_ADJUST_500MV

ipeak detect reference adjust 500 mV.


sl_hal_leddrv_overcurrent_ref_adjust_t#

sl_hal_leddrv_overcurrent_ref_adjust_t

Over current reference adjust.

Enumerator
SL_HAL_LEDDRV_IPEAK_OVERCURRENT_REF_ADJUST_400MV

Overcurrent reference adjust 400 mV.

SL_HAL_LEDDRV_IPEAK_OVERCURRENT_REF_ADJUST_600MV

Overcurrent reference adjust 600 mV.

SL_HAL_LEDDRV_IPEAK_OVERCURRENT_REF_ADJUST_800MV

Overcurrent reference adjust 800 mV.

SL_HAL_LEDDRV_IPEAK_OVERCURRENT_REF_ADJUST_1000MV

Overcurrent reference adjust 1000 mV.


sl_hal_leddrv_fixed_ton_sel_lsb_t#

sl_hal_leddrv_fixed_ton_sel_lsb_t

Fixed Ton Select LSBs.

Enumerator
SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_0MV

LSB is 0 mV.

SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_1MV

LSB is 1 mV.

SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_2MV

LSB is 2 mV.

SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_3MV

LSB is 3 mV.

SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_4MV

LSB is 4 mV.

SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_5MV

LSB is 5 mV.

SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_6MV

LSB is 6 mV.

SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_7MV

LSB is 7 mV.

SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_8MV

LSB is 8 mV.

SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_9MV

LSB is 9 mV.

SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_10MV

LSB is 10 mV.

SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_11MV

LSB is 11 mV.

SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_12MV

LSB is 12 mV.

SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_13MV

LSB is 13 mV.

SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_14MV

LSB is 14 mV.

SL_HAL_LEDDRV_FIXED_TON_SEL_LSB_15MV

LSB is 15 mV.


sl_hal_leddrv_port_select_t#

sl_hal_leddrv_port_select_t

Port selection for LEDDRV gpio selection (only ports C/D allowed).

Enumerator
SL_HAL_LEDDRV_PORT_SELECT_NONE

Select no Port.

SL_HAL_LEDDRV_PORT_SELECT_PORT_C

Select Port C.

SL_HAL_LEDDRV_PORT_SELECT_PORT_D

Select Port D.


Function Documentation#

sl_hal_leddrv_init#

void sl_hal_leddrv_init (LEDDRV_TypeDef * leddrv, const sl_hal_leddrv_init_t * init)

Initialize LEDDRV.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

A pointer to the LEDDRV peripheral register block.

const sl_hal_leddrv_init_t *[in]init

A pointer to the LEDDRV initialization structure.

This function will allocate GPIO CD bus to LEDDRV. Make sure to set port/pin to C/D ports and pins in the init structure.


sl_hal_leddrv_wait_ready#

void sl_hal_leddrv_wait_ready (LEDDRV_TypeDef * leddrv)

Wait for disabling to finish.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.


sl_hal_leddrv_enable#

void sl_hal_leddrv_enable (LEDDRV_TypeDef * leddrv)

Enable LEDDRV.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.


sl_hal_leddrv_disable#

void sl_hal_leddrv_disable (LEDDRV_TypeDef * leddrv)

Disable LEDDRV.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.


sl_hal_leddrv_enable_dual_drive_mode#

void sl_hal_leddrv_enable_dual_drive_mode (LEDDRV_TypeDef * leddrv)

Enable LEDDRV dual drive mode.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.


sl_hal_leddrv_disable_dual_drive_mode#

void sl_hal_leddrv_disable_dual_drive_mode (LEDDRV_TypeDef * leddrv)

Disable LEDDRV dual drive mode.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.


sl_hal_leddrv_enable_peak_current_foldback#

void sl_hal_leddrv_enable_peak_current_foldback (LEDDRV_TypeDef * leddrv)

Enable LEDDRV peak current foldback mode.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.


sl_hal_leddrv_disable_peak_current_foldback#

void sl_hal_leddrv_disable_peak_current_foldback (LEDDRV_TypeDef * leddrv)

Disable LEDDRV peak current foldback mode.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.


sl_hal_leddrv_enable_direct_drive_mode#

void sl_hal_leddrv_enable_direct_drive_mode (LEDDRV_TypeDef * leddrv)

Enable LEDDRV direct drive mode.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.


sl_hal_leddrv_disable_direct_drive_mode#

void sl_hal_leddrv_disable_direct_drive_mode (LEDDRV_TypeDef * leddrv)

Disable LEDDRV direct drive mode.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.


sl_hal_leddrv_enable_ocflag_hardware_control#

void sl_hal_leddrv_enable_ocflag_hardware_control (LEDDRV_TypeDef * leddrv)

Enable LEDDRV Hardware overcurrent control.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.


sl_hal_leddrv_disable_ocflag_hardware_control#

void sl_hal_leddrv_disable_ocflag_hardware_control (LEDDRV_TypeDef * leddrv)

Disable LEDDRV Hardware overcurrent control.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.


sl_hal_leddrv_set_ton_forced_calibration#

void sl_hal_leddrv_set_ton_forced_calibration (LEDDRV_TypeDef * leddrv)

Set LEDDRV Ton calibration trigger.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.


sl_hal_leddrv_clear_ton_forced_calibration#

void sl_hal_leddrv_clear_ton_forced_calibration (LEDDRV_TypeDef * leddrv)

Clear LEDDRV Ton calibration trigger.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.


sl_hal_leddrv_clear_ocflag_channel0#

void sl_hal_leddrv_clear_ocflag_channel0 (LEDDRV_TypeDef * leddrv)

Clear LEDDRV Overcurrent Flag on channel 0.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.


sl_hal_leddrv_clear_ocflag_channel1#

void sl_hal_leddrv_clear_ocflag_channel1 (LEDDRV_TypeDef * leddrv)

Clear LEDDRV Overcurrent Flag on channel 1.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.


sl_hal_leddrv_reset#

void sl_hal_leddrv_reset (LEDDRV_TypeDef * leddrv)

Reset the LEDDRV.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

A leddrv peripheral module.


sl_hal_leddrv_get_status#

uint32_t sl_hal_leddrv_get_status (LEDDRV_TypeDef * leddrv)

Gets LEDDRV STATUS register value.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

A LEDDRV peripheral module.

Returns

  • Current STATUS register value.


sl_hal_leddrv_clear_interrupts#

void sl_hal_leddrv_clear_interrupts (LEDDRV_TypeDef * leddrv, uint32_t flags)

Clear one or more pending LEDDRV interrupts.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.

uint32_t[in]flags

Pending LEDDRV interrupt source(s) to clear. Use one or more valid interrupt flags for the LEDDRV module (LEDDRV_IF_nnn) OR'ed together.


sl_hal_leddrv_set_interrupts#

void sl_hal_leddrv_set_interrupts (LEDDRV_TypeDef * leddrv, uint32_t flags)

Set one or more pending LEDDRV interrupts from SW.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.

uint32_t[in]flags

LEDDRV interrupt source(s) to set to pending. Use one or more valid interrupt flags for the LEDDRV module (LEDDRV_IF_nnn) OR'ed together.


sl_hal_leddrv_disable_interrupts#

void sl_hal_leddrv_disable_interrupts (LEDDRV_TypeDef * leddrv, uint32_t flags)

Disable one or more LEDDRV interrupts.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.

uint32_t[in]flags

LEDDRV interrupt source(s) to disable. Use one or more valid interrupt flags for the LEDDRV module (LEDDRV_IEN_nnn) OR'ed together.


sl_hal_leddrv_enable_interrupts#

void sl_hal_leddrv_enable_interrupts (LEDDRV_TypeDef * leddrv, uint32_t flags)

Enable one or more LEDDRV interrupts.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.

uint32_t[in]flags

LEDDRV interrupt source(s) to enable. Use one or more valid interrupt flags for the LEDDRV module (LEDDRV_IEN_nnn) OR'ed together.

Note

  • Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using sl_hal_leddrv_clear_interrupts() prior to enabling the interrupt.


sl_hal_leddrv_get_pending_interrupts#

uint32_t sl_hal_leddrv_get_pending_interrupts (LEDDRV_TypeDef * leddrv)

Get pending LEDDRV interrupt flags.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.

Note

  • Event bits are not cleared by this function.

Returns

  • LEDDRV interrupt source(s) pending. Returns one or more valid interrupt flags for the LEDDRV module (LEDDRV_IF_nnn) OR'ed together.


sl_hal_leddrv_get_enabled_interrupts#

uint32_t sl_hal_leddrv_get_enabled_interrupts (LEDDRV_TypeDef * leddrv)

Get enabled LEDDRV interrupt flags.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.

Note

  • Event bits are not cleared by this function.

Returns

  • LEDDRV interrupt source(s) enabled. Returns one or more valid enabled interrupt sources in LEDDRVx_IEN_nnn.


sl_hal_leddrv_get_enabled_pending_interrupts#

uint32_t sl_hal_leddrv_get_enabled_pending_interrupts (LEDDRV_TypeDef * leddrv)

Get enabled and pending LEDDRV interrupt flags.

Parameters
TypeDirectionArgument NameDescription
LEDDRV_TypeDef *[in]leddrv

Pointer to the LEDDRV peripheral register block.

Useful for handling more interrupt sources in the same interrupt handler.

Note

  • Interrupt flags are not cleared by this function.

Returns

  • Pending and enabled LEDDRV interrupt sources. The return value is the bitwise AND combination of

    • the OR combination of enabled interrupt sources in LEDDRVx_IEN_nnn register (LEDDRVx_IEN_nnn) and

    • the OR combination of valid interrupt flags of the LEDDRV module (LEDDRVx_IF_nnn).


Macro Definition Documentation#

SL_HAL_LEDDRV_REF_VALID#

#define SL_HAL_LEDDRV_REF_VALID
Value:
(leddrv_ref)

Check if LEDDRV instance is valid.


SL_HAL_LEDDRV_GPIO_SELECT_DEFAULT#

#define SL_HAL_LEDDRV_GPIO_SELECT_DEFAULT
Value:
{ \
_LEDDRV_ABUSCTRL0_VACPORTSEL_DEFAULT, /* Default port. */ \
_LEDDRV_ABUSCTRL0_VACPINSEL_DEFAULT /* Default pin. */ \
}

Default configuration for LEDDRV port/pin structure.


SL_HAL_LEDDRV_INIT_DEFAULT#

#define SL_HAL_LEDDRV_INIT_DEFAULT
Value:
{ \
_LEDDRV_CTRL_ENADUALMODE_DEFAULT, /* Disable dual drive mode. */ \
_LEDDRV_CTRL_ENDIRDRV_DEFAULT, /* Disable direct drive mode. */ \
_LEDDRV_CTRL_IPKFOLDBACK_DEFAULT, /* Disable peak current foldback. */ \
_LEDDRV_CTRL_HWOCFLAGDIS_DEFAULT, /* Enable over current flag hardware control is set. */ \
_LEDDRV_CTRL_ENFRC_DEFAULT, /* Force enable is not set; Override for internal enable. */ \
_LEDDRV_CFG_TONMAXVAL_DEFAULT, /* Time On max default value is 44p8us. */ \
_LEDDRV_CFG_TOFFMAXVAL_DEFAULT, /* Time Off max default value. is 44p8us */ \
_LEDDRV_CFG_IPKDETREFADJ_DEFAULT, /* Default peak current detect reference adjust value is 300mV. */ \
_LEDDRV_CFG_IOCREFADJ_DEFAULT, /* Default over current reference adjust value is 1000mV. */ \
_LEDDRV_CFG_TONCALMODE_DEFAULT, /* Default time On calibration channel mode is both channels . */ \
_LEDDRV_CFG_FIXEDTONSEL_DEFAULT, /* Default fixed Ton select LSB is 0mV. */ \
SL_HAL_LEDDRV_GPIO_SELECT_DEFAULT, /* Default Vac gpio select. */ \
SL_HAL_LEDDRV_GPIO_SELECT_DEFAULT, /* Default Current sense 0 gpio select. */ \
SL_HAL_LEDDRV_GPIO_SELECT_DEFAULT, /* Default Drain sense 0 gpio select. */ \
SL_HAL_LEDDRV_GPIO_SELECT_DEFAULT, /* Default Current sense 1 gpio select. */ \
SL_HAL_LEDDRV_GPIO_SELECT_DEFAULT /* Default Drain sense 1 gpio select. */ \
}

Default configuration for LEDDRV initialization structure.