PIXELRZ - Serial Pixel Interface#


Introduction#

PIXELRZ relays on external addressable LED to be configured correctly. In this example we will use WS2812B LEDS. Check datasheet of WS2812B for timing. To configure the timing, user must call @sl_hal_pixelrz_get_symbol_configuration().


Example#

{
  #define PIXELRZ_GPIO         PB0
  #define PIXELRZ_PIXEL_COUNT  60  // 60 pixels
  #define PIXELRZ_PIXEL_WIDTH  24  // 24 bits per pixel
  #define PIXELRZ_PIXEL_TRAIL  0   // no trail data

  // WS2812B timing values in microseconds. Check datasheet.
  #define WS2812B_T0_HIGH    0.4f
  #define WS2812B_T0_LOW     0.85f
  #define WS2812B_T1_HIGH    0.8f
  #define WS2812B_T1_LOW     0.45f
  #define WS2812B_TRST_HIGH  0.0f
  #define WS2812B_TRST_LOW   60.0f

  sl_hal_pixelrz_init_t init_serial = SL_HAL_PIXELRZ_CONFIG_SEQUENTIAL_DEFAULT;
  uint32_t freq;

  sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_PIXELRZ0);
  sl_clock_manager_get_clock_branch_frequency(SL_CLOCK_BRANCH_PIXELRZCLK, &freq);

  init_serial.pixel_number = PIXELRZ_PIXEL_COUNT;
  init_serial.pixel_width = PIXELRZ_PIXEL_WIDTH;
  init_serial.trail_data_width = PIXELRZ_PIXEL_TRAIL;

  init_serial.zero_symbol = sl_hal_pixelrz_get_symbol_configuration(WS2812B_T0_HIGH, WS2812B_T0_LOW, freq);
  init_serial.one_symbol = sl_hal_pixelrz_get_symbol_configuration(WS2812B_T1_HIGH, WS2812B_T1_LOW, freq);
  init_serial.reset_symbol = sl_hal_pixelrz_get_symbol_configuration(WS2812B_TRST_HIGH, WS2812B_TRST_LOW, freq);

  // Configure the GPIO.
  sl_gpio_set_pin_mode(PIXELRZ_GPIO, SL_GPIO_MODE_PUSH_PULL, 0);
  GPIO->PIXELRZROUTE[PIXELRZ_NUM(PIXELRZ0)].RZTXOUTROUTE = (PIXELRZ_GPIO->port << _GPIO_PIXELRZ_RZTXOUTROUTE_PORT_SHIFT)
                                                         | (PIXELRZ_GPIO->pin << _GPIO_PIXELRZ_RZTXOUTROUTE_PIN_SHIFT);
  GPIO->PIXELRZROUTE[PIXELRZ_NUM(PIXELRZ0)].ROUTEEN = GPIO_PIXELRZ_ROUTEEN_RZTXOUTPEN;

  sl_hal_pixelrz_init(PIXELRZ0, &init_serial);
  sl_hal_pixelrz_enable(PIXELRZ0);
  sl_hal_pixelrz_enable_tx(PIXELRZ0);
  sl_hal_pixelrz_wait_sync(PIXELRZ0);

  // User can start transmitting data directly or using LDMA.
}

Modules#

sl_hal_pixelrz_symbol_t

sl_hal_pixelrz_init_t

Enumerations#

enum
SL_HAL_PIXELRZ_MODE_SEQUENTIAL = _PIXELRZ_CFG_MODE_SEQUENTIAL
SL_HAL_PIXELRZ_MODE_PARALLEL = _PIXELRZ_CFG_MODE_PARALLEL
}

PIXELRZ mode. Serial or parallel.

enum
SL_HAL_PIXELRZ_TRIG_SW = _PIXELRZ_CFG_TRIGSEL_SW
SL_HAL_PIXELRZ_TRIG_AUTO = _PIXELRZ_CFG_TRIGSEL_AUTO
SL_HAL_PIXELRZ_TRIG_PRS = _PIXELRZ_CFG_TRIGSEL_PRS
}

The frame trigger source.

Functions#

void
sl_hal_pixelrz_init(PIXELRZ_TypeDef *pixelrz, const sl_hal_pixelrz_init_t *init)

Initialize PIXELRZ.

sl_hal_pixelrz_get_symbol_configuration(float time_high_us, float time_low_us, uint32_t freq)

Get symbol from time settings.

void
sl_hal_pixelrz_wait_sync(PIXELRZ_TypeDef *pixelrz)

Wait for ongoing sync of register(s) to the low-frequency domain to complete.

void
sl_hal_pixelrz_wait_ready(PIXELRZ_TypeDef *pixelrz)

Wait for disabling to finish.

void
sl_hal_pixelrz_enable(PIXELRZ_TypeDef *pixelrz)

Enable PIXELRZ.

void
sl_hal_pixelrz_disable(PIXELRZ_TypeDef *pixelrz)

Disable PIXELRZ.

void
sl_hal_pixelrz_tx(PIXELRZ_TypeDef *pixelrz, uint32_t data)

Transmits one data word.

void
sl_hal_pixelrz_enable_tx(PIXELRZ_TypeDef *pixelrz)

Enable PIXELRZ transmitter.

void
sl_hal_pixelrz_disable_tx(PIXELRZ_TypeDef *pixelrz)

Disable PIXELRZ transmitter.

void
sl_hal_pixelrz_clear_tx(PIXELRZ_TypeDef *pixelrz)

Clear TX FIFO.

void
sl_hal_pixelrz_reset(PIXELRZ_TypeDef *pixelrz)

Reset the PIXELRZ.

uint32_t
sl_hal_pixelrz_get_status(PIXELRZ_TypeDef *pixelrz)

Gets PIXELRZ STATUS register value.

void
sl_hal_pixelrz_clear_interrupts(PIXELRZ_TypeDef *pixelrz, uint32_t flags)

Clear one or more pending PIXELRZ interrupts.

void
sl_hal_pixelrz_set_interrupts(PIXELRZ_TypeDef *pixelrz, uint32_t flags)

Set one or more pending PIXELRZ interrupts from Software.

void
sl_hal_pixelrz_disable_interrupts(PIXELRZ_TypeDef *pixelrz, uint32_t flags)

Disable one or more PIXELRZ interrupts.

void
sl_hal_pixelrz_enable_interrupts(PIXELRZ_TypeDef *pixelrz, uint32_t flags)

Enable one or more PIXELRZ interrupts.

uint32_t
sl_hal_pixelrz_get_pending_interrupts(PIXELRZ_TypeDef *pixelrz)

Get pending PIXELRZ interrupt flags.

uint32_t
sl_hal_pixelrz_get_enabled_interrupts(PIXELRZ_TypeDef *pixelrz)

Get enabled PIXELRZ interrupt flags.

uint32_t

Get enabled and pending PIXELRZ interrupt flags.

Macros#

#define

Check if PIXELRZ instance is valid.

#define

Default sequential configuration.

#define

Default parallel configuration.

Enumeration Documentation#

sl_hal_pixelrz_mode_t#

sl_hal_pixelrz_mode_t

PIXELRZ mode. Serial or parallel.

Enumerator
SL_HAL_PIXELRZ_MODE_SEQUENTIAL

Sequential mode.

SL_HAL_PIXELRZ_MODE_PARALLEL

Parallel mode.


sl_hal_pixelrz_trigger_t#

sl_hal_pixelrz_trigger_t

The frame trigger source.

Enumerator
SL_HAL_PIXELRZ_TRIG_SW

Software trigger mode.

SL_HAL_PIXELRZ_TRIG_AUTO

Auto trigger mode.

SL_HAL_PIXELRZ_TRIG_PRS

Software trigger mode.


Function Documentation#

sl_hal_pixelrz_init#

void sl_hal_pixelrz_init (PIXELRZ_TypeDef * pixelrz, const sl_hal_pixelrz_init_t * init)

Initialize PIXELRZ.

Parameters
TypeDirectionArgument NameDescription
PIXELRZ_TypeDef *[in]pixelrz

A pointer to the PIXELRZ peripheral register block.

const sl_hal_pixelrz_init_t *[in]init

A pointer to the PIXELRZ initialization structure.


sl_hal_pixelrz_get_symbol_configuration#

sl_hal_pixelrz_symbol_t sl_hal_pixelrz_get_symbol_configuration (float time_high_us, float time_low_us, uint32_t freq)

Get symbol from time settings.

Parameters
TypeDirectionArgument NameDescription
float[in]time_high_us

High time in microseconds.

float[in]time_low_us

Low time in microseconds.

uint32_t[in]freq

PIXELRZ source clock frequency.

Check the datasheet for timing configuration.

Returns

  • Symbol high/low time values in clock cycles.


sl_hal_pixelrz_wait_sync#

void sl_hal_pixelrz_wait_sync (PIXELRZ_TypeDef * pixelrz)

Wait for ongoing sync of register(s) to the low-frequency domain to complete.

Parameters
TypeDirectionArgument NameDescription
PIXELRZ_TypeDef *[in]pixelrz

Pointer to the PIXELRZ peripheral register block.


sl_hal_pixelrz_wait_ready#

void sl_hal_pixelrz_wait_ready (PIXELRZ_TypeDef * pixelrz)

Wait for disabling to finish.

Parameters
TypeDirectionArgument NameDescription
PIXELRZ_TypeDef *[in]pixelrz

Pointer to the PIXELRZ peripheral register block.


sl_hal_pixelrz_enable#

void sl_hal_pixelrz_enable (PIXELRZ_TypeDef * pixelrz)

Enable PIXELRZ.

Parameters
TypeDirectionArgument NameDescription
PIXELRZ_TypeDef *[in]pixelrz

Pointer to the PIXELRZ peripheral register block.


sl_hal_pixelrz_disable#

void sl_hal_pixelrz_disable (PIXELRZ_TypeDef * pixelrz)

Disable PIXELRZ.

Parameters
TypeDirectionArgument NameDescription
PIXELRZ_TypeDef *[in]pixelrz

Pointer to the PIXELRZ peripheral register block.


sl_hal_pixelrz_tx#

void sl_hal_pixelrz_tx (PIXELRZ_TypeDef * pixelrz, uint32_t data)

Transmits one data word.

Parameters
TypeDirectionArgument NameDescription
PIXELRZ_TypeDef *[in]pixelrz

Pointer to the PIXELRZ peripheral register block.

uint32_t[in]data

Data to transmit.

Data will be written into FIFO.


sl_hal_pixelrz_enable_tx#

void sl_hal_pixelrz_enable_tx (PIXELRZ_TypeDef * pixelrz)

Enable PIXELRZ transmitter.

Parameters
TypeDirectionArgument NameDescription
PIXELRZ_TypeDef *[in]pixelrz

Pointer to the PIXELRZ peripheral register block.

The behaviour of this command will depend on the trigger configuration. If trigger is set to Software mode, this command will trigger transmission of one frame and stop, user must run this command for every frame. If trigger is set to Auto mode, the data will be transmitted whenever there's data in the FIFO and it will trigger transmission of all frames.


sl_hal_pixelrz_disable_tx#

void sl_hal_pixelrz_disable_tx (PIXELRZ_TypeDef * pixelrz)

Disable PIXELRZ transmitter.

Parameters
TypeDirectionArgument NameDescription
PIXELRZ_TypeDef *[in]pixelrz

Pointer to the PIXELRZ peripheral register block.


sl_hal_pixelrz_clear_tx#

void sl_hal_pixelrz_clear_tx (PIXELRZ_TypeDef * pixelrz)

Clear TX FIFO.

Parameters
TypeDirectionArgument NameDescription
PIXELRZ_TypeDef *[in]pixelrz

Pointer to the PIXELRZ peripheral register block.


sl_hal_pixelrz_reset#

void sl_hal_pixelrz_reset (PIXELRZ_TypeDef * pixelrz)

Reset the PIXELRZ.

Parameters
TypeDirectionArgument NameDescription
PIXELRZ_TypeDef *[in]pixelrz

A pixelrz peripheral module.


sl_hal_pixelrz_get_status#

uint32_t sl_hal_pixelrz_get_status (PIXELRZ_TypeDef * pixelrz)

Gets PIXELRZ STATUS register value.

Parameters
TypeDirectionArgument NameDescription
PIXELRZ_TypeDef *[in]pixelrz

A PIXELRZ peripheral module.

Returns

  • Current STATUS register value.


sl_hal_pixelrz_clear_interrupts#

void sl_hal_pixelrz_clear_interrupts (PIXELRZ_TypeDef * pixelrz, uint32_t flags)

Clear one or more pending PIXELRZ interrupts.

Parameters
TypeDirectionArgument NameDescription
PIXELRZ_TypeDef *[in]pixelrz

Pointer to the PIXELRZ peripheral register block.

uint32_t[in]flags

Pending PIXELRZ interrupt source(s) to clear. Use one or more valid interrupt flags for the PIXELRZ module (PIXELRZ_IF_nnn) OR'ed together.


sl_hal_pixelrz_set_interrupts#

void sl_hal_pixelrz_set_interrupts (PIXELRZ_TypeDef * pixelrz, uint32_t flags)

Set one or more pending PIXELRZ interrupts from Software.

Parameters
TypeDirectionArgument NameDescription
PIXELRZ_TypeDef *[in]pixelrz

Pointer to the PIXELRZ peripheral register block.

uint32_t[in]flags

PIXELRZ interrupt source(s) to set to pending. Use one or more valid interrupt flags for the PIXELRZ module (PIXELRZ_IF_nnn) OR'ed together.


sl_hal_pixelrz_disable_interrupts#

void sl_hal_pixelrz_disable_interrupts (PIXELRZ_TypeDef * pixelrz, uint32_t flags)

Disable one or more PIXELRZ interrupts.

Parameters
TypeDirectionArgument NameDescription
PIXELRZ_TypeDef *[in]pixelrz

Pointer to the PIXELRZ peripheral register block.

uint32_t[in]flags

PIXELRZ interrupt source(s) to disable. Use one or more valid interrupt flags for the PIXELRZ module (PIXELRZ_IEN_nnn) OR'ed together.


sl_hal_pixelrz_enable_interrupts#

void sl_hal_pixelrz_enable_interrupts (PIXELRZ_TypeDef * pixelrz, uint32_t flags)

Enable one or more PIXELRZ interrupts.

Parameters
TypeDirectionArgument NameDescription
PIXELRZ_TypeDef *[in]pixelrz

Pointer to the PIXELRZ peripheral register block.

uint32_t[in]flags

PIXELRZ interrupt source(s) to enable. Use one or more valid interrupt flags for the PIXELRZ module (PIXELRZ_IEN_nnn) OR'ed together.

Note

  • Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using sl_hal_pixelrz_clear_interrupts() prior to enabling the interrupt.


sl_hal_pixelrz_get_pending_interrupts#

uint32_t sl_hal_pixelrz_get_pending_interrupts (PIXELRZ_TypeDef * pixelrz)

Get pending PIXELRZ interrupt flags.

Parameters
TypeDirectionArgument NameDescription
PIXELRZ_TypeDef *[in]pixelrz

Pointer to the PIXELRZ peripheral register block.

Note

  • Event bits are not cleared by this function.

Returns

  • PIXELRZ interrupt source(s) pending. Returns one or more valid interrupt flags for the PIXELRZ module (PIXELRZ_IF_nnn) OR'ed together.


sl_hal_pixelrz_get_enabled_interrupts#

uint32_t sl_hal_pixelrz_get_enabled_interrupts (PIXELRZ_TypeDef * pixelrz)

Get enabled PIXELRZ interrupt flags.

Parameters
TypeDirectionArgument NameDescription
PIXELRZ_TypeDef *[in]pixelrz

Pointer to the PIXELRZ peripheral register block.

Note

  • Event bits are not cleared by this function.

Returns

  • PIXELRZ interrupt source(s) enabled. Returns one or more valid enabled interrupt sources in PIXELRZx_IEN_nnn.


sl_hal_pixelrz_get_enabled_pending_interrupts#

uint32_t sl_hal_pixelrz_get_enabled_pending_interrupts (PIXELRZ_TypeDef * pixelrz)

Get enabled and pending PIXELRZ interrupt flags.

Parameters
TypeDirectionArgument NameDescription
PIXELRZ_TypeDef *[in]pixelrz

Pointer to the PIXELRZ peripheral register block.

Useful for handling more interrupt sources in the same interrupt handler.

Note

  • Interrupt flags are not cleared by this function.

Returns

  • Pending and enabled PIXELRZ interrupt sources. The return value is the bitwise AND combination of

    • the OR combination of enabled interrupt sources in PIXELRZx_IEN_nnn register (PIXELRZx_IEN_nnn) and

    • the OR combination of valid interrupt flags of the PIXELRZ module (PIXELRZx_IF_nnn).


Macro Definition Documentation#

SL_HAL_PIXELRZ_REF_VALID#

#define SL_HAL_PIXELRZ_REF_VALID
Value:
(pixelrz_ref)

Check if PIXELRZ instance is valid.


SL_HAL_PIXELRZ_SEQUENTIAL_INIT_DEFAULT#

#define SL_HAL_PIXELRZ_SEQUENTIAL_INIT_DEFAULT
Value:
{ \
SL_HAL_PIXELRZ_MODE_SEQUENTIAL, /* mode is sequential. */ \
false, /* LSB first. */ \
false, /* Memory alignment of 8bits. */ \
false, /* Do not invert output. */ \
false, /* Jitter disabled. */ \
false, /* Stop symbol disabled. */ \
true, /* Reset symbol enabled. */ \
SL_HAL_PIXELRZ_TRIG_SW, /* Software trigger. */ \
0, /* FIFO water mark is 0. */ \
0, /* Prescaler is 0. */ \
0, /* Pixel number is 0. */ \
0, /* Pixel width is 0. */ \
0, /* Trail data width is 0. */ \
{ 0, 0 }, /* Zero symbol high/low times */ \
{ 0, 0 }, /* One symbol high/low times */ \
{ 0, 0 }, /* Stop symbol high/low times */ \
{ 0, 0 }, /* Reset symbol high/low times */ \
}

Default sequential configuration.


SL_HAL_PIXELRZ_PARALLEL_INIT_DEFAULT#

#define SL_HAL_PIXELRZ_PARALLEL_INIT_DEFAULT
Value:
{ \
SL_HAL_PIXELRZ_MODE_PARALLEL, /* Mode is parallel. */ \
false, /* LSB first. */ \
false, /* Memory alignment of 8bits. */ \
false, /* Do not invert output. */ \
false, /* Jitter disabled. */ \
true, /* Stop symbol enabled. */ \
false, /* Reset symbol disabled. */ \
SL_HAL_PIXELRZ_TRIG_SW, /* Software trigger. */ \
0, /* FIFO water mark is 0. */ \
0, /* Prescaler is 0. */ \
0, /* Pixel number is 0. */ \
0, /* Pixel width is 0. */ \
0, /* Trail data width is 0. */ \
{ 0, 0 }, /* Zero symbol high/low times */ \
{ 0, 0 }, /* One symbol high/low times */ \
{ 0, 0 }, /* Stop symbol high/low times */ \
{ 0, 0 }, /* Reset symbol high/low times */ \
}

Default parallel configuration.