You are viewing documentation for version:
PDFCertificate size data structure.
Public Attributes#
uint32_t
size in bytes of the Batch certificate
uint32_t
size in bytes of the SE ID certificate
uint32_t
size in bytes of the Host ID certificate
Public Attribute Documentation#
batch_id_size#
uint32_t sl_se_cert_size_type_t::batch_id_size
size in bytes of the Batch certificate
se_id_size#
uint32_t sl_se_cert_size_type_t::se_id_size
size in bytes of the SE ID certificate
host_id_size#
uint32_t sl_se_cert_size_type_t::host_id_size
size in bytes of the Host ID certificate