Image Feature Generator#
Processes camera images and extracts features for machine learning image classification applications.
The image feature generator process input image captured from camera and extracts required features to use with machine learning image classification applications using a camera as an image source.
Feature Generation#
The captured image pre-processed using crop and mean-std normalization based on model configuration used from application.
Image
│
┌───────▼───────┐
│ Crop │
└───────┬───────┘
│
┌───────▼───────┐
│ Check mean │
└───────┬───────┘
│
┌───────▼───────┐
│ Normalization │
└───────┬───────┘
│
▼
Model
Usage#
sl_ml_image_feature_generation_init() initializes the feature generation based on the configuration in sl_ml_image_feature_generation_config.h. It also initializes and starts the camera in streaming mode, which places the image samples into a ping-pong-buffer.
The image is pre-processed and filled in input tensor when sl_ml_image_feature_generation_fill_tensor() is called.
To retrieve the generated features sl_ml_image_feature_generation_fill_tensor() must be called.
Example#
When used with TensorFlow Lite Micro, the image feature generator can be used to fill a tensor directly by using sl_ml_image_feature_generation_fill_tensor(). However, the model has to be trained using the same feature generator configurations as used for inference, configured in sl_ml_image_feature_generation_config.h.
#include "sl_tflite_micro_init.h"
#include "sl_ml_image_feature_generation.h"
void main(void)
{
sl_ml_image_feature_generation_init();
while(1){ *
if(do_inference){
sl_ml_image_feature_generation_fill_tensor(sl_tflite_micro_get_input_tensor());
sl_tflite_micro_get_interpreter()->Invoke();
}
...
}
}
Functions#
Set up the camera as an image source for feature generation.
Fill a TensorFlow tensor with feature data. Data type of input image for model will be selected based on model configuration.
Set up the aurducam as an image source for feature generation and initialize the camera with configuration.
Set up the JLink stream as output node. Image data streamed over JLink to python interface.
Retrieve image from ping-pog buffer captured from aurducam. Store image data to destination pointer.
Initializes Look up table for croping image.
Retrieve the features, scales them by the given scaler, and fills float buffer.
Computes mean and mean square of input image.
Retrieve the features, normalizes them by centering about their mean and standard deviation and fills float buffer.
Retrieve the features as type float32 and copy them to the provided buffer.
Reset the state of the image feature generator.
Function to convert image color space to gray.
Function Documentation#
sl_ml_image_feature_generation_init#
sl_status_t sl_ml_image_feature_generation_init ()
Set up the camera as an image source for feature generation.
Returns
SL_STATUS_OK if sl_ml_initialize_arducam_camera succeeded. JLink "image" stream registration is optional: on failure, a warning is printed to the log and the function still returns SL_STATUS_OK; sl_ml_dump_image and PC-side visualization are inactive until a future successful registration. If camera init failed, same status as sl_ml_initialize_arducam_camera (e.g. SL_STATUS_BUS_ERROR); sl_ml_image_feature_generation_reset was run before return.
sl_ml_image_feature_generation_fill_tensor#
sl_status_t sl_ml_image_feature_generation_fill_tensor (TfLiteTensor * input_tensor)
Fill a TensorFlow tensor with feature data. Data type of input image for model will be selected based on model configuration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| TfLiteTensor * | [in] | input_tensor | The input tensor to fill with features. |
Note
This function overwrites the entire input tensor.
Returns
SL_STATUS_OK for success SL_STATUS_INVALID_PARAMETER Tensor type or size does not correspond with configuration
sl_ml_initialize_arducam_camera#
sl_status_t sl_ml_initialize_arducam_camera ()
Set up the aurducam as an image source for feature generation and initialize the camera with configuration.
Returns
SL_STATUS_OK for success SL_STATUS_FAIL
sl_ml_dump_image#
void sl_ml_dump_image (const uint8_t * image_data, uint32_t image_length)
Set up the JLink stream as output node. Image data streamed over JLink to python interface.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const uint8_t * | N/A | image_data | |
| uint32_t | N/A | image_length |
Returns
SL_STATUS_OK for success SL_STATUS_FAIL
sl_ml_retrieve_next_camera_image#
void sl_ml_retrieve_next_camera_image (uint8_t ** image_data, uint32_t * image_size)
Retrieve image from ping-pog buffer captured from aurducam. Store image data to destination pointer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t ** | N/A | image_data | |
| uint32_t * | N/A | image_size |
sl_ml_image_crop_lut_init#
void sl_ml_image_crop_lut_init ()
Initializes Look up table for croping image.
sl_ml_image_feature_generation_get_image_scaled#
sl_status_t sl_ml_image_feature_generation_get_image_scaled (uint8_t * image_data, float * buffer, size_t num_elements, float scaler)
Retrieve the features, scales them by the given scaler, and fills float buffer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [out] | image_data | Pointer to the buffer to store the scaled feature data |
| float * | [in] | buffer | The number of elements corresponding to the size of the buffer; If this is not large enough to store the entire feature buffer the function will return with an error. |
| size_t | [in] | num_elements | The scaling factor to apply to each feature value. |
| float | N/A | scaler |
buffer = (float)image_data * scaler
Note
This function overwrites the entire buffer.
Returns
SL_STATUS_OK for success SL_STATUS_INVALID_PARAMETER num_elements too small
sl_ml_get_image_mean#
sl_status_t sl_ml_get_image_mean (uint8_t * in_cam_image, float * mean, float * mean2, size_t num_elements)
Computes mean and mean square of input image.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [out] | in_cam_image | Pointer to the running mean; reset to 0 at entry, then set to the sample mean. |
| float * | [out] | mean | Pointer to the Welford M2 accumulator; reset to 0 at entry, then set so that population variance is mean2 / num_elements. |
| float * | [in] | mean2 | The number of elements corresponding to the size of the buffer; If this is not large enough to store the entire feature buffer the function will return with an error. |
| size_t | N/A | num_elements |
mean = ((float)image_data / (width*length)
Returns
SL_STATUS_OK for success SL_STATUS_INVALID_PARAMETER num_elements too small
sl_ml_image_feature_generation_get_image_mean_std_normalized#
sl_status_t sl_ml_image_feature_generation_get_image_mean_std_normalized (uint8_t * image_data, float * buffer, float mean, float mean2, size_t num_elements)
Retrieve the features, normalizes them by centering about their mean and standard deviation and fills float buffer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [out] | image_data | Pointer to the buffer to store the normalized feature data |
| float * | [in] | buffer | float mean, mean value of image. |
| float | [in] | mean | Welford M2 from sl_ml_get_image_mean; population variance is mean2 / num_elements. |
| float | [in] | mean2 | The number of elements corresponding to the size of the buffer; If this is not large enough to store the entire feature buffer the function will return with an error. |
| size_t | N/A | num_elements |
buffer = ((float)image_data - mean(image_data)) / std(image_data)
Note
This function overwrites the entire buffer. std uses population variance: sqrtf(mean2 / num_elements). A small floor is applied to the divisor so uniform or near-uniform crops (std ~ 0) do not produce Inf/NaN; negative variance from float error is clamped to zero before sqrtf.
Returns
SL_STATUS_OK for success SL_STATUS_INVALID_PARAMETER num_elements too small
sl_ml_image_feature_generation_get_image_raw_float32#
sl_status_t sl_ml_image_feature_generation_get_image_raw_float32 (uint8_t * image_data, float * buffer, size_t num_elements)
Retrieve the features as type float32 and copy them to the provided buffer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [out] | image_data | Pointer to the buffer to store the feature data |
| float * | [in] | buffer | The number of elements corresponding to the size of the buffer; If this is not large enough to store the entire feature buffer the function will return with an error. |
| size_t | N/A | num_elements |
Note
This function overwrites the entire buffer.
Returns
SL_STATUS_OK for success SL_STATUS_INVALID_PARAMETER num_elements too small
sl_ml_image_feature_generation_reset#
void sl_ml_image_feature_generation_reset ()
Reset the state of the image feature generator.
sl_ml_convert_rgb565_to_gray#
void sl_ml_convert_rgb565_to_gray (uint8_t * img)
Function to convert image color space to gray.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [out] | img | Pointer holding reference to image data. |