Simplicity Machine Learning Version 1.1.0-beta Release Notes (Jun 23, 2026)#
The Artificial Intelligence and Machine Learning (AI/ML) tools include Simplicity Machine Learning (formerly ML Profiler), the model graph viewer, and the model converter. Use these tools to prepare and profile models on the host system.
Release Summary#
Key Features | Bug Fixes | Chip Enablement
Key Features#
The "ML Profiler" tool was renamed to "Simplicity Machine Learning".
Added an option to choose kernels when profiling a model.
Improved central processing unit (CPU) and accelerator cycle counts in the profiler.
Added a model graph viewer to Simplicity Machine Learning based on Model Explorer.
Added an alpha release of the ML Model Converter to convert PyTorch and Open Neural Network Exchange (ONNX) models to TensorFlow Lite (TFLite).
Bug Fixes#
None.
Chip Enablement#
None.
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
Note: See Feature Matrix for a list of any applicable application programming interfaces (APIs), examples, software variants, modes, hardware, and host interfaces for each feature.
New Features#
Simplicity Machine Learning profiler: Renamed from "ML Profiler" to "Simplicity Machine Learning". This host-side tool profiles ML models on target hardware.
Kernel selection: Added an option to choose kernels when profiling a model.
Model graph viewer: Integrated a model graph viewer in Simplicity Machine Learning based on Model Explorer. Linux and macOS are supported natively; Windows is supported through Windows Subsystem for Linux (WSL).
ML Model Converter: Added a unified graphical user interface (GUI) and command-line interface (CLI) to convert PyTorch and ONNX models to TFLite.
manifest.jsonoutput: When--save-manifestcommand line argument is passed on the CLI, amanifest.jsonfile is saved with conversion metadata including conversion time, conversion ratio, input shape, and output shape. The GUI generates this file every time.
Enhancements#
Profiler metrics: Improved CPU and accelerator cycle count reporting in Simplicity Machine Learning.
Removed Features#
None.
Deprecated Features#
Deprecated Feature | Planned Removal Date |
|---|---|
"ML Profiler" tool | Superseded by Simplicity Machine Learning |
The "ML Profiler" tool will not receive any updates. In Simplicity Studio, search for Simplicity Machine Learning (GUI) or Simplicity Machine Learning (CLI).
Bug Fixes#
None.
Chip Enablement#
None.
Known Issues and Limitations#
Refer to the ML Profiler Troubleshooting section for known issues and their solutions.
Refer to the ML Model Converter Troubleshooting section for known issues and their solutions.
The model graph viewer is not supported natively on Windows; use WSL to launch the GUI tool.
The model converter is not supported natively on Windows; use WSL to launch the GUI tool.
ONNX models are converted using
onnx2tf. Non-self-contained ONNX models with external weights are rejected with a clear messagePyTorch models with dynamic graphs require an explicit input shape input.
Quantization is not applied.
Output models are generated in float32.
Installation and Use#
Refer to the Getting Started guide for installation and usage instructions.
For information about Secure Vault Integration, see Secure Vault.
Help and Feedback#
Contact Silicon Labs Support.
To use the Ask AI tool, see the search field at the top of this page.
Get help from our developer community.
Feature Matrix#
Supported Features | Unsupported Features
Supported Features#
| Feature Name | Description | Quality | Related API Names | Supported Software Variants, Hardware, Modes, Host Interfaces | Related Example Names |
|---|---|---|---|---|---|
| ML Model profiler | Profile ML models on target hardware. Choose kernels when profiling. Improved CPU and accelerator cycle counts. | Beta |
|
|
|
| Model graph viewer | Integrated model graph viewer in Simplicity Machine Learning based on Model Explorer. | Beta |
|
|
|
| ML Model converter | Convert PyTorch and ONNX models to TFLite on the host. Optional manifest.json output with conversion metadata. |
Alpha |
|
|
Unsupported Features#
The model graph viewer is not supported natively on Windows. Use WSL to launch the GUI tool.
The model converter is not supported natively on Windows. Use WSL to launch the GUI tool.
SDK Release and Maintenance Policy#
See our SDK Release and Maintenance Policy.