TensorFlow Lite Micro Init#
The TensorFlow Lite Micro Init functions are autogenerated from the flatbuffer file provided in the configuration, which includes an opsResolver generated according to the included operators in the flatbuffer. Helper functions to access the input and output tensors are also provided.
Functions#
Estimate the arena size for a given model.
Dynamically allocate a buffer that can be used for the tensor arena.
Get a pointer to the TensorFlow Lite Micro error reporter created by the init function.
Get a pointer to the TensorFlow Lite Micro interpreter created by the init function.
Get a pointer to the input tensor, set by the init function.
Get a pointer to the output tensor, set by the init function.
Get a pointer to the opcode resolver for the flatbuffer given by the configuration.
Create the error reporter and opcode resolver and initialize variables for the flatbuffer given by the configuration.
Function Documentation#
sl_tflite_micro_estimate_arena_size#
sl_status_t sl_tflite_micro_estimate_arena_size (const tflite::Model * model, const tflite::MicroOpResolver & opcode_resolver, size_t * estimated_size)
Estimate the arena size for a given model.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const tflite::Model * | [in] | model | Pointer to the model to estimate the arena size for. |
| const tflite::MicroOpResolver & | [in] | opcode_resolver | The opcode resolver to use for the model. |
| size_t * | [out] | estimated_size | The estimated size of the arena, as output. |
Returns
SL_STATUS_OK if the estimation was successful.
sl_tflite_micro_allocate_tensor_arena#
uint8_t * sl_tflite_micro_allocate_tensor_arena (size_t arena_size, uint8_t ** tensor_arena)
Dynamically allocate a buffer that can be used for the tensor arena.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| size_t | [in] | arena_size | The size of the arena to allocate. |
| uint8_t ** | [out] | tensor_arena | Pointer to the allocated tensor arena buffer. |
Returns
A pointer to the allocated base buffer. Returns nullptr if the allocation failed. The base buffer is used for freeing the allocated memory.
sl_tflite_micro_get_error_reporter#
tflite::ErrorReporter * sl_tflite_micro_get_error_reporter ()
Get a pointer to the TensorFlow Lite Micro error reporter created by the init function.
Returns
A pointer to the error reporter.
sl_tflite_micro_get_interpreter#
tflite::MicroInterpreter * sl_tflite_micro_get_interpreter ()
Get a pointer to the TensorFlow Lite Micro interpreter created by the init function.
Returns
A pointer to the interpreter.
sl_tflite_micro_get_input_tensor#
TfLiteTensor * sl_tflite_micro_get_input_tensor ()
Get a pointer to the input tensor, set by the init function.
Returns
A pointer to the input tensor.
sl_tflite_micro_get_output_tensor#
TfLiteTensor * sl_tflite_micro_get_output_tensor ()
Get a pointer to the output tensor, set by the init function.
Returns
A pointer to the output tensor.
sl_tflite_micro_opcode_resolver#
tflite::MicroOpResolver & sl_tflite_micro_opcode_resolver ()
Get a pointer to the opcode resolver for the flatbuffer given by the configuration.
Returns
The address to the opcode resolver.
sl_tflite_micro_init#
void sl_tflite_micro_init (void )
Create the error reporter and opcode resolver and initialize variables for the flatbuffer given by the configuration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |