Unify Matter Bridge User's Guide#
The Unify Matter Bridge is a Unify IoT Service that enables interaction with Unify devices from a Matter fabric. For a more thorough description see the Unify Matter Bridge Overview.
As a prerequisite for the Matter Bridge to work, at least one Unify protocol controller should be set up and running. This guide assumes that you have set up the Z-Wave Protocol Controller (uic-zpc) to run on a Raspberry Pi 4 and connected it to an MQTT broker in your network. Read the Unify Host SDK's Getting Started Guide for information on how to set this up.
Once a protocol controller is running, the Matter Bridge can be started.
The following documentation assumes that you have built the Unify Matter Bridge application by following the Build Guide and have transferred the unify-matter-bridge to your Raspberry Pi 4 (RPi4) running the 32-bit version of Raspberry Pi OS Buster.
Note:
The requirements for using the Matter Bridge with the Google Home App (GHA) are:
Inclusion in the Matter Early Access Program (EAP).
A project properly configured in the Google Home Developer Console.
Use of the specified version of the Google Home App for Android.
This guide will use the CLI tool called
chip-toolfor commissioning and device control.
Running the Matter Bridge#
At start-up, the Matter Bridge needs to connect to the Matter Fabric as well as the MQTT Broker. It is therefore critical that you have access to port 1883, the default MQTT Broker's port, as well as a network setup that allows mDNS through.
A few important runtime configurations must be considered, along with some other configuration options. A full list of command-line parameters is provided in the Command line arguments section.
Important Configuration Settings#
Network Interface#
Specify the network interface on which the Matter Fabric runs. In a regular RPi4 setup it would be
wlan0for WiFi andeth0for ethernet. Specify this with the '--interface' argument, as such:./unify-matter-bridge --interface eth0Key-Value store (KVS)#
The Matter Bridge uses a Key-Value store for persisting various run-time configurations. Make sure to have read/write access to the default path '
/var/chip_unify_bridge.kvs' or provide the path to where writing this data is allowed. If this file is deleted before start-up, everything is reset and the bridge will not belong to any Matter Fabric until it has again been commissioned../unify-matter-bridge --kvs ./matter-bridge.kvsMQTT Host#
If you have followed the Unify Host SDK's Getting Started Guide, your MQTT Broker should now be running on '
localhost'. If you have decided to run the MQTT broker on a different host, you can tell the Unify Matter Bridge to connect to a different host../unify-matter-bridge --mqtt.host 10.0.0.42Vendor and Product ID#
If you have access to the EAP and you want to use the Google Home App, you need to set a specific VID and PID for the Matter Bridge.
./unify-matter-bridge --vendor fff1 --product 8001
Starting the Matter Bridge#
Once the configuration parameters are set it is time to start the bridge application.
./unify-matter-bridge --interface eth0 --kvs ./matter-bridge.kvs --mqtt.host localhost --mqtt.port 1337Commissioning the Bridge to a Network#
To include the bridge in the Matter network, it must first be commissioned.
The first time the bridge starts it will automatically go into commissioning mode. After 10 minutes the bridge will exit commissioning mode.
If the bridge has not been commissioned within this window, the application must be restarted to open the commissioning window again or the window can be opened by writing commission in the CLI when running the bridge. The commission command may also be used for multi-fabric commissioning.
The Unify Matter Bridge uses the "On Network" commissioning method. For now, there is no Bluetooth commissioning support.
The commissioning procedure requires use of a pairing code.
This pairing code is written to the console when running the Matter Bridge.
Look for something similar to 'MT:-24J029Q00KA0648G00', used as the pairing code in the following example.
This code can be used when commissioning with the CLI commissioning tool chip-tool.
[1659615301.367669][1967:1967] CHIP:SVR: SetupQRCode: [MT:-24J029Q00KA0648G00]A simpler, more user-friendly way of commissioning is to use the Google Home App with a QR code containing the pairing code. The QR code can be obtained by following the link seen in the console, similar to the line below:
[1659615301.367723][1967:1967] CHIP:SVR: https://dhrishi.github.io/connectedhomeip/qrcode.html?data=MT%3A-24J029Q00KA0648G00It should be noted that the commissioner must be on the same network as the Raspberry Pi. Note that by default the bridge binds to the eth0 interface. If another interface is to be used, see the description of the command line arguments for setting Network Interface.
Using the chip-tool to Commission#
In the following procedure make sure to use the pairing code taken from the console output, as described above.
To commission the Matter Bridge with the chip-tool and assign the bridge the Node ID 1:
chip-tool pairing code 1 MT:-24J0AFN00KA0648G00Toggle an OnOff device#
To send an OnOff cluster Toggle command to a bridged endpoint with id 2, via Matter Fabric Node ID 1:
chip-tool onoff toggle 1 2For more information on how to use the chip-tool see the Chip Tool Manual located in the Matter repo at /docs/guides/chip_tool_guide.md
Toggle a Group of OnOff Devices#
The Matter Bridge has support for forwarding group messages from the Matter Fabric to Unify Nodes. The protocol controllers will send the group messages as actual group cast messages on the destination network (Z-Wave/Zigbee).
To send a group command, first set up the group keys in the bridge. This example assumes the bridge to be Node ID 1, and GroupKeySetID 42 is added to Group ID 1:
chip-tool accesscontrol write acl '[{"fabricIndex": 1, "privilege": 5, "authMode": 2, "subjects": [112233], "targets": null },{"fabricIndex": 1, "privilege": 4, "authMode": 3, "subjects": [1], "targets": null }]' 1 0
chip-tool groupkeymanagement key-set-write '{"groupKeySetID": 42, "groupKeySecurityPolicy": 0, "epochKey0": "d0d1d2d3d4d5d6d7d8d9dadbdcdddedf", "epochStartTime0": 2220000,"epochKey1": "d1d1d2d3d4d5d6d7d8d9dadbdcdddedf", "epochStartTime1": 2220001,"epochKey2": "d2d1d2d3d4d5d6d7d8d9dadbdcdddedf", "epochStartTime2": 2220002 }' 1 0
chip-tool groupkeymanagement write group-key-map '[{"groupId": 1, "groupKeySetID": 42, "fabricIndex": 1}]' 1 0Next, add bridge endpoint 2 to Group ID 0x0001
chip-tool groups add-group 0x0001 grp1 1 2Next, program the chip-tool:
chip-tool groupsettings add-group grp1 0x0002
chip-tool groupsettings add-keysets 0x0042 0 0x000000000021dfe0 hex:d0d1d2d3d4d5d6d7d8d9dadbdcdddedf
chip-tool groupsettings bind-keyset 0x0001 0x0042As Matter is based on IPv6 and the group message will be sent as a multicast message, a multicast route must be set up to tell the Linux kernel what interface to send the group message to.
sudo route add -6 ff35:40:fd00::/24 dev eth0Finally, a multicast command may be sent using the chip-tool.
// Send actual multicast command
./chip-tool onoff toggle 0xffffffffffff0001 1Command Line Arguments#
The Unify Matter Bridge provides the following command line arguments:
Using --help displays the following text.
Usage: ./unify_matter_bridge [Options]
Options:
--conf arg (=/etc/uic/uic.cfg) Config file in YAML format. UIC_CONF
env variable can be set to override the
default config file path
--help Print this help message and quit
--dump-config Dump the current configuration in a
YAML config file format that can be
passed to the --conf option
--version Print version information and quitThe following options can also be in a config file. Options and values passed on the command line take precedence over the options and values in the config file.
--log.level arg (=i) Log Level (d,i,w,e,c)
--log.tag_level arg Tag-based log level
Format: <tag>:<severity>,
<tag>:<severity>, ...
--interface arg (=en0) Ethernet interface to use
--kvs arg (=/var/chip_unify_bridge.kvs)
Matter key value store path
--vendor arg (=65521) Vendor ID
--product arg (=32769) Product ID
--mqtt.host arg (=localhost) MQTT broker hostname or IP
--mqtt.port arg (=1883) MQTT broker port
--mqtt.cafile arg Path to file containing the PEM-encoded
CA certificate to connect to Mosquitto
MQTT broker for TLS encryption
--mqtt.certfile arg Path to file containing the PEM-encoded
client certificate to connect to
Mosquitto MQTT broker for TLS
encryption
--mqtt.keyfile arg Path to a file containing the PEM-
encoded unencrypted private key for
this client
--mqtt.client_id arg (=unify_matter_bridge_71460)
Set the MQTT client ID of the
application.