Matter Hardware Requirements#
To run Matter over Thread or over Wi-Fi requires some Silicon Labs hardware in order to run demos and do development. Following are the hardware requirements for both Thread and Wi-Fi use cases broken down by platform and transport protocol.
The following sections describe the hardware that may be used for Matter+OpenThread (Matter Hub and Accessory Device) and for Matter+Wi-Fi (Accessory Device). The EFRMG24 is the preferred starting point for Matter MCUs (including the Matter Hub RCP and both Accessory Devices). It provides Secure Vault and can use the internal flash of the device to store an upgrade image. The EFR32MG24 is recommended for running the Matter over Thread and Matter over Wi-Fi Quick-Start guides.
Matter Over Thread "Matter Hub" Requirements#
If you are running Matter over Thread and do not have a platform on which to run the Open Thread Border Router and chip-tool, Silicon Labs recommends that you run them on a Raspberry Pi. To do so you will need:
Raspberry Pi
Raspberry Pi 4 with an SD card with storage >= 64 GB
The Raspberry Pi 4 is used to run the Open Thread Border Router and the chip-tool. In this documentation the combination of this software on the Raspberry Pi is also called the 'Matter Hub' A software image for the Raspberry Pi is provided on the Matter Artifacts page.
Radio Co-Processor (RCP)
The Matter Hub needs a 15.4 Radio Co-Processor (RCP) in order to create and interact with the Thread network. The RCP can be any Silicon Labs development board that is capable of running the OpenThread RCP firmware. The RCP radio board is connected to the Raspberry Pi via USB.
Over 60 Silicon Labs boards support running the RCP firmware. To build an image for a board which is not listed here, download and build your image in Simplicity Studio. Pre-built OpenThread RCP firmware images are provided for the following boards on the Matter Artifacts page:
Note: The EFR32MG24 is the preferred starting point for Matter MCUs. It provides Secure Vault and can use the internal flash of the device to store an upgrade image.
MG24 boards:
BRD4186C / SLWSTK6006A / Wireless Starter Kit / 2.4GHz@10dBm
BRD4187C / SLWSTK6006A / Wireless Starter Kit / 2.4GHz@20dBm
MG12 boards:
BRD4161A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@19dBm
BRD4162A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@10dBm
BRD4163A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@19dBm
BRD4164A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@19dBm
Matter Over Thread Accessory Device Requirements#
The Matter Accessory Device (MAD) is the actual device that the Matter application firmware (such as the Matter Light or Matter Switch) runs on. Several different platforms for the Matter Accessory Device are supported. Pre-built binary images for the Matter accessory devices are provided on the Matter Artifacts page. Silicon Labs supports development of Matter Accessory Devices for Matter over Thread on the following platforms:
Note: The EFR32MG24 is the preferred starting point for Matter MCUs. It provides Secure Vault and can use the internal flash of the device to store an upgrade image.
MG24 boards:
BRD4186C / SLWSTK6006A / Wireless Starter Kit / 2.4GHz@10dBm
BRD4187C / SLWSTK6006A / Wireless Starter Kit / 2.4GHz@20dBm
BRD2703A / MG24 Explorer Kit Note: This board has yet to be released to the public, but it is supported in the Silicon Labs build flow.
BRD2601B / MG24 Explorer Kit
BRD4319A / SLWSTK6006A / Wireless Starter Kit/ 2.4GHz@20dBm Note: This board has yet to be released to the public, but it is supported in the Silicon Labs build flow.
BRD4316A / SLWSTK6006A / Wireless Start Kit / 2.4GHz@10dBm
BRD4317A / SLWSTK6006A / Wireless Starter Kit/ 2.4GHz@20dBm
MG12 boards:
BRD4161A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@19dBm
BRD4162A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@10dBm
BRD4163A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@19dBm
BRD4164A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@19dBm
BRD4166A / SLTB004A / Thunderboard Sense 2 / 2.4GHz@10dBm
BRD4170A / SLWSTK6000B / Multiband Wireless Starter Kit / 2.4GHz@19dBm, 915MHz@19dBm
Matter over Wi-Fi Accessory Device Requirements for NCP mode#
The Silicon Labs Matter over Wi-Fi NCP mode demo and development requires two boards: the Silicon Labs EFR32 Radio board to run the Matter code and either the RS9116, SiWx917 or WF200 to run the Wi-Fi protocol stack. Pre-built images for the EFR32 are provided on the Matter Artifacts page. Pre-built images for SiWx917 or RS9116 connectivity firmware are also provided on the Matter Artifacts page.
Note:
The EFR32MG24 is the preferred starting point for Matter MCUs. It provides Secure Vault and can use the internal flash of the device to store an upgrade image.
The WF200 connectivity firmware image is included in the EFR32MG12 or EFR32MG24 images on the Matter Artifacts page for running with the WF200 in NCP mode. The Matter application downloads the connectivity firmware onto the WF200 on first-time startup.
The following boards are supported for the Matter over Wi-Fi demos and development:
MG24 boards:
BRD4186C / SLWSTK6006A / Wireless Starter Kit / 2.4GHz@10dBm
MG24 with WSTK : xG24-PK6009A
BRD4187C / SLWSTK6006A / Wireless Starter Kit / 2.4GHz@20dBm
MG24 with WSTK : xG24-PK6010A
Wi-Fi NCP Dev Kits & boards
RS9116
SB-EVK1 / Single Band Wi-Fi Development Kit / 2.4GHz
SB-EVK2 / Single Band Wi-Fi Development Kit / 2.4GHz
DB-EVK1 / Dual Band Wi-Fi Development Kit / 2.4GHz & 5GHz
RS9116X-DB-EVK1Note: Matter only supported over 2.4GHz on this Dev kit.
Interconnect board (included in the Wi-Fi kits)
SPI Cable (included in the RS9116 kit)
Jumper Cables (included in the RS9116 kit)
SiWx917
SiWx917 NCP Mode / Wi-Fi Expansion Board / 2.4GHz
BRD8036A (A0 Expansion v1.0)
BRD8036A (A0 Expansion v1.1)
WF200
WF200 / Single Band Wi-Fi Expansion Board / 2.4GHz
WFM200S / Single Band Wi-Fi Expansion Board / 2.4GHz
Matter over Wi-Fi Accessory Device Requirements for SoC mode#
The Silicon Labs Matter over Wi-Fi demo and development for SoC mode requires the SiWx917 SoC board that supports Matter over Wi-Fi in a single-chip package - the integrated MCU is dedicated for peripheral and application-related processing (Matter), while the multi-threaded processor runs the wireless and networking protocol stacks.
Pre-built images for the SiWx917 connectivity firmware are available as per the instructions on the Matter Artifacts page. The following boards are supported for the Matter over Wi-Fi demos and development:
Wi-Fi SoC boards:
SiWx917 / BRD4002A / Wireless Starter Kit
SiWx917 SoC Mode
SiWx917 SoC / Dual Flash Radio Board / 2.4GHz
BRD4325B - A0 dual flash 1.1
BRD4325B - A0 dual flash 1.2
SiWx917 SoC / Common Flash Radio Board / 2.4GHz
BRD4325C - B0 common flash v1.2
BRD4325G - B0 Stacked Flash + External PSRAM v1.2
Note: Refer SiWx917 SoC for more details
Additional Matter over Wi-Fi Hardware Requirements#
In addition to your Matter over Wi-Fi Accessory Device you will need the following for both running the demo and for development:
Access point with Internet access
microSD card (>=32GB) (if using Raspberry Pi)
[Optional] Android Mobile phone (If using the chip-tool on Android)