Building the 917 SoC Matter Accessory Devices (MADs) using Simplicity Studio#
In Simplicity Studio 5, create the Light MAD:
- Download and Install Simplicity Studio 5. 
- To install the prerequisites for Simplicity Studio, click on - Install -> SDKsin launcher tab and install the following packages in the given order:
   Gecko SDK
   Silicon Labs Matter
   WiseconnectNote: Version numbers mentioned in the screenshot might be outdated. Install the latest packages available with the studio.


- If you have more than one Gecko SDK then select the preferred version of Gecko SDK. So for that in launcher tab go to - preferences -> Simplicity Studio -> SDKs.  
- Switch to the Launcher view (if not already in it).   
- Go to - All Productsin launcher tab and select one compatible board from the below supported list of SiWx917 SOC dev boards.
  BRD4325B (Dual Flash)
  BRD4325C (Common Flash)
  BRD4325G (Common Flash)

- Once it shows up in the Debug Adapters view, select it.   
- Open the Example Projects and Demos tab, select the Matter filter and enter "Wi-Fi" in Filter on keywords.   
- Select the Matter - SoC Lighting over Wi-Fi example for SiWx917 SOC, click Create, rename the project if you wish, and click Finish.   
- Once the project is created, right-click on the project and select Build Project in the Project Explorer tab.   
- To flash the application, connect the compatible dev board to the machine or PC if not yet done. 
- Once the project is compiled successfully, Go to the Project Explorer view and select the binary to be flashed.   
- Right-click on the selected _isp.bin binary and click on flash to device.   
- Flash programmer window will be opened, Click on Program button to start the flashing.   
Note: Output of the SiWX917 SoC application will be displayed on the J-Link RTT Viewer.
- In order to debug Matter Application, Right-click on the selected _isp.bin binary and click on Debug As.