Creating Matter Applications using SLC CLI#
The Silicon Labs Configurator (SLC) offers command-line access to application configuration and generation functions. Software Project Generation and Configuration with SLC-CLI provides a complete description and instructions on downloading and using the SLC-CLI tool.
This guide lists the steps to create and build a Silicon Labs Matter SLC project using SLC-CLI and make. These scripts are evaluation quality and have been verified to work on Ubuntu 22.04.3 LTS, MacOS Version 13.5.1, and Windows 10.
Setting up the Environment#
Clone Gecko SDK:
git clone https://github.com/SiliconLabs/gecko_sdk.gitCreate a directory named extension inside the Gecko SDK directory.
Clone the Matter GSDK Extension inside the extension directory:
git clone https://github.com/SiliconLabs/matter_extension.gitYour path to the Matter extension should look like
<Path/To/Gsdk/Download>/extension/matter_extensionInstall the following python packages:
pip3 install dloadChange directory to cloned extension directory and run the sl_setup.py script. This will install the ARM gcc toolchain, SLC-CLI, ZAP, Simplicity-commander, and Java.
For Mac and Linux:
cd extension/matter_extension
python3 slc/sl_setup_env.pyFor Windows:
cd extension\matter_extension
python slc\sl_setup_env.pyThe sl_setup_env.py script creates an .env file to be used to set the environment variables needed for the installed tools, ARM toolchain, SLC-CLI, Java ZAP, Simplicity-commander, and Java.
Creating an Application Project#
Run the sl_create_new_app.py script to create a BRD4161A project with name MyNewApp starting from the lighting-app-thread.slcp example application project file:
The script will ask user permission to trust the gecko_sdk and matter_extension before generating.
For Mac and Linux:
python3 slc/sl_create_new_app.py MyNewApp slc/sample-app/lighting-app/efr32/lighting-app-thread.slcp brd4161aFor Windows:
python slc\sl_create_new_app.py MyNewApp slc\sample-app\lighting-app\efr32\lighting-app-thread.slcp brd4161aBuilding an Application Project#
After a project is created the sl_build.py script can be used to re-generate the MyNewApp project and build it:
For Mac and Linux:
python3 slc/sl_build.py MyNewApp/lighting-app-thread.slcp brd4161aFor Windows:
python slc\sl_build.py MyNewApp\lighting-app-thread.slcp brd4161aAlternately, one can use SLC-CLI commands directly to generate the project and then use make to build it.
Windows users will need to install make in their system. You can use your own or follow these steps to get make.
Install the MSYS terminal, which provides a Unix-like environment on Windows.
Open the MSYS terminal and install
makeusing the commandpacman -S make.Run command
where make, copy the path, and add it to the PATH environment variable.Restart your command line terminal and run
slc/sl_build.pyor run make directly. You might need to reboot.
Note: In rare cases, the build may fail due to missing files in the zap-generated/ directory. The workaround is to delete the .zap folder in the home directory.
Modifying an Application Project#
The resulting user project can be modified like any other SLC project: software components can be added or removed by modifying the project's .slcp file, configuration can be applied by modifying the files in the config directory, the application logic can be managed through the files in the src directory. Various SLC-CLI commands can be used to examine, validate, or re-generate the project after a modification, see Software Project Generation and Configuration with SLC-CLI for more information.
For modifying Matter endpoints and clusters invoke the ZAP tool passing to it the application's ZAP file:
./scripts/tools/zap/run_zaptool.sh MyNewApp/config/common/lighting-thread-app.zap