How to Flash a Silicon Labs Device#

Once you have an image built, you can flash it onto your EFR or SiWx917 device (either a development board or the Thunderboard Sense 2) over USB connected to your development machine. This can be done using either Simplicity Studio or the standalone Simplicity Commander.

Simplicity Studio#

Simplicity Studio is a complete development environment and tool suite. It has the ability to discover USB-connected development boards and flash them.

Simplicity Commander#

Links to download Simplicity Commander's standalone versions are included below. Full documentation on Simplicity Commander is included in the Simplicity Commander Reference Guide