Event#
Events are records of past state transitions such as a light device's on-off attribute changing from on to off.
The autogenerated file include/AppEvent.h
houses the definition of the event object used by the application. It contains the event types, the structures for each event, and event handler.
Header File#
This file contains the high level namespaces and constant definitions for Events. In Simplicity Studio, this will be generated in the autogen/zap-generated/ folder of the matter project.