Edit

Matter Intermittently Connected Devices over OpenThread#

This page explains how Matter OpenThread Intermittently Connected Devices (ICDs) work and how to configure an ICD example.

Overview#

Matter provides an Intermittently Connected Device (ICD) operating mode to extend the battery life of power-limited devices. The Matter ICD manager leverages subscription report synchronization and OpenThread functionalities to allow devices to sleep for set periods without disrupting their Matter sessions.

Currently, in Matter v1.2, only ICD with Short Idle Time (SIT) is supported. ICD SIT are devices that SHOULD be configured with a Slow Polling Interval shorter than or equal to 15 seconds. For example, in a typical scenario for door locks and window coverings, commands need to be sent to the ICD with a use-case imposed latency requirement. Typically, devices that are Short Idle Time ICDs are not initiators in the communication flow.

Operating Modes#

ICDs have two operating modes: Idle and Active. An ICD alternates normally between the Idle mode and Active mode based on the IdleModeInterval and ActiveModeInterval respectively.

When the device is in Active Mode, the ICD is set into a fast-polling interval for maximum responsiveness. The CHIP_DEVICE_CONFIG_ICD_FAST_POLL_INTERVAL parameter communicates the maximum sleep interval of a node in active mode.

Any of the following device states will start or keep the ICD in Active Mode:

  • A commissioning window is open

  • An exchange context is awaiting a response or ack

  • The fail-safe is armed

Any of the following events can trigger the start of the Active Mode interval or extend it by one ActiveModeThreshold:

  • A message needs to be sent

  • A message was received

  • An implemented user action occurred

Once the active mode is triggered, the ICD stays in this mode for a minimum duration of ActiveModeInterval When the active interval has elapsed and none of the aforementioned states are active, the device will switch its operating mode to the Idle Mode.

In Idle mode, the ICD will poll its associated router at its slow-polling interval to see if another device has tried to communicate with it while it was sleeping. If no event occurs, the ICD stays in its idle mode for the entirety of the IdleModeInterval. The CHIP_DEVICE_CONFIG_ICD_SLOW_POLL_INTERVAL parameter communicates the slow-polling interval and therefore the maximum sleep interval of the node in idle mode. This parameter affects both the minimum power consumption and maximum latency.

Thread Communication#

In order to receive messages that were sent while the ICD was sleeping, the ICD relies on its associated Thread router which buffers any incoming messages. The Thread router will send all buffered messages to the ICD when it polls the router at the end of its slow-polling interval.

Configuration#

Matter exposes some defines to configure the polling intervals of the OpenThread stack in both Idle and Active modes.

Parameter Name

Define

Description

Default Value

Maximum Allowed Value

SlowPollInterval

CHIP_DEVICE_CONFIG_ICD_SLOW_POLL_INTERVAL (SL_OT_IDLE_INTERVAL)

Interval, in milliseconds, at which the thread radio will poll its network in idle mode.

15000 ms

<= IdleModeInterval

FastPollInterval

CHIP_DEVICE_CONFIG_ICD_FAST_POLL_INTERVAL (SL_OT_ACTIVE_INTERVAL)

Interval, in milliseconds, at which the thread radio will poll its network in active mode.

200 ms

< ActiveModeInterval