Edit

Serial Port Communication on the Silicon Labs Platform (Matter Shell)#

The matter-shell exposes the configuration and the management APIs via the matter command line interface (matter CLI). This interface can be used to change the state of the device.

Hardware Requirements#

To run matter shell on the Silicon Labs Platform, refer to the Hardware Requirements.

Software Requirements#

To run matter shell on the Silicon Labs Platform, refer to the Software Requirements.

Execute Matter Shell on Silicon Labs Platform#

  1. Download and install Simplicity Studio.

  2. To install the software packages for Simplicity Studio, refer to Software Package Installation.

  3. Log in to Simplicity Studio and connect the EFR32MG2x or SiWx917 SOC board to the computer.

  4. Go to the All Products section.

    Silicon Labs - designSilicon Labs - design

  5. Type and select the radio board from the displayed list and click Start.

    Silicon Labs - designSilicon Labs - design

  6. The Launcher page will display the selected radio board's details.

    Silicon Labs - designSilicon Labs - design

  7. Verify the following in the General Information section:

    • The Debug Mode is Onboard Device (MCU).

    • The Preferred SDK is the version you selected earlier.

    Silicon Labs - designSilicon Labs - design

  8. Open the Example Projects and Demos tab and create a project for the Matter Lock Application.

    Silicon Labs - designSilicon Labs - design

  9. In the New Project Wizard window, click Finish.

    Silicon Labs - designSilicon Labs - design

  10. After creation of project, open the Software Components tab and, in the search bar, type Matter Shell and install it.

    Silicon Labs - designSilicon Labs - design

  11. Build the project after enabling the Matter Shell component.

  12. After a successful build, commission the device as described in Commission Matter Platform.

  13. Open Tera Term and under New connection, select Serial, and in the dropdown, select the JLink port, and click OK.

    Silicon Labs - designSilicon Labs - design

  14. In the menu bar, click Setup > Terminal.

    Silicon Labs - designSilicon Labs - design

  15. Inside Terminal, set the values below and click OK.

    • Terminal Size : 80 * 24

    • New-Line

      • Receive : CR+LF

      • Transmit : CR+LF

    Silicon Labs - designSilicon Labs - design

  16. In the menu bar, click Setup > Serial port.

    Silicon Labs - designSilicon Labs - design

  17. Increase the speed to 115200 and click New setting.

    Silicon Labs - designSilicon Labs - design

  18. In the menu bar, click File > TTY Record. Create any empty file with extension ".tty" and click Save.

    Silicon Labs - designSilicon Labs - design

  19. After creating the tty file, press Enter to open the matterCli terminal.

    Silicon Labs - designSilicon Labs - design

  20. Send any command through the matterCli terminal, from the below list of commands:

    • doorlock event door-state-change "DoorState"

      • Door State List

      • DoorOpen = 0

      • DoorClosed = 1

      • DoorJammed = 2

      • DoorForcedOpen = 3

      • DoorUnspecifiedError = 4

      • DoorAjar = 5

    • doorlock event lock-alarm "AlarmCode"

      • Alarm Code List

      • LockJammed = 0

      • LockFactoryReset = 1

      • LockRadioPowerCycle = 3

      • WrongCodeEntryLimit = 4

      • FrontEsceutcheonRemoved = 5

      • DoorForcedOpen = 6

      • DoorAjar = 7

      • ForcedUser = 8

    • onboardingcodes ble, command will show QR Code.

      Silicon Labs - designSilicon Labs - design

  21. After changing DoorState and AlarmCode in matterCli, run the commands below using chip-tool on Raspberry PI to verify the event.

    • To Read Door State

      ./chip-tool doorlock read-event door-state-change "node_id" "endpoint"

    • To Read Alarm Code

      ./chip-tool doorlock read-event door-lock-alarm "node_id" "endpoint"

Note: Type help in matterCli terminal for more information about supported features.