Matter + AWS Component#
Matter + AWS is a Silicon Labs–specific feature that enables Matter devices to connect directly to proprietary cloud solutions, such as AWS Cloud. As such, a Matter Wi-Fi device must support connecting locally on the Matter Fabric via IPv6 and connecting to the Internet via IPv4.
Matter devices can be controlled by chip-tool or a controller. The status of the modified attributes will be published to the cloud.
Remote users can install a cloud-specific application to receive notifications about the attribute status.
Matter + AWS Flavors#
Matter + AWS is available in two build flavors:
Standard flavor — For 917 SoC and standard 917 NCP boards. Uses the host LwIP stack for both Matter (IPv6) and AWS (IPv4) with
matter_lwipandmatter_aws_transport_lwip. See Build Procedure for Matter + AWS.Dual-stack flavor (917 NCP) — For 917 NCP boards only. Uses a split-stack architecture: Matter over IPv6 on the EFR32 host LwIP stack and AWS over IPv4 on the SiWx917 NWP offload stack with
matter_dual_stackandmatter_aws_transport_nwp. See Matter + AWS Dual Stack Overview and Build Procedure for Matter + AWS Dual Stack.
Matter + AWS Feature Diagram#
The following diagram shows end-to-end flow for Direct Internet Connectivity.


Prerequisites#
Hardware Requirements#
For a list of hardware requirements for the Matter + AWS feature, see the official Silicon Labs Matter hardware requirements documentation.
Note: The standard flavor is supported for 917 SoC and NCP boards. The dual-stack flavor is supported for 917 NCP boards only (EFR32 host + BRD4346A).
Software Requirements#
For a list of software requirements for the Matter + AWS feature, see the official Silicon Labs Matter Software requirements documentation.
End-to-End Set-up bring up#
Message Queuing Telemetry Transport (MQTT)#
MQTT is an OASIS standard messaging protocol for the Internet of Things (IoT). It is designed as an extremely lightweight publish/subscribe messaging transport that is ideal for connecting remote devices with a small code footprint and minimal network bandwidth. For more details, visit https://mqtt.org/.
Configuring the MQTT server#
To set up and configure AWS for Matter + AWS support, see the following documentation:
Remote User Setup (MQTT Explorer) (optional)#
Remote users are used to check the state of Matter devices. In this context, MQTT Explorer acts as a remote user. For more information, see MQTT Explorer Setup and Configuration.
Building Matter + AWS Application using Simplicity Studio#
Follow the steps in Build Procedure for Matter + AWS to enable the Matter + AWS feature for the standard flavor (917 SoC and standard 917 NCP).
For the dual-stack flavor on 917 NCP boards, follow Build Procedure for Matter + AWS Dual Stack.
End-to-End Test of Matter + AWS Application#
User Setup (MQTT Explorer):
Sharing status of device to cloud
The following diagram shows the end-to-end flow for sharing status from a Matter device to the cloud.


Note: For reference, the diagram shows Lighting App commands. Other application commands also can be passed.
For the end-to-end commands to be executed from chip-tool, refer to Running the Matter Demo Over Wi-Fi.
The following application-specific attributes or states are shared to the cloud:
For Lighting App, On/Off Attributes
For Lock App, lock/unlock Attributes
For Windows App, lift/tilt Attributes
For Thermostat App, SystemMode/CurrentTemp/LocalTemperature/OccupiedCoolingSetpoint/OccupiedHeatingSetpoint Attributes
For On/off Plug App, On/Off Attributes
The MQTT Explorer UI updates the application status as shown in following image.


Control of the device through cloud interface
The following diagram shows the end-to-end flow for control of the Matter device through a cloud interface.


Note: For reference, the diagram shows Lighting App commands. Other application commands also can be passed.
Ensure that the Matter device is running and successfully commissioned. For detailed steps, refer to Running the Matter Demo Over Wi-Fi.
To control the device, set the topic name and the commands to be executed in the MQTT Explorer for the following applications.
- Lighting App
- Topic: command
- Commands:
- toggle
- on
- off
- Onoff Plug
- Topic: command
- Commands:
- toggle
- on
- off
- Lock App
- Topic: command
- Commands:
- lock
- unlock
- Thermostat App
- Topic: command
- Commands:
- SetMode/value(value need to provide 1,2,3,4 ex:SetMode/1)
- Heating/value(value need to provide 2500,2600 ex:HeatingSetPoint/2500)
- Cooling/value(value need to provide 2500,2600 ex:CoolingSetPoint/2500)
- Window App
- Topic: command
- Commands:
- Lift/value(value need to provide in range 1000 to 10000)
- Tilt/value(value need to provide in range 1000 to 10000)Click Publish to execute the command.