Amazon Web Services (AWS)#
Amazon Web Services offers reliable, scalable, and inexpensive cloud computing services. Refer to AWS Documentation for more details.
AWS CA Certificate Registration#
Open AWS.
Log in using your AWS credentials.
Go to Security > Policies and select Create Policy. Enter the policy name (e.g.,
MATTER_AWS_POLICY_). In the policy statements, select JSON and replace the contents with the JSON provided below:{ "Version": "2012-10-17", "Statement": [ { "Effect": "Allow", "Action": "*", "Resource": "*" } ] }Once done, select Create.
Create a client CSR certificate and a client key by following the steps in the OpenSSL Certificate Creation documentation.
Complete the following steps to create a thing and generate certificates for your Matter application to use in the
MatterAwsNvmCert.cppsource file:Go to All Devices > Things and select Create Things.
Select Create Single Thing and click Next.
Under Info > Give the thing a name, specify the thing name (this will be the client ID), then click Next.
(Optional) Configure the device certificate under Info > Upload CSR.
In Certificate > Choose file (Choose Client CSR generated in Openssl Certificate Creation ex:
device.csr). Click Next.Use the policy (e.g.,
MATTER_AWS_POLICY_) created in AWS Certificate creation.Once the thing is successfully created, activate and download the certificate.
Copy the contents of AWS_CA CERT and add it as CA certificate in
MatterAwsNvmCert.cpp.Repeat Step 5 to create a new thing for use in MQTT Explorer, using the certificate generated for MQTT Explorer during OpenSLL certificate creation (e.g.,
explorer.csr). Create a.pemfile from the CA certificate in step 8 and use it as the server certificate in MQTT Explorer.Note: The thing name must be unique as it will be used as the client ID.