OpenSSL Certificate Creation#
An SSL certificate is an important way to secure user information and protect against hackers.
Openssl Installation (In ubuntu 22.04)#
To install OpenSSL (v 3.0.2), issue the following command:
sudo apt install openssl
Certificates Creation#
Use the following commands to generate certificates:
Generate the client key:
openssl ecparam -name prime256v1 -genkey -noout -out device.key
Generate the client certificate (e.g.,
device.crtanddevice.key) using a CA certficate:openssl req -new -out device.csr -key device.key
Upload CSR to AWS: While creating the AWS IoT thing, use the Upload CSR option in the configure device certificate step. Once the CSR generated in step 2 is uploaded, AWS will generate an AWS CA-authenticated
device.crt.

To use MQTT Explorer, repeat steps 1 and 2 to create an additional set of certificates
(e.g., explorer.crt and explorer.key). Use a different name to uniquely identify the certificates.