Reset cause of the bootloader.
Public Attributes#
uint16_t
Reset reason as defined in the reset information.
uint16_t
Signature indicating whether the reset reason is valid.
Public Attribute Documentation#
reason#
uint16_t BootloaderResetCause_t::reason
Reset reason as defined in the reset information.
Definition at line
158
of file platform/bootloader/api/ember_btl_interface.h
signature#
uint16_t BootloaderResetCause_t::signature
Signature indicating whether the reset reason is valid.
Definition at line
159
of file platform/bootloader/api/ember_btl_interface.h