Application Properties struct.
Public Attributes#
uint8_t
Magic value indicating this is an ApplicationProperties_t struct.
uint32_t
Version number of this struct.
uint32_t
Type of signature this application is signed with.
uint32_t
Location of the signature. Typically points to the end of the application.
Information about the application.
Pointer to information about the certificate.
uint8_t *
Pointer to Long Token Data Section.
const uint8_t
Parser Decryption Key.
Public Attribute Documentation#
magic#
uint8_t ApplicationProperties_t::magic[16]
Magic value indicating this is an ApplicationProperties_t struct.
Must equal APPLICATION_PROPERTIES_MAGIC
signatureType#
uint32_t ApplicationProperties_t::signatureType
Type of signature this application is signed with.
signatureLocation#
uint32_t ApplicationProperties_t::signatureLocation
Location of the signature. Typically points to the end of the application.
cert#
ApplicationCertificate_t* ApplicationProperties_t::cert
Pointer to information about the certificate.
longTokenSectionAddress#
uint8_t* ApplicationProperties_t::longTokenSectionAddress
Pointer to Long Token Data Section.