LZMA Programming Tag#

Tag to handle LZMA compressed programming data.

Functions#

int32_t
gbl_lzmaEnterProgTag(ParserContext_t *ctx)

Enter an LZMA compressed programming tag.

int32_t
gbl_lzmaParseProgTag(ParserContext_t *ctx, void *data, size_t length, const BootloaderParserCallbacks_t *callbacks)

Parse a chunk of data from an LZMA compressed programming tag.

int32_t
gbl_lzmaExitProgTag(ParserContext_t *ctx, const BootloaderParserCallbacks_t *callbacks)

Exit an LZMA compressed programming tag.

size_t
gbl_lzmaNumBytesRequired(ParserContext_t *ctx)

Number of bytes needed for next stage of parsing.

Macros#

#define
LZMA_COUNTER_SIZE_KB (10UL)

The maximum size of the array holding probability model counters.

#define
LZMA_DICT_SIZE_KB (8UL)

The maximum size of the dictionary.

Function Documentation#

gbl_lzmaEnterProgTag#

int32_t gbl_lzmaEnterProgTag (ParserContext_t * ctx)

Enter an LZMA compressed programming tag.

Parameters
TypeDirectionArgument NameDescription
ParserContext_t *N/Actx

Parser context

Returns

  • Error code


Definition at line 124 of file platform/bootloader/parser/compression/btl_decompress_lzma.h

gbl_lzmaParseProgTag#

int32_t gbl_lzmaParseProgTag (ParserContext_t * ctx, void * data, size_t length, const BootloaderParserCallbacks_t * callbacks)

Parse a chunk of data from an LZMA compressed programming tag.

Parameters
TypeDirectionArgument NameDescription
ParserContext_t *N/Actx

Parser context

void *N/Adata

Input data to parse

size_tN/Alength

Length of data

const BootloaderParserCallbacks_t *N/Acallbacks

Callbacks to call with parsed data

Returns

  • Error code


Definition at line 135 of file platform/bootloader/parser/compression/btl_decompress_lzma.h

gbl_lzmaExitProgTag#

int32_t gbl_lzmaExitProgTag (ParserContext_t * ctx, const BootloaderParserCallbacks_t * callbacks)

Exit an LZMA compressed programming tag.

Parameters
TypeDirectionArgument NameDescription
ParserContext_t *N/Actx

Parser context

const BootloaderParserCallbacks_t *N/Acallbacks

Callbacks to call with parsed data

Returns

  • Error code


Definition at line 147 of file platform/bootloader/parser/compression/btl_decompress_lzma.h

gbl_lzmaNumBytesRequired#

size_t gbl_lzmaNumBytesRequired (ParserContext_t * ctx)

Number of bytes needed for next stage of parsing.

Parameters
TypeDirectionArgument NameDescription
ParserContext_t *N/Actx

Parser context

Returns

  • Number of bytes required


Definition at line 156 of file platform/bootloader/parser/compression/btl_decompress_lzma.h