Reset cause of the bootloader.

Public Attributes#

uint16_t

Reset reason as defined in the reset information.

uint16_t

Signature indicating whether the reset reason is valid.

Public Attribute Documentation#

reason#

uint16_t BootloaderResetCause_t::reason

Reset reason as defined in the reset information.


Definition at line 56 of file platform/bootloader/api/btl_reset_info.h

signature#

uint16_t BootloaderResetCause_t::signature

Signature indicating whether the reset reason is valid.


Definition at line 58 of file platform/bootloader/api/btl_reset_info.h